Tutorials

Hookup Guide for the SparkFun Artemis Thing Plus

September 19, 2019
Get started with our SparkFun Artemis Thing Plus - our popular Thing Plus footprint with the powerful Artemis module for ultimate functionality.

SparkFun Pulse Oximeter and Heart Rate Monitor Hookup Guide

September 12, 2019
Find out your oxygen saturation level or check out your heart rate using the MAX30101 biometric sensor and MAX32664 Biometric Hub via I2C!

ESP32 Relay Web Server

September 10, 2019
The goal of this project is to have a website hosted on an ESP32 that controls any relay controlled device connected to a local network and keeps a dynamically updated state of those devices.

SparkFun gator:RTC Hookup Guide

September 5, 2019
The gator:RTC is an I2C based, real-time clock (RTC) for keeping time while your micro:bit isn't powered. This tutorial will get you started using the gator:RTC with the micro:bit platform.

SparkFun gator:UV Hookup Guide

September 5, 2019
The gator:UV is an I2C based UV sensor. This tutorial will get you started using the gator:UV with the micro:bit platform.

SparkFun gator:log Hookup Guide

September 5, 2019
The gator:log is a serial communication based data logger. This tutorial will get you started using the gator:log with the micro:bit platform.

Hookup Guide for the SparkFun RedBoard Artemis Nano

August 28, 2019
Get started with the powerful RedBoard Artemis Nano

Hookup Guide for the SparkFun RedBoard Artemis

August 28, 2019
Get started with the RedBoard Artemis - all the functionality of the SparkFun Artemis module wrapped in the familiar Uno R3 footprint

Hookup Guide for the SparkFun RedBoard Artemis ATP

August 28, 2019
Get started with the RedBoard Artemis ATP - all the functionality of the SparkFun Artemis module wrapped in the Mega Arduino Footprint

XBee3 Thing Plus Hookup Guide

August 22, 2019
Get started with SparkFun's XBee3 Thing Plus - both the u.FL as well as the PCB antenna versions.

Qwiic Atmospheric Sensor (BME280) Hookup Guide

August 21, 2019
Measure temperature, humidity, barometric pressure with the SparkFun Atmospheric Sensor Breakout BME280 (Qwiic).

SparkFun Inventor's Kit Experiment Guide - v4.1

August 8, 2019
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.1.2 and v4.1.

How to Install CH340 Drivers

August 6, 2019
How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.

PCA9306 Logic Level Translator Hookup Guide (v2)

July 25, 2019
A quick primer to get you going with the PCA9306 Logic Level Converter - a dedicated I2C translator.

SparkFun AS3935 Lightning Detector Hookup Guide (v20)

July 25, 2019
Are you worried about the looming clouds in the distance, how far away is that storm exactly? Add lightning detection with the AS3935 to your next weather station or your next bike ride!

LilyPad RGB LED Hookup Guide

July 18, 2019
Learn how to hook up the LilyPad RGB LED and use a common cathode RGB LED in e-textile projects.

EL Wire Pants

July 18, 2019
In this tutorial, we will sew standard electroluminescent (EL) wire to a pair of pants.

Modifying Your EL Wire Inverter

July 18, 2019
In this tutorial, we will modify the 12V EL wire inverter to power the EL Sequencer/EL Escudo Dos off a single power supply.

Qwiic Ambient Light Sensor (VEML6030) Hookup Guide

July 18, 2019
The VEML6030 is a high accuracy ambient light sensor with 16-bit resolution. This I2C sensor can detect light similar to the human eye response. Start detecting light levels in your environment!

Pi Servo pHAT (v2) Hookup Guide

July 11, 2019
This hookup guide will get you started with connecting and using the Pi Servo pHAT on a Raspberry Pi.

SparkFun 9DoF IMU (ICM-20948) Breakout Hookup Guide

June 27, 2019
How to use the SparkFun 9DoF ICM-20948 breakout board for your motion sensing projects. This breakout is ideal for wearable sensors and IoT applications.

Artemis Development with Arduino

June 20, 2019
Get our powerful Artemis based boards (Artemis Nano, BlackBoard Artemis, and BlackBoard Artemis ATP) blinking in less than 5 minutes using the SparkFun Artemis Arduino Core!

Designing with the SparkFun Artemis

June 20, 2019
Let's chat about layout and design considerations when using the Artemis module.

SparkFun gator:particle Hookup Guide

June 13, 2019
The gator:particle is an I2C heart-rate monitor and pulse oximeter that can be used as a particle sensor. This tutorial will get you started using the gator:particle with the micro:bit platform.