Hookup
This type of tutorial shows people how to get a specific product hooked up and working.
Sort by:
Recently Added
Viewing 572 Hookup Tutorials.
View All Tutorials.
Little Soundie Audio Player Hookup Guide
Add sound effects to your project, prop or costume with Little Soundie Audio Player.
Noisy Cricket Stereo Amplifier - 1.5W Hookup Guide
A hookup guide for the Noisy Cricket Stereo Amplifier - 1.5W.
LilyPad Tri-Color LED Hookup Guide
Learn how to hook up the LilyPad Tri-Color LED and use a common anode RGB LED in e-textile projects.
Addressable LED Neon Flex Rope Hookup Guide
The addressable (UCS1903) LED neon flex rope adds cool lighting effects for outdoor and indoor uses including in hallways and stairs, holiday lighting, and more! In this hookup guide, you will learn how to connect, power, and control the LED segments with an Arduino and the FastLED library.
TFMini - Micro LiDAR Module Hookup Guide
The TFMini is a ToF (Time of Flight) LiDAR sensor capable of measuring the distance to an object as close as 30 cm and as far as 12 meters! The TFMini allows you to integrate LiDAR into applications traditionally reserved for smaller sensors such as the SHARP GP-series infrared rangefinders.
Qwiic Accelerometer (MMA8452Q) Hookup Guide
Freescale’s MMA8452Q is a smart, low-power, three-axis, capacitive micro-machined accelerometer with 12-bits of resolution. It’s perfect for any project that needs to sense orientation or motion. We’ve taken that accelerometer and stuck it on a Qwiic-Enabled breakout board to make interfacing with the tiny, QFN package a bit easier.
Qwiic Distance Sensor (RFD77402) Hookup Guide
The RFD77402 uses an infrared VCSEL (Vertical Cavity Surface Emitting Laser) TOF (Time of Flight) module capable of millimeter precision distance readings up to 2 meters. It’s also part of SparkFun’s Qwiic system, so you won’t have to do any soldering to figure out how far away things are.
Getting Started with Chibi Chip and Clip
This tutorial goes over the how to assemble the Chibitronics' Chibi Chip programmable microcontroller with the Chibi Clip to add more functionality to your paper circuits! Start programming your Chibi Chip by writing code (block-based and text-based) in a browser-based code editor and then transmit code through sound to your board!
Fingerprint Scanner (GT-521Fxx) Hookup Guide
This tutorial provides information about how to connect to ADH-Tech's fingerprint scanner (GT-521F32) and how to use it with Hawley's FPS_GT511C3 library for Arduino.
AST-CAN485 Hookup Guide
The AST CAN485 is a miniature Arduino in the compact form factor of the ProMini. In addition to all the usual features it has on-board CAN and RS485 ports enabling quick and easy interfacing to a multitude of industrial devices.
Getting Started with Walabot
See through walls, track objects, monitor breathing patterns, and more using the power of radio frequency with the Walabot! In this tutorial, we will explore Walabot’s features using the Software Demo Kit (SDK) on Windows and the Application Programming Interface (API) on Linux-based distributions for embedded projects.
FreeSoC2 Hookup Guide V14
The FreeSoC2 is an Arduino-compatible PSoC5LP-based development board, produced by SparkFun in collaboration with Jon Moeller (developer of the original FreeSoC) and Cypress Semiconductor.
AT42QT101X Capacitive Touch Breakout Hookup Guide
Learn how to use the simple SparkFun AT42QT1010 and AT42QT1011 capacitive touch breakout boards.
LilyPad Temperature Sensor Hookup Guide
How to hook up the LilyPad Temperature Sensor as well as some project ideas and example code.
Qwiic Human Presence Sensor (AK9753) Hookup Guide
How to get started with your Qwiic enabled AK9753 Human Presence Sensor.
Qwiic Micro OLED Hookup Guide
Get started displaying things with the Qwiic Micro OLED.
Makey Makey Classic Hookup Guide
Be stoked! The world is your construction kit. How to turn everyday objects into computer inputs with the Makey Makey Classic from JoyLabz.
H3LIS331DL Accelerometer Breakout Hookup Guide
Hookup guide and library usage details for the triple axis accelerometer H3LIS331DL high-g accelerometer.
Getting Started with TJBot
This post will walk you through setting up your TJBot and getting started with the first three recipe examples provided by IBM.
LilyPad E-Sewing ProtoSnap Hookup Guide
Explore the LilyPad E-Sewing ProtoSnap and learn how to build it into a project.
Qwiic Adapter Hookup Guide
Get started with your Qwiic adapter board. This adapter breaks out the I2C pins from the Qwiic connectors to pins that you can easily solder with your favorite I2C enabled device.
Qwiic HAT for Raspberry Pi Hookup Guide
Get started interfacing your Qwiic enabled boards with your Raspberry Pi. This Qwiic connects the I2C bus (GND, 3.3V, SDA, and SCL) on your Raspberry Pi to an array of Qwiic connectors.
ESP32 Thing Motion Shield Hookup Guide
Getting started with the ESP32 Thing Motion Shield to detect movements using the on-board LSM9DS1 IMU and adding a GPS receiver. Data can be easily logged by adding an microSD card to the slot.
SparkFun Inventor's Kit Experiment Guide - v4.0
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.0a.
Sort by:
Recently Added
Viewing 572 Hookup Tutorials.
View All Tutorials.