Getting Started with Chibi Chip and Clip

≡ Pages
Contributors: bboyho

Introduction

Looking to add more functionality to your paper circuits? This tutorial goes over the how to assemble the Chibi Chip programmable microcontroller with the Chibi Clip to add more functionality to your paper circuits! We will also go over how to program your Chibi Chip microcontroller board by writing code (block-based and text-based) in a browser-based code editor and then transmit code through sound to your board.

Love to Code Chibi Chip Microcontroller Board

DEV-14591
Retired

Love to Code Chibi Clip Mounting Accessory

DEV-14593
Retired

Ready? Let’s get started!

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

  • Chibi Chip Programmable Microcontroller Board
  • Chibi Clip Mounting Accessory
  • Programming Cable with USB and Audio Connectors
  • USB Power Supply
    • (i.e. Computer, Wall Plug or Portable USB Battery Charger)
  • Programming Device with 3mm Audio Jack
    • (i.e. Computer, Phone, or Tablet)
  • Internet Connection

Suggested Videos

Suggested Reading

You may need to know the following concepts before working with one of these boards:

What is a Circuit?

Every electrical project starts with a circuit. Don't know what a circuit is? We're here to help.

Voltage, Current, Resistance, and Ohm's Law

Learn about Ohm's Law, one of the most fundamental equations in all electrical engineering.

Polarity

An introduction to polarity in electronic components. Discover what polarity is, which parts have it, and how to identify it.

The Great Big Guide to Paper Circuits

Let's take a look at different materials we can use to combine paper crafting and electronics.

Assemble Your Chibi Clip

The following will show you how to connect the Chibi Chip programmable board into a reusable clip to add more functionality to your paper circuits!

Assembled Chibi Chip and Clip

Suggested Viewing

Hardware Hookup

Remove example paper insert.

Remove Paper

Remove the adhesive tape from your clip holder.

Remove Adhessive

Flip the clip over so that the flat side showing “Chibitronics” faces up and open the clip.

Flip Open Clip

Hold your Chibi Chip with flat side facing up and insert the flexible part into the three notches on the mouth of the clip.

Close the clip and gently bend the board up over the clip.

Bend Board Over Clip

Slide the rigid board into the hook at the top of your clip.

Slide Board into Tab

You’re done! Now you can open and close the clip with your Chibi Chip attached.

Try creating a simple circuit with one LED and traces that align to the Chibi Chip and clip's tabs.

Attaching/Detaching Chibi Chip and Clip To/From Circuit

Removing Chibi Chip from Clip

If you need to remove the Chibi Chip from your clip, slide out the flexible part from the clip and the rest of the board will slide off.

Removing Chibi Chip from Clip

Power Your Circuit

You can power your Chibi Chip with any 5V USB power supply! Here are a few examples.

Love to Code Powered Binder

If you have a Love to Code powered binder with batteries, you can plug in the USB cable directly into the binder. To turn on your binder, slide the power switch to the left like this:

Plugging in and Powering on from Chibitronics on Vimeo.

Computer USB Port

You can also use a computer or laptop USB port to power the Chibi Chip.

Comptuer USB Port

USB Wall Adapter

USB wall adapters also make great power supplies since you don’t need to worry about running down batteries.

USB Wall Adapter

USB Battery Packs

Finally, USB phone charger battery packs work as a handy portable power supply! Make sure your charger battery pack has an on/off switch so that you can keep the power supply on. The Chibi Chip runs on low power so the battery pack may automatically turn off by itself.

Uploading via Audio

The Chibi Chip uses an audio connector to upload code! Let's go over how to make the connection.

Hardware Hookup

Plug in the other end of the micro-B USB into the Chibi Chip board's USB connector.

Connect to Chibi Chip

Plug the audio cable into the audio jack of your programming device (i.e computer, phone, or tablet).

Unmute your device and turn the volume all the way up. This will make sure the code plays to your Chibi Chip loud and clear!

Volume

Press the PROG button on the Chibi Chip and hold it until the PROG light blinks and stays red. This puts your Chibi Chip into programming mode – it’ll know to listen for code!

Open your programming editor of your choice and write some code! You can either go with a block-based code editor or text-based code editor.

Software: MakeCode

To program the Chibi Chip, there are a two options available depending on your preference. Both require an internet connection to upload code to the microcontroller.

Block-Based Code w/ Microsoft MakeCode Online Editor

If you’re new to code, try Chibitronic's Scratch-inspired block-based code editor in Microsoft MakeCode!

Program Chibi Chip w/ MakeCode

To start coding in the editor, head over to https://makecode.chibitronics.com/.

Chibi Chip's MakeCode Online Editor

Upload Your Block-Based Code

Once you head over to MakeCode, click on the "+ New Project". You can also follow along by clicking on "Get Started! > Start Tutorial" to guide you this tutorial.

Chibi Chip MakeCode

Then drag and drop the forever and pause code blocks in the Control category.

Loops

Then drag and drop two set D0 to ON blocks of the Lights category. Change one of the blocks to OFF.

Output

Link the blocks together to blink the LED like so.

Blink Example Block Code

Check to see that the PROG light on your board is red. If it isn’t, press the PROG button until the light stays red.

Press PROG Button

Then press the Upload button at the bottom of the page.

Upload

Now you should see this sound animation appear on the screen. When the sound animation stops, the code is finished uploading. Congrats! You’ve uploaded your code!

Upload Graphic

Now your board should have a blinking light.

Uploaded Code

Now that you have your first program uploaded. Try playing with the code and creating your own light and blink patterns!

Software: ChibiScript (Arduino)

If you would like to start with text-based coding, try using ChibiScript, an Arduino-based beginner-friendly coding language. You can code directly in Arduino programming language with this text-based editor!

Program Chibi Chip w/ ChibiScript the Arduino Online Code Editor

To start coding, head over to https://ltc.chibitronics.com/.

ChibiScript Arduino Online Editor

Upload Your Text-Based Code

After heading to ChibiScript, click on Examples > 1. Basics > Blink to open up the blink example code. It should look similar to the image below.

Arduino Blink Example

Once the blink example is open, you should see an example of how to blink the LED connected to pin 0 similar to the image below. Let's change the pin by replacing "0" to "1".

Blink Example Code

Check to see that the PROG light on your board is red. If it isn’t, press the PROG button until the light stays red.

PROG Button

Finally, click the Upload button to play the code to your Chibi Chip!

Upload

You will see a sound animation appear on the bottom of the screen.

Sound Graphic

That means the code is being uploaded! When the code is done uploading, the red PROG light on your board will turn back to green to let you know that programming is done successfully. Now you should see your LED blink on the defined pin. Congrats! You’ve uploaded your code. Your Chibi Chip should now have a light blinking!

Blinking LED

Now that you have your first program uploaded. Try playing with the code and creating your own light and blink patterns!

Love to Code (LtC)

STEM Reimagined: Craft Meets Code

Check out Jie Qi's Love to Code Volume 1 for the MakeCode block-based and ChibiScript/Arduino text-based editor. You’ll learn to make LED lights shine and blink with loops and variables, craft paper switches and program them with conditional statements, and make complex light patterns with multithreaded programming. Finally, level up your coding skills with our debugging chapter, which shows you how to find and fix problems in projects.

Fern's Story from Chibitronics on Vimeo.

Love to Code Volume 1

Both adaptations are free for download! Click on the links below based on your programming preference and download to start coding with the Chibi Chip.

Love to Code Volume 1 for
MakeCode (PDF)
Love to Code Volume 1 for
ChibiScript and Arduino (PDF)

Walk-Through Demo Videos

Check out the Chibitroinics demo videos to help guide you through the chapters. The following videos were filmed for the Chibiscript and Arduino code. If you are following along with the Love to Code Volume 1 MakeCode Edition, the code will be similar but in block-based code.

Chapter 1: Light Up an LED

Walk-through of Chapter 1: Light up an LED from Chibitronics on Vimeo.

Chapter 2: Code to Blink!

Walk-through of Chapter 2: Code a Blink! from Chibitronics on Vimeo.

Chapter 3: Add a Switch

Walk-through of Chapter 3: Add a Switch! (part 1) from Chibitronics on Vimeo.

Walk-through of Chapter 3: Add a Switch! (part 2) from Chibitronics on Vimeo

Chapter 4: Fade In and Out!

Walk-through of Chapter 4: Fade in and out! from Chibitronics on Vimeo.

Troubleshooting

  • If the sound animation didn’t appear, try refreshing the page and uploading again.
  • Check that your volume is all the way up and unmuted. You can test this by unplugging the audio cable and see if you can hear the static (that’s your code!) when you press the upload button. If you hear the sound then plug the audio cable back in and try uploading again.
  • Remember to press the PROG button on your board before you click upload so that it’s in programming mode and the PROG light is red.
  • If you are having issues with your circuit or compiling code, check out the debugging tips or chapter listed in the:

Still having challenges? Send us a email at info@chibitronics.com.

Resources and Going Further

Thanks for trying out Chibitronics Love to Code boards. They would love your feedback to make the experience even better! Do you have ideas or comments for us? Please send them our way at info@chibitronics.com. Happy making!


Now that you've successfully got your Chibi Chip up and running, it's time to incorporate it into your own project! For more information related to paper circuits and the Chibi Chip, check out the resources below:

Need some inspiration for your next project? Try crafting your own paper circuit holiday greeting card from Chibitronics!

Craft a Holiday Greeting with Love to Code

March 23, 2018
Craft your own paper circuit holiday greeting using the LEDs, a Chibi Chip, Love to Code!

Or check out some of these related tutorials:

The Great Big Guide to Paper Circuits

Let's take a look at different materials we can use to combine paper crafting and electronics.

LED Robot Pop Up Card

Craft a paper circuit pop up card with a cycling RGB LED, battery, and copper tape.

Paper Circuit Pin

This quick craft project shows you how to create a circuit using copper tape instead of wire to light up an LED and make a wearable piece of e-craft art.

Red Hat Instrument Kit Hookup Guide

Get started with the Red Hat Instrument kit!