Artemis



The SparkFun Artemis Module is a Cortex-M4F with BLE 5.0 running up to 96MHz and with as low power as 6uA per MHz (less than 5mW). This is the world's first module to bridge the market between hobbyists and consumer products. We've packaged all the power of a modern microcontroller into a module that is both extremely easy to use but is mass-market ready. Measuring 10x15mm, this board has all the support circuitry you need to use the fantastic Apollo3 processor in your next project. We custom built the Arduino core from the ground up, making it fast and as light weight as possible. Additionally, the Artemis has an advanced HAL (hardware abstraction layer) allowing users to push the modern Cortex-M4F architecture to its limit. With 1M flash and 384k RAM you'll have plenty of room for your code. The Artemis module runs at 48MHz with a 96MHz turbo mode available and with Bluetooth to boot!

We recommend looking at our Designing with the SparkFun Artemis and Artemis Development with Arduino tutorials to get started, or check out tutorials tagged with Artemis to start working with hardware!

GeoFence Treasure Hunt With Artemis Global Tracker

July 31, 2024

Follow along with an engineering student as he creates a distance-based game using the Artemis Global Tracker!

Getting Started with Machinechat

October 7, 2022

Organize and display your data with SparkFun's Artemis OpenLog and MachineChat's JEDIOne!

Getting Started with the MyoWare® 2.0 Muscle Sensor Ecosystem

April 1, 2022

The MyoWare® 2.0 Muscle Sensor, an Arduino-compatible, all-in-one electromyography (EMG) sensor from Advancer Technologies. In this tutorial, we will go over the features and related shields to connect the sensor to a muscle group.

Artemis Global Tracker Hookup Guide

December 9, 2021

The SparkFun Artemis Global Tracker combines the Artemis processor with an Iridium 9603N satellite transceiver, ZOE-M8Q GNSS transceiver, and MS8607 PHT sensor. With a clear view of the sky, this board allows you to send and receive short data messages from anywhere in the world including remote locations far beyond the reach of WiFi and GSM networks. Follow this guide to get started with the Artemis Global Tracker.

SparkFun expLoRaBLE Hookup Guide

February 4, 2021

Check out our latest LoRaWAN development board with Bluetooth capabilities! With this guide, we'll get you passing data to The Things Network in no time.

MicroMod Artemis Processor Board Hookup Guide

October 21, 2020

Get started with the Artemis MicroMod Processor Board in this tutorial!

MicroMod All The Pins (ATP) Carrier Board

October 21, 2020

Access All The Pins (ATP) of the MicroMod Processor Board with the Carrier Board!

Getting Started with MicroMod

October 21, 2020

Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

MicroMod Machine Learning Carrier Board Hookup Guide

October 21, 2020

Get hacking with this tutorial on our Machine Learning Carrier Board!

Artemis Development with the Arduino IDE

September 10, 2020

This is an in-depth guide on developing in the Arduino IDE for the Artemis module and any Artemis microcontroller development board. Inside, users will find setup instructions and simple examples from blinking an LED and taking ADC measurements; to more complex features like BLE and I2C.

Getting Started with the Artemis Development Kit

September 10, 2020

This guide covers the general design of the board, the installation of the recommended software used to program the Artemis DK, and some basic examples. For more advanced functionalities, we have separate software development guides for the AmbiqSDK, Arm® Mbed™ OS, and the Arduino IDE platforms that users can reference.

Artemis Development on Arm® Mbed™ OS (Beta)

September 10, 2020

With the latest Artemis DK, board, we now offer full Bluetooth support within the Arduino IDE and development with Mbed™ OS. While we have worked tirelessly to get the Artemis module supported in the next Mbed™ OS release, the next release isn't slated until after the Artemis DK becomes available to the public. Therefore, this post will provide users with a jump start for developing with Mbed™ Studio, prior to the next release (in a beta of sorts), by utilizing our fork of Mbed™ OS.

Installing Board Definitions in the Arduino IDE

September 9, 2020

How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

OpenLog Artemis Hookup Guide

August 20, 2020

How to use and re-program the OpenLog Artemis, an open source datalogger. The OLA comes preprogrammed to automatically log data. The OLA can also record serial data, analog voltages, or readings from external Qwiic-enabled I2C devices. Some of these Qwiic-enabled devices include GPS/GNSS modules, pressure, altitude, humidity, temperature, air quality, environment, distance, and weight sensors.

RFID Beginners Tutorial

June 15, 2020

Make a remote work logger using an RFID reader and a GPS module. Scan a card and get ID, location, and time. All the perfect data to punch in and punch out from the middle of Nowhere!

Secure DIY Garage Door Opener

January 16, 2020

Did you know that most garage doors are at risk of a roll jam attack? Here we make a DIY garage door remote-control system that is much more secure than most commercial-ready products using the latest in ECC cryptography.

Cryptographic Co-Processor ATECC508A (Qwiic) Hookup Guide

October 17, 2019

Learn how to use some of the standard features of the SparkFun Cryptographic Co-processor.

SparkFun Edge Hookup Guide

September 26, 2019

Get to know your Edge board, including both the hardware features for you to utilize as well as how to get talking to it.

Hookup Guide for the SparkFun Artemis Thing Plus

September 19, 2019

Get started with our SparkFun Artemis Thing Plus - our popular Thing Plus footprint with the powerful Artemis module for ultimate functionality.

Hookup Guide for the SparkFun RedBoard Artemis ATP

August 28, 2019

Get started with the RedBoard Artemis ATP - all the functionality of the SparkFun Artemis module wrapped in the Mega Arduino Footprint

Hookup Guide for the SparkFun RedBoard Artemis

August 28, 2019

Get started with the RedBoard Artemis - all the functionality of the SparkFun Artemis module wrapped in the familiar Uno R3 footprint

Designing with the SparkFun Artemis

June 20, 2019

Let's chat about layout and design considerations when using the Artemis module.
Viewing 25 Artemis Tutorials. View All Tutorials.

Old Tutorials

Looking for the old, archived tutorials? Head on over to the archived tutorials on the main SparkFun site.
Please be aware that the tutorials you find there are no longer actively maintained.