Tutorials
IoT RedBoard ESP32 Development Board Hookup Guide
Delve into the functionality-rich world of the IoT RedBoard ESP32 Development Board!
ESP32 Thing Plus (USB-C) Hookup Guide
Meet the updated ESP32 Thing Plus (USB-C) development board. We have included some extra bells and whistles that users will appreciate, so check out out hookup guide for all the details!
MicroMod GNSS Function Board - NEO-M9N Hookup Guide
The u-blox NEO-M9N is a powerful GPS unit that now comes populated on a MicroMod Function Board! In this tutorial, we will quickly get you set up using it with the MicroMod ecosystem and Arduino so that you can start reading the output.
MicroMod GNSS Function Board - ZED-F9P Hookup Guide
Add millimeter precision location data to your MicroMod project with this guide for the SparkFun MicroMod GNSS Function Board - ZED-F9P.
Monitor Sensor Data from Anywhere
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.
Qwiic 9DoF - ISM330DHCX, MMC5983MA Hookup Guide
Find all your degrees of freedom with this little Qwiic breakout board combining the ISM330DHCX 6Dof and the MMC5983MA Magnetometer!
Qwiic Micro Magnetometer - MMC5983MA Hookup Guide
Let's figure out where we're going with the SparkFun Qwiic Micro Magnetometer - MMC5983MA!
Qwiic 6DoF - ISM330DHCX Hookup Guide
Get started with the Qwiic 6DoF ISM330DHCX Breakout Board!
Qwiic Pressure Sensor (BMP581) Hookup Guide
Get started with the SparkFun Pressure Sensor - BMP581 (Qwiic) following this Hookup Guide
The 970-HA-JOKES Payphone Project
A payphone turned into a bit of fun.
Qwiic Digital Desk Sign with MicroMod
Make a Qwiic-enabled digital desk sign with a MicroMod SAMD51 Processor Board's USB Host and a USB keyboard!
Thing Plus Dual-Port Logging Shield Hookup Guide
This tutorial shows you how to hook up and use the SparkFun Thing Plus Dual-Port Logging Shield.
LoRaSerial Hookup Guide
Simple serial over LoRa!
SparkFun RTK Facet L-Band Hookup Guide
Setup the RTK Facet L-Band in minutes to begin gathering millimeter level geospatial coordinates.
Qwiic Pressure Sensor (BMP384) Hookup Guide
Get started with the SparkFun Pressure Sensor - BMP384 (Qwiic) following this guide.
Level Shifter - 8 Channel (TXS0108E) Hookup Guide
Get started with the SparkFun Level Shifter - 8 Channel (TXS0108E) Breakout to shift between 5V, 3.3V and 1.8V logic level systems.
MicroMod Single Pair Ethernet Function Board - ADIN1110 Hookup Guide
With the SparkFun MicroMod Single Pair Ethernet Function Board - ADIN1110 you can prototype and create 10BASE-T1L Ethernet connections that work in noisy environments and over exceptionally long distances of over 1 kilometer! Follow this guide to get started with this Function Board.
MicroMod Alorium Sno M2 Processor Board Hookup Guide
Get started with the MicroMod Alorium Sno M2 Processor Board!
Qwiic dToF Imager (TMF882X) Hookup Guide
Getting started with the AMS dToF imagers (TMF8820 and TMF8820).
Getting Started with the MyoWare® 2.0 Muscle Sensor Ecosystem
The MyoWare® 2.0 Muscle Sensor, an Arduino-compatible, all-in-one electromyography (EMG) sensor from Advancer Technologies. In this tutorial, we will go over the features and related shields to connect the sensor to a muscle group.
Analog MEMS Microphone Breakout - SPH8878LR5H-1 Hookup Guide
Get started with sound monitoring using the SparkFun analog MEMS microphone breakout board with Arduino!
MicroMod Ethernet Function Board - W5500 Hookup Guide
Add Ethernet and PoE capabilities to your MicroMod project using the Ethernet Function Board - W5500.
MicroMod mikroBUS™ Carrier Board Hookup Guide
This carrier board takes advantage of the MicroMod, Qwiic, and the mikroBUS™ ecosystems and allows users to take advantage of the growing number of 7 MicroMod processor boards, 83 Qwiic (add-on) boards, and +1100 drop-in Click boards™, which equates to +51M different board combinations. Click to learn more.
Getting Started with Necto Studio
Necto Studio is a user friendly development environment for users looking to get started with MikroElektronika's MIKROE products.