Tutorials
Interactive 3D Printed LED Diamond Prop
In this tutorial, we will learn about how to create an interactive theatrical prop for a performance by 3D printing a translucent diamond prop using a non-addressable RGB LED strip and AT42QT1011 capacitive touch sensing.
TFMini - Micro LiDAR Module Hookup Guide
The TFMini is a ToF (Time of Flight) LiDAR sensor capable of measuring the distance to an object as close as 30 cm and as far as 12 meters! The TFMini allows you to integrate LiDAR into applications traditionally reserved for smaller sensors such as the SHARP GP-series infrared rangefinders.
How to Use a Hot Air Rework Station
Hot-air stations or heat guns are very useful tools and are essential for any electronics workbench. When working with or building printed circuit boards, there is a lot of room for errors to be made. Have no fear though, there are ways to remedy this with a hot air rework station!
Qwiic Accelerometer (MMA8452Q) Hookup Guide
Freescale’s MMA8452Q is a smart, low-power, three-axis, capacitive micro-machined accelerometer with 12-bits of resolution. It’s perfect for any project that needs to sense orientation or motion. We’ve taken that accelerometer and stuck it on a Qwiic-Enabled breakout board to make interfacing with the tiny, QFN package a bit easier.
Qwiic Distance Sensor (RFD77402) Hookup Guide
The RFD77402 uses an infrared VCSEL (Vertical Cavity Surface Emitting Laser) TOF (Time of Flight) module capable of millimeter precision distance readings up to 2 meters. It’s also part of SparkFun’s Qwiic system, so you won’t have to do any soldering to figure out how far away things are.
How to Work with Jumper Pads and PCB Traces
Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.
Using Artnet DMX and the ESP32 to Drive Pixels
In this tutorial, we'll find out how to use Resolume Arena, a popular video jockey software, to control custom-made ArtNet DMX fixtures.
Craft a Holiday Greeting with Love to Code
Craft your own paper circuit holiday greeting using the LEDs, a Chibi Chip, Love to Code!
Getting Started with Chibi Chip and Clip
This tutorial goes over the how to assemble the Chibitronics' Chibi Chip programmable microcontroller with the Chibi Clip to add more functionality to your paper circuits! Start programming your Chibi Chip by writing code (block-based and text-based) in a browser-based code editor and then transmit code through sound to your board!
Tech Prank: Hardware Mouse Jiggler
Create an innocuous-looking USB stick with an Arduino Pro Micro and a 3D printed case that moves your mouse pointer randomly every few seconds. Sure to anger your coworkers and friends!
Raspberry Pi Stand-Alone Programmer
This tutorial will show you how to use a headless Raspberry Pi to flash hex files onto AVR microcontrollers as a stand-alone programmer. It also tells the story about production programming challenges, how SparkFun came to this solution, and all the lessons learned along the way.
Raspberry Pi Zero Helmet Impact Force Monitor
How much impact can the human body handle? This tutorial will teach you how to build your very own impact force monitor using a helmet, Raspberry Pi Zero, and accelerometer!
Fingerprint Scanner (GT-521Fxx) Hookup Guide
This tutorial provides information about how to connect to ADH-Tech's fingerprint scanner (GT-521F32) and how to use it with Hawley's FPS_GT511C3 library for Arduino.
AST-CAN485 Hookup Guide
The AST CAN485 is a miniature Arduino in the compact form factor of the ProMini. In addition to all the usual features it has on-board CAN and RS485 ports enabling quick and easy interfacing to a multitude of industrial devices.
MIDI BLE Tutorial
Developing a bidirectional MIDI-BLE link with the nRF52832 Breakout.
Getting Started with Walabot
See through walls, track objects, monitor breathing patterns, and more using the power of radio frequency with the Walabot! In this tutorial, we will explore Walabot’s features using the Software Demo Kit (SDK) on Windows and the Application Programming Interface (API) on Linux-based distributions for embedded projects.
Prototype Wearable LED Dance Harness
A project tutorial to add an extra effect for dancers performing a choreographed piece. The harness can be added quickly under a costume.
FreeSoC2 Hookup Guide V14
The FreeSoC2 is an Arduino-compatible PSoC5LP-based development board, produced by SparkFun in collaboration with Jon Moeller (developer of the original FreeSoC) and Cypress Semiconductor.
Using the PSoC 6 Pioneer Board with the Pioneer IoT Add-on Shield
Cypress's PSoC 6 Pioneer Board is a development tool for the powerful PSoC 6 processor. In this tutorial, we'll show you how to use the PSoC 6 Pioneer Board along with the SparkFun/Digi-Key Pioneer IoT Add-on Shield to send data to a Raspberry Pi via BLE or WiFi.
DIY Heated Earmuffs
Embedded with heating pads and four Neopixel rings, these earmuffs do more than your average winter accessory to keep you warm while still looking good.
AT42QT101X Capacitive Touch Breakout Hookup Guide
Learn how to use the simple SparkFun AT42QT1010 and AT42QT1011 capacitive touch breakout boards.
LilyPad Temperature Sensor Hookup Guide
How to hook up the LilyPad Temperature Sensor as well as some project ideas and example code.
Qwiic Micro OLED Hookup Guide
Get started displaying things with the Qwiic Micro OLED.
Qwiic Human Presence Sensor (AK9753) Hookup Guide
How to get started with your Qwiic enabled AK9753 Human Presence Sensor.