Motion
SparkFun 9DoF IMU (ICM-20948) Breakout Hookup Guide
How to use the SparkFun 9DoF ICM-20948 breakout board for your motion sensing projects. This breakout is ideal for wearable sensors and IoT applications.
SparkFun ESP32 DMX to LED Shield
Learn how to utilize your DMX to LED Shield in a variety of different ways.
Qwiic Proximity Sensor (VCNL4040) Hookup Guide
The SparkFun Qwiic Proximity Sensor is a great, qualitative proximity (up to 20 cm) and light sensor. This hookup guide covers a few examples to retrieve basic sensor readings.
Motion Controlled Wearable LED Dance Harness
Control LEDs based on your movement using an accelerometer! Make your LEDs breathe by fading in and out when laying on the floor, turn off the LEDs when moving to your side, or make the LEDs blink in a headstand!
TFMini - Micro LiDAR Module (Qwiic) Hookup Guide
The TFMini is a ToF (Time of Flight) LiDAR sensor capable of measuring the distance to an object as close as 30 cm and as far as 12 meters! The TFMini allows you to easily integrate LiDAR into applications traditionally reserved for smaller sensors such as the SHARP GP-series infrared rangefinders. With the added Qwiic feature, you can quickly connect to the sensor via I2C!
Qwiic VR IMU (BNO080) Hookup Guide
Figure out how things are oriented with the robust 9 degrees of freedom (DOF) BNO080 IMU. Maybe even make your own virtual reality (VR) applications if you're feeling savvy.
TFMini - Micro LiDAR Module Hookup Guide
The TFMini is a ToF (Time of Flight) LiDAR sensor capable of measuring the distance to an object as close as 30 cm and as far as 12 meters! The TFMini allows you to integrate LiDAR into applications traditionally reserved for smaller sensors such as the SHARP GP-series infrared rangefinders.
Qwiic Accelerometer (MMA8452Q) Hookup Guide
Freescale’s MMA8452Q is a smart, low-power, three-axis, capacitive micro-machined accelerometer with 12-bits of resolution. It’s perfect for any project that needs to sense orientation or motion. We’ve taken that accelerometer and stuck it on a Qwiic-Enabled breakout board to make interfacing with the tiny, QFN package a bit easier.
Raspberry Pi Zero Helmet Impact Force Monitor
How much impact can the human body handle? This tutorial will teach you how to build your very own impact force monitor using a helmet, Raspberry Pi Zero, and accelerometer!
Getting Started with Walabot
See through walls, track objects, monitor breathing patterns, and more using the power of radio frequency with the Walabot! In this tutorial, we will explore Walabot’s features using the Software Demo Kit (SDK) on Windows and the Application Programming Interface (API) on Linux-based distributions for embedded projects.
Qwiic Human Presence Sensor (AK9753) Hookup Guide
How to get started with your Qwiic enabled AK9753 Human Presence Sensor.
H3LIS331DL Accelerometer Breakout Hookup Guide
Hookup guide and library usage details for the triple axis accelerometer H3LIS331DL high-g accelerometer.
ESP32 Thing Motion Shield Hookup Guide
Getting started with the ESP32 Thing Motion Shield to detect movements using the on-board LSM9DS1 IMU and adding a GPS receiver. Data can be easily logged by adding an microSD card to the slot.
SparkFun Inventor's Kit Experiment Guide - v4.0
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.0a.
Setting Up the Pi Zero Wireless Pan-Tilt Camera
This tutorial will show you how to assemble, program, and access the Raspberry Pi Zero as a headless wireless pan-tilt camera.
Pi Servo Hat Hookup Guide
This hookup guide will show you how to connect and use the Pi Servo Hat in a project.
SparkFun Inventor's Kit for micro:bit Experiment Guide
This guide contains all the information you will need to explore the twelve circuits of the SparkFun Inventors Kit for micro:bit.
Getting Started with MicroPython and the SparkFun Inventor's Kit for micro:bit
Learn MicroPython with the micro:bit.
ZX Distance and Gesture Sensor SMD Hookup Guide
How to connect and use the SparkFun ZX Distance and Gesture Sensor with an Arduino.
Spectacle Inertia Board Hookup Guide
Everything you need to know about using the Spectacle Inertia Board in one place.
Spectacle Motion Kit Hookup Guide
All the information you need to use the Spectacle Motion Kit in one place.
Spectacle Example: Super Mario Bros. Diorama
A study in building an animated diorama (with sound!) using Spectacle electronics.
Spectacle Motion Board Hookup Guide
All the information you need to use the Spectacle Motion Kit in one place.
OpenPIR Hookup Guide
How to use and customize the SparkFun OpenPIR motion sensor.