Blynk Board Project Guide

≡ Pages
Contributors: jimblom

Project 7: The LCD's Wealth of Information

The 16x2 Liquid-Crystal Display -- a 16-column, 2-row LCD, which can display any combination of up to 32 alphanumeric characters -- is one of the most commonly recurring components in electronic projects. It's simple to use, and it has they ability to convey a wealth of information pertaining to your project.

Alpha-numeric 16x2 LCD

Blynk's LCD widget is similarly useful in displaying diagnostic and other Blynk-project information. In this project, we'll use the LCD widget to display everything from the Blynk Board's temperature and humidity readings, to the length of time it's been up-and-running.

Blynk Setup

This project requires the LCD widget as well as three button widgets, which you can repurpose from the previous projects.

Connect an LCD Widget to V10

Add an LCD widget from the "Displays" section of the widget box, and tap it to bring up the settings page.

Before adjusting anything else, slide the Simple/Advanced slider to Advanced. Then set the pin to V10, and adjust the background and text color as you please (can't beat white text on black).

LCD Widget settings

Add Button Widgets to V11, V12, and V13

Set the three buttons up to trigger virtual pins 11, 12, and 13. Leave them in Push mode:

NamePin
T/HV11
InputsV12
RuntimeV13

Button settings

Blynk Run

Once the button's are set, you're ready to run. Until you hit one of the three buttons, the LCD may print a greeting message, but that will quickly fade once you trigger V11, 12 or 13.

Button running

Although it takes up a lot of room initially, you can see how valuable the LCD is -- and the wealth of information and text it can display. While the Value widgets are limited to four characters, the LCD can display up to 32!