SAMD51 Thing Plus Hookup Guide
Contributors:
santaimpersonator,
Englandsaurus
Resources and Going Further
Now that you've successfully got started with your SAMD51 Thing Plus, it's time to incorporate it into your own project! For more information, check out the resources below:
- Schematic (PDF)
- Eagle Files (ZIP)
- ATSAMD51 Datasheet (PDF)
- Graphical Datasheet (PDF)
- Qwiic Landing Page
- GitHub Hardware Repo
- Product Showcase
Need some inspiration for your next project? Check out some of these related tutorials:
SparkFun Tutorials
Installing an Arduino Library
How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.
What is an Arduino?
What is this 'Arduino' thing anyway? This tutorials dives into what an Arduino is and along with Arduino projects and widgets.
Installing Arduino IDE
A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.
Arduino Board Comparison Guides
Hookup Guides for Other SAMD Boards
Choosing an Arduino for Your Project
Examining the diverse world of Arduino boards and understanding the differences between them before choosing one for a project.
Standard Arduino Comparison Guide
Arduino Comparison Guide Uno or Pro Mini? Bluetooth or wireless? When it comes to Arduinos, there are a lot of choices. We've compiled every Arduino developmentā¦
SAMD21 Mini/Dev Breakout Hookup Guide
An introduction to the Atmel ATSAMD21G18 microprocessor and our Mini and Pro R3 breakout boards. Level up your Arduino-skills with the powerful ARM Cortex M0+ processor.
RedBoard Turbo Hookup Guide
An introduction to the RedBoard Turbo. Level up your Arduino-skills with the powerful SAMD21 ARM Cortex M0+ processor!
Click the buttons above for tutorials relating to the board functionality based on topic difficulty.
Beginner
Serial Communication
Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!
Analog to Digital Conversion
The world is analog. Use analog to digital conversion to help digital devices interpret the world.
Logic Levels
Learn the difference between 3.3V and 5V devices and logic levels.
Analog vs. Digital
This tutorial covers the concept of analog and digital signals, as they relate to electronics.
Data Types in Arduino
Learn about the common data types and what they signify in the Arduino programming environment.
How to Work with Jumper Pads and PCB Traces
Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.
Intermediate
Serial Peripheral Interface (SPI)
SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.
I2C
An introduction to I2C, one of the main embedded communications protocols in use today.
Processor Interrupts with Arduino
What is an interrupt? In a nutshell, there is a method by which a processor can execute its normal program while continuously monitoring for some kind of event, or interrupt. There are two types of interrupts: hardware and software interrupts. For the purposes of this tutorial, we will focus on hardware interrupts.
Adding More SERCOM Ports for SAMD Boards
How to setup extra SPI, UART, and I2C serial ports on a SAMD-based boards.
Advanced
Installing an Arduino Bootloader
This tutorial will teach you what a bootloader is and why you would need to install or reinstall it. We will also go over the process of burning a bootloader by flashing a hex file to an Arduino microcontroller.
Integrated Circuits
An introduction to integrated circuits (ICs). Electronics' ubiquitous black chips. Includes a focus on the variety of IC packages.
Reading and Writing Serial EEPROMs
EEPROM is a great way to add extra memory to your microcontroller project. Wait 'til you see how easy it is to use!
Looking for project ideas? Check out some of these Qwiic products and tutorials:
SparkFun Qwiic Shield for Teensy Hookup Guide
A short guide for assembling and using the SparkFun Qwiic Shield for Teensy and Qwiic Shield for Teensy Extended.
Qwiic PIR Hookup Guide
Get started passively monitoring motion using the Panasonic EKMC and EKMB sensors with the SparkFun Qwiic PIR.
MicroMod Asset Tracker Carrier Board Hookup Guide
Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.
Fading with the MOSFET Power Switch and Buck Regulator
In this tutorial, we will slowly turn on the load and then slowly turn it off using the N-channel MOSFET.
Or check out this blog post for ideas: