Artemis Development with the Arduino IDE

≡ Pages
Contributors: santaimpersonator, Liquid Soulder, Member #1571936

Resources and Going Further

Need some inspiration for your next project? Check out some of these related tutorials:

SparkFun Tutorials

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

What is an Arduino?

What is this 'Arduino' thing anyway? This tutorials dives into what an Arduino is and along with Arduino projects and widgets.

Installing Arduino IDE

A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

Installing Board Definitions in the Arduino IDE

How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

Arduino Tutorials

Arduino Board Comparison Guides

Choosing an Arduino for Your Project

Examining the diverse world of Arduino boards and understanding the differences between them before choosing one for a project.

Standard Arduino Comparison Guide

Arduino Comparison Guide Uno or Pro Mini? Bluetooth or wireless? When it comes to Arduinos, there are a lot of choices. We've compiled every Arduino development…

RedBoard vs. Uno

In this tutorial we discuss the differences and similarities between the RedBoard and the Arduino Uno (SMD and PTH). The development platforms
Beginner

Click the buttons above for tutorials relating to the board functionality based on topic difficulty.

Beginner

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

Analog to Digital Conversion

The world is analog. Use analog to digital conversion to help digital devices interpret the world.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

Analog vs. Digital

This tutorial covers the concept of analog and digital signals, as they relate to electronics.

Data Types in Arduino

Learn about the common data types and what they signify in the Arduino programming environment.

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

Artemis Development with Arduino

Get our powerful Artemis based boards (Artemis Nano, BlackBoard Artemis, and BlackBoard Artemis ATP) blinking in less than 5 minutes using the SparkFun Artemis Arduino Core!

Intermediate

Serial Peripheral Interface (SPI)

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Processor Interrupts with Arduino

What is an interrupt? In a nutshell, there is a method by which a processor can execute its normal program while continuously monitoring for some kind of event, or interrupt. There are two types of interrupts: hardware and software interrupts. For the purposes of this tutorial, we will focus on hardware interrupts.

Advanced

Integrated Circuits

An introduction to integrated circuits (ICs). Electronics' ubiquitous black chips. Includes a focus on the variety of IC packages.

Bluetooth Basics

An overview of the Bluetooth wireless technology.

Reading and Writing Serial EEPROMs

EEPROM is a great way to add extra memory to your microcontroller project. Wait 'til you see how easy it is to use!

ARM Programming

How to program SAMD21 or SAMD51 boards (or other ARM processors).

Designing with the SparkFun Artemis

Let's chat about layout and design considerations when using the Artemis module.

Software Development Guides

Using SparkFun Edge Board with Ambiq Apollo3 SDK

We will demonstrate how to get started with your SparkFun Edge Board by setting up the toolchain on your computer, examining an example program, and using the serial uploader tool to flash the chip.

Artemis Development with Arduino

Get our powerful Artemis based boards (Artemis Nano, BlackBoard Artemis, and BlackBoard Artemis ATP) blinking in less than 5 minutes using the SparkFun Artemis Arduino Core!

Artemis Development on Arm® Mbed™ OS (Beta)

With the latest Artemis DK, board, we now offer full Bluetooth support within the Arduino IDE and development with Mbed™ OS. While we have worked tirelessly to get the Artemis module supported in the next Mbed™ OS release, the next release isn't slated until after the Artemis DK becomes available to the public. Therefore, this post will provide users with a jump start for developing with Mbed™ Studio, prior to the next release (in a beta of sorts), by utilizing our fork of Mbed™ OS.

Example Projects

Programming the SparkFun Edge with Arduino

Running low-power machine learning examples on the SparkFun Edge can now be done using the familiar Arduino IDE. In this follow-up to the initial Edge tutorial, we'll look at how to get three examples up and running without the need to learn an entirely new SDK.