STK-node

≡ Pages
Contributors: D___Run___

Software Installation and Setup

Node.js

Node.js is a JavaScript runtime, that is, it's software that can execute your JavaScript code. Node.js has special features that support some of the best potentials of the JavaScript programming language, like event-driven, non-blocking I/O. npm is Node's package manager. It's a giant repository of encapsulated bits of reusable useful code, called modules, that you can use in your programs. npm will get installed for you when you install Node.js.

alt text

Installing Node.js is a straightforward download-and-double-click process. Head on over to the Node.js website. Heads up: You'll want to select the "LTS" version for download (LTS stands for long-term support). At time of writing, LTS is v4.4.5:

alt text

Text Editor (Atom)

You will need a text editor in which to edit and save your JavaScript files. This means a plain text editor, not a Word document. If you've already got one, like SublimeText, Notepad++, vim, etc., groovy. If not, go ahead and install Atom.

atom text editor logo

You can use any text editor you like if you already have on installed and are up and running. But, if you have never used a text editor to write JavaScript, HTML, etc. we recommend using Atom. Atom is a free and open source text editor that works on all three major operating systems, is light weight and when you get comfortable...it's hackable!

Download Atom by heading to the Atom website.

alt text

FTDI Drivers

To use the RedBoard or Arduino with Node.js and Johnny-Five you will need FTDI Drivers installed on your computer. We have a tutorial to help walk you through that process. Don't worry we will wait for you to come back before moving on.

How to Install FTDI Drivers

June 4, 2013
How to install drivers for the FTDI Basic on Windows, Mac OS X, and Linux.

Flashing Firmata

To use Johnny-Five with an Arduino we need to install the Firmata firmware on the board. Firmata is a firmware for microcontrollers that turns the microcontroller into a slave of sorts. It sets it up so that is listening for commands from another device or computer. In essence it allows us to control the Arduino without uploading code and just running it on our computer.

There are two ways to install firmata on your redBoard. These are dependent on whether you have the Arduino IDE installed on your computer or not.

Installing Firmata through Arduino

If you already have Arduino installed you can install Firmata from the examples that come with Arduino. To do this, open your Arduino IDE and plug your board into your computer using a USB cable.

USB hooked up

Then in the Arduino IDE at the Tools drop down menu set the board type by selecting the following Tools > Board > Uno.

alt text

Now, from the Tools menu select your Serial port by selecting the following Tools > Port > COM## The COM## will probably be somewhere in the 3 to 5 range.

Note: Mac users your port list will look different. You are looking for "/dev.cu.usbserial-XXXXX" rather than "COM##"

alt text

Now, to open Firmata from the examples folder! Select the following File > Examples > Firmata > standardFirmataPlus

alt text

Now click the upload (Arrow button at the top left) to upload Firmata. With that you are done installing Firmata from the Arduino IDE. You can now close Arduino.

Installing Firmata through Interchange

If you have never used Arduino and/or installed the Arduino IDE, there is no point in installing it for a single time use. There is a command line tool that you can use to install Firmata without the fuss of installing Arduino only to use it once and then never use it again (that is if you stick with Node.js)

The command line tool we are talking about is called Interchange and it is designed specifically for this reason.

Installing interchange through npm

To install interchange type the following into your console.

npm install nodebots-interchange -g

Note: Mac users, you will need to add `sudo` before the command line entry to install anything globally (`-g`) and then enter your password.

Interchange will install with an output that will look somewhat scary to a newcomer of Node.js. It will look like this.

alt text

Flashing the RedBoard with Interchange

Now, to install Firmata onto your redboard, plug the board into your computer using a USB cable then type the following command to launch the Interchange tool.

interchange install --interactive

The --interactive flag allows you to use the user interface to select your board and firmware options.

Select your firmware that you would like to install. We want to install Standard Firmata. Select it using your arrow keys.

language:console
 ? Choose a firmware 
  node-pixel 
  hc-sr04 
❯ StandardFirmata 

Next select your board. The RedBoard is the same as the Arduino Uno. So, select 'Uno' from the list.

language:console
? Choose a firmware StandardFirmata
? Choose a board 
❯ uno 
  nano 
  pro-mini 

Finally, select your port, it should be "COM##" on windows or "/dev/tty/cu.usbserial-XXXX..." on mac.

language:console
? Choose a firmware StandardFirmata
? Choose a board uno
? Choose a port 
  /dev/cu.Bluetooth-Incoming-Port 
  /dev/cu.Sphero-OOG-AMP-SPP 
❯ /dev/cu.usbserial-AI02KHSB 

With that Interchange will install firmata for you. You should see the terminal out information similar to this...

language:console
? Choose a firmware StandardFirmata
? Choose a board uno
? Choose a port /dev/cu.usbserial-AI02KHSB
 Retrieving manifest data from GitHub
 Downloading hex file
 connected
 reset complete.
 flashing, please wait...
 flash complete.

Now your RedBoard is ready to be programmed using Johnny-Five and Node.js

Project Directory Setup

When you want to build a Johnny-Five project you want to build a directory for the project. Why? you may ask. Because like any other Javascript project it can scale up to be pretty large using a number of modules and files beyond the basic single file you end up creating in Arduino.

For Example when you install a node module a node_modules directory is created. We want to keep each node_modules directory seperate from your other projects.

Node Projects Directory

From the command line you should navigate to where you would like to store all of your node.js projects. For example I store all of my projects in a directory in my documents folder. Let's do that.

From the command line change directory (cd)to your documents directory. As an example I typed the following.

cd documents

Now create a new directory to store all of your node projects by typing the following.

mkdir node_projects

Once you have created your directory you can now cd into it by typing

cd node_projects

SIK Project Directory

now that you are in your projects folder you will want be creating a project directory for each experiment. You will do this at the beginning of each experiment so that each one will be a standalone project. We highly recommend that you group them all together in one directory. I created one called sik and then navigated into it by typing the following commands.

mkdir sik
cd sik