SparkFun Inventor's Kit for micro:bit Experiment Guide

≡ Pages
Contributors: D___Run___, bboyho

Introduction to Microsoft MakeCode

What is MakeCode?

MakeCode is an open programming environment built by Microsoft for the micro:bit, as well as other boards. You can navigate to MakeCode for the micro:bit by clicking on the button below.

Once you have launched MakeCode, you will be greeted by its basic layout with a simulator on the left and a block-based environment on the right, as shown here.

MakeCode for micro:bit

Click on the image above for a larger view.

Let's take a quick tour and check out what is available to us!

  1. Projects --- A cloud storage system connected to your computer with no account setup required.
  2. Share --- Allows you to share your project code in a number of different ways with your friends!
  3. Blocks/JavaScript/Python --- Choose your own adventure by programming in blocks (default) or in JavaScript. Not shown in the image, Microsoft also eventually added an additional option to use convert the code to MicroPython.
  4. Program Space --- This is where the magic happens and where you build your program...where you "make code."
  5. Zoom/Undo-Redo --- Sometimes you need to undo things, or zoom out and look around; these are the buttons for that.
  6. Name & Save --- Name your program and save it (download it) to your computer.
  7. Download --- Similar to Save, download your program as a .hex file and drag it into your micro:bit.
  8. Block Library --- All of the options in terms of program building blocks, which are color-coded by function.
  9. Simulator Hide/Show --- You can hide/show the simulator if you would like.
  10. Simulator --- You don't need hardware! MakeCode has a real-time simulator! As you change your program, you can see what it will do on this virtual micro:bit!

Phew! Now you have a choice: block- or text-based programming?

Blocks or Text

For this guide and the majority of the content that you will find on SparkFun for the micro:bit, we will be using block-based programming examples.

[Block Mode(https://cdn.sparkfun.com/assets/learn_tutorials/6/3/9/Screen_Shot_2017-03-02_at_4.03.08_PM.png)

But, if you so choose, there is a JavaScript (and also MicroPython) option to use as well. The choice is yours, and the good news is that you can switch back and forth from one to the other in the same program; one will populate the other, which is really nice if you are new to programming!

Simulator

MakeCode includes a simulator for the micro:bit, meaning if you don't have your micro:bit in hand you can still write code for it. Or if you want to try out an idea before you upload it to your micro:bit, you can do that too!

simulator

The simulator will update as you build your code, and if you want to run it from the beginning you can click the stop and run buttons to start it over again!

Speaking of code, let's write a quick program and get it onto your micro:bit!