SparkFun Inventor's Kit for micro:bit Experiment Guide

≡ Pages
Contributors: D___Run___, bboyho

Experiment 6: Reading a Button Press

Introduction

Up until now, we’ve focused mostly on outputs. Now we’re going to go to the other end of the spectrum and play around with inputs. In Experiment 2, we used an analog input to read the potentiometer. In this experiment, we’ll be reading one of the most common and simple inputs – a push button – by using a digital input. We will use it to cycle through different colors on the RGB.

Parts Needed

You will need the following parts:

  • 1x micro:bit
  • 1x Micro B USB Cable
  • 1x micro:bit Breakout (with Headers)
  • 1x Breadboard
  • 8x Jumper Wires
  • 1x Momentary Push Button
  • 1x 10kΩ Resistor
  • 1x Common Cathode RGB LED
  • 3x 100Ω Resistors

Didn't Get the SIK for micro:bit?

If you are conducting this experiment and didn't get the Inventor's Kit, we suggest using these parts:

Breadboard - Full-Size (Bare)

PRT-12615
$7.75

micro:bit v2 Board

DEV-17287
$16.50

Multicolor Buttons - 4-pack

PRT-14460
$1.95

LED - RGB Diffused Common Cathode

COM-09264
$2.30

SparkFun Qwiic micro:bit Breakout (with Headers)

BOB-16446
$6.25

Jumper Wires Standard 7" M/M - 30 AWG (30 Pack)

PRT-11026
$3.50

USB Micro-B Cable - 6 Foot

CAB-10215
$6.50

Resistor 10K Ohm 1/4 Watt PTH - 20 pack (Thick Leads)

PRT-14491
$1.50

Resistor 100 Ohm 1/4 Watt PTH - 20 pack (Thick Leads)

PRT-14493
$1.50

Suggested Reading

Before continuing with this experiment, we recommend you be somewhat familiar with the concepts in these tutorials:

Button and Switch Basics

May 7, 2013
A tutorial on electronics' most overlooked and underappreciated component: the switch! Here we explain the difference between momentary and maintained switches and what all those acronyms (NO, NC, SPDT, SPST, ...) stand for.

Analog vs. Digital

July 18, 2013
This tutorial covers the concept of analog and digital signals, as they relate to electronics.

Introducing the Push Button

A momentary push button closes or completes the circuit only while it is being pressed. The button has four pins, which are broken out into two sets of two pins. When you press down on the button and get a nice "click," the button bridges the two sets of pins and allows current to flow through the circuit.

Momentary Push Button

How do you know which pins are paired up? The buttons included in this kit will only fit across the breadboard ditch in one direction. Once you get the button pressed firmly into the breadboard (across the ditch), the pins are horizontally paired. The pins toward the top of the breadboard are connected, and the pins toward the button of the breadboard are connected.

Note: Not all buttons share this pin format. Please refer to the datasheet of your specific button to determine which pins are paired up.

Hardware Hookup

Ready to start hooking everything up? Check out the wiring diagram and hookup table below to see how everything is connected.

Polarized Components Pay special attention to the component’s markings indicating how to place it on the breadboard. Polarized components can only be connected to a circuit in one direction.

Wiring Diagram for the Experiment

Fritzing Diagram: micro:bit SIK Exp  6

Having a hard time seeing the circuit? Click on the wiring diagram for a closer look.

Note: The full sized breadboard power rails have a break down the middle. If you end up using the lower half of the power rail you will need to jump between the upper end and lower end.

Run Your Script

Either copy and paste, or re-create the following code into your own MakeCode editor by clicking the open icon in the upper right-hand corner of the editor window. You can also just download this example by clicking the download button in the lower right-hand corner of the code window.

Note: You may need to disable your ad/pop-up blocker to interact with the MakeCode programming environment and simulated circuit!

Code to Note

Let's take a look at the code blocks in this experiment.

Code to Note: Exp 6

If you are having a hard time viewing this code, click on the image above to get a better look!

Set Pull Pin

When you start your micro:bit, some pins can be set to be naturally on or naturally off. The set pull pin block allows you to set an initial state of a pin by selecting a pin and then its pull state, which is UP, DOWN or NONE.

Set Pin to Emit Event

Just like the button event in Experiment 4 there are events that you can read. But first, you have to set a pin to emit an event. You use the set pin to emit event block to create a type of event for a specific pin to emit or send out when it reaches that state. As an example, we set P16 to emit an EDGE event, which means that it changed from HIGH to LOW or LOW to HIGH.

On Event

Under the Advanced blocks you can find the Control blocks. These are the blocks that are the most complicated to use, but are the most powerful. The On Event block accepts an event type to watch for and a pin that event should happen on. When that specific event is emitted from that pin, it will trigger whatever code is inside of it. Take a moment to look through the list of different events that you can listen for!

if / Else if / Else

Finally, inside of the forever block is a more complex if block, which is an if / if else / else tree. To build this more complex "if" statement, add a standard if / else block into your program. Then click on this small gear in the upper left-hand corner of the block. This will open a tiny interface with more blocks in it. You can drag more else if blocks into the structure here to build your decision tree. Here is what ours looks like:

if else block

Once you are done rearranging your "if" statement you can close this menu by clicking on the gear again.

What You Should See

When you press the button, the RGB will turn on to a color. When you press it again, the color will change and another press will change the color once again. Press it one more time, and it will turn off. Every time you press the button, it increments a variable, and then we check against it to set the color. If the variable goes over the value of 2, we reset it to 0, which is off.

Exp 6 Final Assembly

While the image shows a black momentary pushbutton, you can use any colored button as long as it is momentary pushbutton to cycle through the colors!

Troubleshooting

Light Not Turning On

The push button is square, and because of this it is easy to put it in the wrong way. Give it a 90-degree twist and see if it starts working.

Underwhelmed

No worries; these circuits are all super stripped-down to make playing with the components easy, but once you throw them together the sky is the limit.