Pi Servo pHAT (v2) Hookup Guide

≡ Pages
Contributors: QCPete, santaimpersonator

Resources and Going Further

For more information, check out the resources below:

Need help getting started with your Raspberry Pi? Check out these resources here:

Need help getting started with Python and I2C? Check out these resources here:

Need some inspiration for your next project? Check out the tutorials below:

Raspberry Pi Tutorials

Headless Raspberry Pi Setup

Configure a Raspberry Pi without a keyboard, mouse, or monitor.

How to Use Remote Desktop on the Raspberry Pi with VNC

Use RealVNC to connect to your Raspberry Pi to control the graphical desktop remotely across the network.

Graph Sensor Data with Python and Matplotlib

Use matplotlib to create a real-time plot of temperature data collected from a TMP102 sensor connected to a Raspberry Pi.

How to Run a Raspberry Pi Program on Startup

In this tutorial, we look at various methods for running a script or program automatically whenever your Raspberry Pi (or other Linux computer) boots up.

Robotics Tutorials

Hackers In Residence - The Tethered Quad

Our first-ever "Hackers in Residence" Tara Tiger Brown and Sean Bonner created a quadcopter that stays tethered to the ground. Here's how they did it!

Ardumoto Kit Hookup Guide

Learn how to assemble and drive DC motors using the v2.0 Ardumoto Shield.

Assembly Guide for SparkFun JetBot AI Kit V2.0

Assembly Guide for the SparkFun JetBot AI Kit v2.0. This tutorial includes photos & comments to assemble the two-layer chassis & additional components unique to the JetBot kit.

Red Hat Co.Lab Robotic hand kit curriculum guide

Hookup guide for Red Hat Robotic Hand kit

Servo and Motor Control Tutorials

Blynk Board Project Guide

A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.

micro:bit Educator Lab Pack Experiment Guide

A quickstart guide for the micro:bit educator lab pack.

ESP32 Thing Power Control Shield Hookup Guide

This tutorial shows you how to get started with the ESP32 Thing Power Control Shield.

Tinker Kit Circuit Guide

This guide takes you through the basics of building 11 different circuits with the SparkFun Tinker Kit and how to program them using the Arduino IDE.

Python Logo