LED Cloud-Connected Cloud

≡ Pages
Contributors: Sarah Al-Mutlaq

Introduction

Make a rainbow LED colored cloud light that you can control from your phone. You can even have it change color based on the weather outside.

Rainbow colored LED Clouds

These are the clouds from episode 3 The Fellowship of the Things, which you can watch below if you haven't already.

Required Materials:

To follow along with this tutorial, you'll need the following materials.

Cloud Cloud required electronics materials

You Will Also Need

Other Cloud Cloud materials

  • long hook-up wire for cloud power (I used stereo wire)
  • Paper lanterns (white)
  • Pillow filling (I used polyfil)
  • Lots of hot glue and a hot glue gun
  • Fishing wire
  • A wooden dowel for support
  • A power source; you will need something that can put out at least 5V and 4A, but for the best results you can get a pricier 6V 8A power source.

alt text

Optional part included: Thing dev board (in the wishlist, but only needed if you want to hook up to your phone and/or weather info)

Suggested Reading:

If any of these subjects sound unfamiliar, considering reading the following tutorials before continuing on.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

Installing Arduino IDE

A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

Using the Arduino Pro Mini 3.3V

This tutorial is your guide to all things Arduino Pro Mini. It explains what it is, what it's not, and how to get started using it.

WS2812 Breakout Hookup Guide

How to create a pixel string with the WS2812 and WS2812B addressable LEDs!

ESP8266 Thing Development Board Hookup Guide

An overview of SparkFun's ESP8266 Thing Development Board - a development board for the Internet of Things.