Advanced Autonomous Kit for Sphero RVR Assembly Guide

≡ Pages
Contributors: Pearce, Ell C

Plugging the System into the RVR

In the final step we'll then connect the 4 pin Ribbon Cable from the four pin connector on the Servo pHAT to the UART Connector on the RVR.

To keep the UART cable from obscuring the view for the pan-tilt camera, I run it under the mounting plate. Refer to the images below - feel free to click on an image to see it more closely!


Cable outside the mounting plate Cable run under the mounting plate

Congratulations! You've completed the kit and are ready to start coding!