Advanced Autonomous Kit for Sphero RVR Assembly Guide

≡ Pages
Contributors: Pearce, Ell C

Introduction

The SparkFun Advanced Autonomous Kit for Sphero RVR provides all the functionality of the basic kit with the addition of time-of-flight distance sensing in the front and rear. Based around Raspberry Pi’s small yet powerful Zero W model, the kit provides distance sensing, global positioning, and vision to the Sphero RVR. In this tutorial we'll cover assembly of the kit's hardware. Most of the steps are fairly straight forward and just require a little bit of patience.

SparkFun Advanced Autonomous Kit for Sphero RVR

KIT-15303
Retired

Required Materials

To follow along with this tutorial, you will really only need a phillips-head screwdriver. We have quite a few to choose from - but our Pocket Screwdriver Set is a great option.

Tool Kit - Screwdriver and Bit Set

TOL-10865
$14.95

Pocket Screwdriver Set

TOL-12891
$5.50

iFixit Essential Electronics Toolkit

TOL-15256
Retired

Electric Hobby Screwdriver Set

TOL-15548
Retired

Before We Begin

If you haven't already, start charging the RVR battery. It takes a while to charge, so now would be a good time to get it going.

Pan Tilt Mechanism

Note: Before assembling the pan-tilt mechanism, it is recommended that users follow the instructions for the servo pre-alignment in the getting started guide to avoid issues later.

You will need to build up the Pan-Tilt mechanism. We have instructions over in the Pan-Tilt Mechanism Section of our basic guide - head on over there now as you'll need to have this assembled in order to move forward with this tutorial!

Basic Autonomous Kit for Sphero RVR Assembly Guide

December 12, 2019
Get your Basic Autonomous Kit for Sphero RVR all hooked up with this guide!
Assembling the Pan-Tilt Mechanism Hookup Instructions

GPS Module and Mux

The GPS board and Mux board are the only two boards that will mount directly to the cover plate. It’s best to put these boards on first as the additional mounting plate obscures part of the board. We'll do this using two of the 1/4 inch screws and 2 nuts for each board.

Parts, Boards, and RVR Cover Plate

The antenna (the beige part on the board) will need to be unobstructed and pointed towards the sky, so we'll mount it off to the side and near the front of the cover plate on the inner set of slide holes. The Qwiic cable that runs from the Servo pHAT to the GPS will use the outer set of holes later. If you have the means, putting the GPS board up higher always helps, but be sure not to obscure the pan-tilt camera rig.

GPS Board mounted on RVR Cover Plate

The Mux board will mount to the two screw holes in the middle of the RVR Cover Plate. it's important that the "Main" Connector is facing away from the labeled connector port on the RVR Cover Plate (see photo below).

Mux board mounted on the RVR Cover Plate along with the GPS board

Once the Mux board is in place, we'll plug in the 50mm Qwiic cables (these might be 2x 100mm cables and 1 50mm cable in your kit) into the Mux board. We'll want one cable running from rear-facing Qwiic connector on the GPS board to the "Main" Qwiic connector on the Mux board. Then we'll plug one cable into connector 3 and a separate one into connector 4 on the Mux board (where you'll use the 2 100mm cables if you have them). We'll plug these into the Time of Flight sensors later in the tutorial. It's important to use connectors 3 and 4 (3 for the front facing Time of Flight sensor and 4 for the rear) as this corresponds to code in the example. If you want to change which connectors you're using, you'll have to change some parts of the code.

50mm Qwiic cables plugged into the Mux board

Raspberry Pi Zero

For the advanced kit, all four mounting points on the Pi Zero W will be used. Due to the through hole pins soldered to the Pi Zero W, you need to add a set of nuts between the board and the mounting plate. For this we'll use (4) 1/2 inch screws and (8) 4-40 nuts.

Raspberry Pi Zero with Screws and 4-40 Nuts

When complete, the Raspberry Pi Zero should look like this:

Raspberry Pi Zero with 4-40 Standoff Nuts

Do not mount the Raspberry Pi Zero yet, that will come at a later step.

Mounting Plate and Time of Flight Sensor Brackets

If you have not already, peel the protective layer off of the front and back of the acrylic plate.

peeling the protective layer off the plate

The metal standoffs attach to the mounting plate with the 4-40 nuts. The threaded end of the standoffs will be facing up. Take extra care in tightening the nuts as you can crack the plate if you over-tighten them.

The time of flight sensors will need to be facing forward and backwards unobstructed. 4 right-angle mounting brackets have been included so the sensors can be mounted in the proper position on the mounting plate. The sensors can be added later, but it’s best to get these on the board before the pan-tilt rig is mounted. They're fastened to the mounting plate with a 1/4" screws and a 4-40 nut (for each bracket).

Standoffs and Brackets affixed to mounting plate

Note that the right-angle brackets have one threaded and one un-threaded hole. The threaded holes are smaller than the un-threaded holes, and if you look closely, you'll see the threads in the smaller holes.

Right-angle brackets

It’s important that the threaded holes are perpendicular to the plate, those will be the holes the screws that hold the sensor board in place use.

Mounting the Servo Horn

While the pan-tilt will be facing up, the servo horn (which the servo will be affixed to) is mounted on the bottom of the plate.

Line up the small holes on the plate with the small holes in the servo horn the same. Use the small, self-tapping screws to mount it in place from the top of the mounting plate.

Fastening servo horn to the mounting plate

Two of the small self-tapping screws will suffice, but if desired you can use all four.

Adding the Pan/Tilt Camera and Raspberry Pi Zero

Once the horn is mounted in place, you can use the larger self-tapping screws to mount the pan-tilt rig. It’s important that the rig is mounted so that the middle of the servo travel faces forward. This will take some trial and error, but you want the servo to be able to move an equal amount in either direction when facing directly forward (it’s okay to move the servo when it isn’t powered, just don’t force it).

Pan-tilt mechanism mounted to mounting plate

Add the Pi Zero W (with the spacer nuts installed) to the mounting plate with another 4 of the 4-40 nuts. For the best access to all the connectors on the Pi Zero, make sure the USB and HDMI Connectors are facing the back of the plate and the pins are facing the pan-tilt rig.

Raspberry Pi Zero mounted to mouting plate

Attaching the Raspberry Pi Zero Camera Cable

You'll need to mount the Raspberry Pi Camera to the pan-tilt mechanism using the included square of double sided tape. However, I recommend you plug in the camera to the ribbon cable before securing the camera to the tape square.

To connect the ribbon cable, you'll need to carefully slide the flexible ribbon cable connector's locking tab out. The locking tab slides out parallel to the board so you'll need to push each side of the tab with your fingernails. The image below highlights where you would need to place your fingernails to slide the tab out.

Highlighted camera connector tabs

Once the locking tab is out, you can insert the camera connector into the slot. Face the camera's exposed contacts toward the PCB in order to make a connection with the connector's pins. Then insert the cable until it is firmly into the connector. Care must be taken to ensure that the ribbon cable does not have any sharp bends when installing the camera.

Inserting the camera connector ribbon into the camera connector slot

When ready, carefully slide the tab back into the locking position using your fingernails.

Gently push the locking mechanism back into place

Now you can mount the Raspberry Pi Camera to the pan-tilt mechanism. Make sure the correct side is facing up. Once mounted, it should look something like what we see here:

mounting camera to RVR pan tilt mechanism

You'll also need to connect the camera ribbon cable to the Pi Zero W. The locking mechanism for the cable is exactly the same as you saw above. Make sure the pads point upward as you see here:

Raspberry Pi Zero camera cable plugged into camera and pi

Connecting the Servo pHAT and Servos

The Servo pHAT is the interface for both the pan-tilt rig and the Qwiic sensors. The pHAT plugs in so that it's stacked directly above the Pi Zero.

Servo pHAT plugged into Raspberry Pi Zero GPIO header

Click the image for a closer look.

The servo cables for the pan-tilt rig will run underneath the mounting plate, under the board and pop out on the opposite side. The bottom servo plugs into ROW 0 and the top servo into ROW 1.

Highlighted Row 0 and Row 1

The brown wires should be on the pins closest to GPS board. See the image below.

Servo cables from pan-tilt mechanism plugged in

Click the image for a closer look.

The Qwiic cable that connects the GPS Board to the Servo pHAT through the time of flight sensor becomes obscured by the cover plate. It’s best to plug in the 50mm Qwiic cable to the GPS Board Qwiic connector facing the center of the cover plate at this point (don't plug it into the time of flight sensor quite yet).

Time of Flight Sensors

Next, we'll mount the time of flight sensors to the mounting plate. The holes from the metal bracket should line up with the holes on the top of the board as to not interfere with the pan-tilt mechanism. It should look like this:

Time of flight sensor mounted to metal mounting brackets on mounting plate

Affixing the Mounting Plate to the RVR and Connecting the Remaining Qwiic Cables

Take four of the remaining 1/4 inch screws and fasten the mounting plate to the cover plate of the RVR. The holes should lineup like this from below the cover plate:

Bottom of the RVR Cover Plate with the Mounting Plate Affixed

Again, be mindful with how tight you make the screws so as to not crack the acrylic plates.

With all the boards in place, we can plug in the remaining boards to the Qwiic bus. The two 50mm Qwiic cables connected to connectors 3 and 4 on the Mux board will plug into the front and rear facing Time of Flights sensors (respectively).

The remaining unplugged Qwiic connectors sticking out from under the mounting plate

The 50mm Qwiic Cables plugged into the Time of Flight Sensors

The rear Time of Flight sensor plugged into connector 4 on the Mux board

Finally, we'll plug the GPS board into the Servo pHAT. Take the 200mm Qwiic cable and plug it into the Qwiic connector on the Servo pHAT. Then, we'll run the cable through the slot in the mouting plate, then down through the slot directly underneath it in the RVR Cover Plate.

200mm Qwiic cable plugged into the Servo pHAT and run down through the slots into to below the RVR Cover Plate

On your build, the camera cable will be plugged in, we removed it for this photo to give you a better view of the Qwiic cable plugged in

Next, we'll run the cable back up through the outside slot next to the GPS board mentioned in the first steps. Plug the cable into the Qwiic connector on the GPS board facing forward.

200mm Qwiic Cable plugged into the GPS board

We'll take any slack from the 200mm cable and pull it gently under the RVR Cover Plate giving the system a cleaner look from the visible side.

Bottom of the RVR Cover Plate showing the 200mm Qwiic cable running underneath

Congratulations! You've built the entire system. Now it's time to connect it to the RVR. Gently clip the RVR Cover Plate into place.

RVR Cover Plate with the system built on top

Plugging the System into the RVR

In the final step we'll then connect the 4 pin Ribbon Cable from the four pin connector on the Servo pHAT to the UART Connector on the RVR.

To keep the UART cable from obscuring the view for the pan-tilt camera, I run it under the mounting plate. Refer to the images below - feel free to click on an image to see it more closely!


Cable outside the mounting plate Cable run under the mounting plate

Congratulations! You've completed the kit and are ready to start coding!

Troubleshooting

Resources and Going Further

So you've got this amazing looking robot. Now what? Time to program it!

Head on over to the Getting Started with the Autonomous Kit for the Sphero RVR Tutorial to get coding.

Getting Started with the Autonomous Kit for the Sphero RVR

December 13, 2019
Want to get started in robotics? Look no further than the SparkFun autonomous kit for the Sphero RVR! Whether you purchased the Basic or Advanced kit, this tutorial will get you rolling...

Need more information on the components included in this kit? We've got it!

Need more inspiration? Check out some of these other great SparkFun tutorials!

Assembly Guide for RedBot with Shadow Chassis

Assembly Guide for the RedBot Kit. This tutorial includes extra parts to follow to go along with the RedBot Inventor's Kit tutorial.

Continuous Rotation Servo Trigger Hookup Guide

How to use the SparkFun Continuous Rotation Servo Trigger with continuous rotation servos, without any programming!

Qwiic Joystick Hookup Guide

Looking for an easy way to implement a joystick to your next Arduino or Raspberry Pi project? This hookup guide will walk you through using the Qwiic Joystick with the Arduino IDE on a RedBoard Qwiic and in Python on a Raspberry Pi.

SparkFun Auto pHAT Hookup Guide

The pHAT to get your projects moving. This guide will help you get started using the Auto pHAT.