SparkFun Qwiic Micro (SAMD21E) Hookup Guide

≡ Pages
Contributors: M-Short, Elias The Sparkiest, bboyho

Example 1: Blink

Here's a quick example sketch to get the iconic blinking blue stat LED for Arduino blinking on the SparkFun Qwiic Micro; simply copy and paste from below, then click upload!

language:c
const int LED = 13; // Blue "stat" LED on pin 13

void setup() 
{
  pinMode(LED, OUTPUT); //set pin as output
  digitalWrite(LED, LOW); //turn LED off
}

void loop() 
{

  digitalWrite(LED, HIGH); // Blue LED on
  delay(250);
  digitalWrite(LED, LOW); // Blue LED off
  delay(250);
}

Now that you've passed the Arduino litmus test, you're all set up to start building your first project. If you haven't already, go check out our Qwiic eco-system which allows you to easily connect with sensors and other devices without the need for soldering.

Qwiic Connect System

In addition each add-on board within this eco-system has a library to get you started right away. For example, do you want to turn on a lamp with your SparkFun Qwiic Micro, better yet four lamps, or perhaps you'd like to see how much light your plants are getting? Check out any tutorial tagged with Arduino, sensor, and Qwiic for more ideas!

Qwiic Real Time Clock Module (RV-1805) Hookup Guide

Find out what time it is, even after the power's been out on your project for a while with the Qwiic Real Time Clock (RTC) module.

SparkFun LoRa Gateway 1-Channel Hookup Guide

How to setup and use the LoRa Gateway 1-Channel in Arduino.

SparkFun GPS-RTK Dead Reckoning ZED-F9R Hookup Guide

The u-blox ZED-F9R is a powerful GPS-RTK unit that uses a fusion of IMU, wheel ticks, a vehicle dynamics model, correction data, and GNSS measurements to provide highly accurate and continuous position for navigation in the difficult conditions. We will quickly get you set up using the Qwiic ecosystem through Arduino and Python so that you can start reading the output!

Qwiic Haptic Driver DA7280 Hookup Guide

The Qwiic Haptic Driver includes an itty-bitty, Linear Resonant Actuator (LRA) vibration motor and Dialog Semiconductor's DA7280 motor driver IC for applications that require haptic feedback.