SparkFun GPS-RTK Dead Reckoning ZED-F9R Hookup Guide

≡ Pages
Contributors: bboyho, Elias The Sparkiest

Hardware Overview (pHAT)

Power

Power for this board is 3.3V. Unlike the breakout board, the pHAT version pulls power from the Raspberry Pi's 3.3V pin on the 2x20 header. The Qwiic Connector's voltage pin is connected to this rail. The 3.3V pin should only be provided a clean 3.3V power signal from the Pi.

3.3V Power

Backup Battery

Just like the breakout board, the small metal disk in the just to the right of the ZED-F9R module is a small lithium battery. This battery does not provide power to the IC like the 3.3V system does, but to relevant systems inside the IC that allow for a quick reconnection to satellites. The time to first fix will about ~26 seconds, but after it has a lock, that battery will allow for a two second time to first fix. This is known as a hot start and lasts for four hours after the board is powered down. The battery provides over a years worth of power to the backup system and charges slowly when the board is powered. To charge it to full, leave your module plugged in for 48 hours.

Backup Battery

LEDs

Just like the breakout board, there are four LEDs on the bottom left of the board. Starting from the left:

  • PWR: The power LED labeled as PWR will illuminate when 3.3V is activated.
  • PPS: The pulse per second LED labelled as PPS will illuminate each second once a position lock has been achieved. This generates a pulse that is synchronized with a GPS or UTC time grid. By default, you'll see one pulse a second.
  • RTK: The RTK LED will be illuminated constantly upon power up. Once RTCM data has been successfully received it will begin to blink. This is a good way to see if the ZED-F9R is getting RTCM from various sources. Once an RTK fix is obtained, the LED will turn off.
  • GEO: The GEO LED can be configured to turn on/off for geofencing applications.

Status LEDs

Jumpers

On the top side of the board, you will notice a few jumper pads.

  • I2C: This three way jumper labeled I2C connects two pull-up resistors to the I2C data lines. For general use, you can leave this jumper unmodified. If you have many I2C devices (about 7x devices, each with their own pull-up resistors), you will need to cut the jumpers.
  • SPI: The jumper labeled SPI is open by default. Closing the jumper with solder enables the SPI data bus thus disabling the UART functions on those lines. This also disables I2C interface. USB will still function.
  • PWR: Starting from the right side is a jumper labeled PWR. If you cut this trace, it will disconnect the Power LED.
  • PPS: On the left of the jumper is the PPS jumper that when cut disconnects the PPS LED.
  • GEO: Cutting the GEO jumper disconnect the LED used to indicate when we reach a certain condition for geofencing applications.
  • RTK: The RTK jumper disconnects the LED used for RTK applications.
  • SHLD: On the back of the board, the SHLD jumper connects the USB Type C connector's shield pin to GND. Cut this to isolate the USB Type C connector's shield pin. This was added in v1.1.

For more information, check out our tutorial on How to Work with Jumper Pads and PCB Traces .

U.FL Connector

The ZED-F9R requires a good quality L1/L2 GPS or GNSS (preferred) antenna. A U.FL connector is provided. Note: U.FL connectors are rated for only a few mating cycles (about 30) so we recommend you set it and forget it. You may need to secure the u.FL to SMA cable depending on your application. For more information on working with u.FL connectors, we recommend checking out our tutorial about using u.FL connectors.

u.FL Connector

Qwiic and I2C

After stacking the pHAT on a Raspberry Pi, you still have access to the I2C pins (GPIO02 and GPIO03) on the top side. Alternatively, you can use the Qwiic connector to daisy chain additional I2C devices on the bus. The Qwiic ecosystem is made for fast prototyping by removing the need for soldering. All you need to do to connect additional Qwiic devices is plug a Qwiic cable into the Qwiic connector and voila! You can also access those pins from the 2x20 header.

I2C

SPI

The pins for SPI (GPIO08, GPIO09, GPIO10, and GPIO11) are connected to the Pi if you decide to use this protocol. As mentioned in the jumpers section, you'll need to close the SPI jumper on the top to enable SPI.

SPI

UART

The ZED-F9R's UART1 is connected to the Pi's UART0 port (GPIO14, GPIO15). Keep in mind that the pins are tied to the MISO and MOSI pins. By default, we will be using the UART to read data from the u-blox module.

UART1

There is a row of through holes next to the USB Type-C connector labeled for their UART functionality. This is primarily used for RTCM3 correction data. By default, this port will automatically receive and parse incoming RTCM3 strings enabling RTK mode on the board like the other RTK breakout boards for the NEO-M8P-2 and ZED-F9P. The RTCM Correction port pins are arranged to match the industry standard serial connection (aka the 'FTDI' pinout). This pinout is compatible with our Bluetooth Mate and Serial Basic so you can send RTCM correction data from a cell phone or another computer. Note that RTCM3 data can also be sent over I2C, UART1, SPI, or USB if desired.

UART2 RTCM Correction Port

USB

To connect the ZED-F9R to u-center software, you can attach a USB Type-C cable to the connector. Keep in mind that the power pin is not connected to the USB-C connector. You will need to draw power from the qwiic conenctor or the Pi's 2x20 header pins.

USB-C Connector

Wheel Tick and Direction Pins

For advanced users that are interested in taking advantage of your vehicle's sensor readings, you can connect the following pins. Caution is advised however as this requires you to open up up the hood of your car and hack into the its system.

  • D-: The reference GND pin (D-) when connecting the direction pin.
  • D+: The direction pin is labeled as (D+) tells the ZED-F9R what direction the vehicle is moving (forward/reverse).
  • W-: The reference GND pin (W-) when connecting the wheel tick pin.
  • W+: The wheel tick pin (W+) tells the ZED-F9R the distance a vehicle's wheel has traveled. Depending on the odometer type that you connect to, the ZED-F9R can also receive speed data from the vehicle.

Wheel Tick and Direction Pins

Broken Out Pins

There are four other pins broken out:

  • RESET: The reset pin (RESET) resets the chip.
  • SAFEBOOT: The safeboot pin (SAFEBOOT) is used to start up the IC in safe boot mode, this could be useful if you somehow manage to corrupt the module's Flash memory.
  • INT: The interrupt pin (INT) can be used to wake the chip from power save mode.
  • PPS: The pulse per second pin (PPS) outputs pulse trains synchronized with the GPS or UTC time grid. The signal defaults to once per second but is configurable over a wide range. Read the u-blox Receiver Protocol Specification in the Resources and Going Further tab for more information.

Broken Out Pins

3D IMU Orientation and Reference

For easy reference, we've documented the IMU's vectors with 3D Cartesian coordinate axes on the top and bottom side of the board. Make sure to orient and mount the board correctly so that the ZED-F9R can accurately calculate navigation information. Remember, it's all relative.

Top View with the Axis for Reference Bottom View with the Axis for Reference

GPS Capabilities

The ZED-F9R is able to connect to up to four different GNSS constellations simultaneously with the 3D gyro and 3D accelerometer making it very accurate for its size. Below are the listed capabilities of the GPS unit.

Parameter Specification
Max navigation update rate (RTK) Priority navigation mode 30 Hz
Non-Priority navigation mode 2 Hz
Velocity Accuracy 0.05m/s
Dynamic Attitude Accuracy Heading 0.2 degrees
Pitch 0.3 degrees
Roll 0.5 degrees
Navigation Latency Priority Navigation Mode 15ms
Max Sensor Output Rate 100Hz
GNSS GPS+GLO+GAL +BDS GPS+GLO+GAL GPS+GAL GPS+GLO BDS+GLO
Time-To-First-Fix Cold Start 26s 25s 30s 25s 28s
Hot Start 2s 2s 2s 2s 2s
Aided Start 3s 3s 3s 3s 3s
Re-convergence time RTK ≤ 10s ≤ 10s ≤ 10s ≤ 10s ≤ 30s
SensitivityTracking and Navigation -160dBm -160dBm -160dBm -160dBm -160dBm
Reacquisition -157dBm -157dBm -157dBm -157dBm -157dBm
Cold Start -147dBm -147dBm -147dBm -147dBm -145dBm
Hot Start -158dBm -158dBm -158dBm -158dBm -158dBm

Performance in Different GNSS Modes from the ZED-F9R Datasheet

1.5m CEP
Horizontal Position Accuracy PVT1.5m CEP1.5m CEP1.5m CEP1.5m CEP1.5m CEP
SBAS1.0m CEP1.0m CEP1.0m CEP1.0m CEP1.0m CEP
RTK0.01m
+ 1ppm CEP
0.01m
+ 1ppm CEP
0.01m
+ 1ppm CEP
0.01m
+ 1ppm CEP
0.01m
+ 1ppm CEP
Vertical Position AccuracyRTK0.01m
+1ppm R50
0.01m
+1ppm R50
0.01m
+1ppm R50
0.01m
+1ppm R50
0.01m
+1ppm R50

Position accuracy in Different GNSS Modes from the ZED-F9R Datasheet

Board Dimensions

The board is slightly bigger than the breakout version. Overall, it is is 65.00mmx56.50mm (2.56"x2.22"). There are 4x mounting holes by each corner of the board.

Board Dimensions