Comments: SIK Experiment Guide for Arduino - V3.3

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • -------------------- Tech Support Tips/Troubleshooting/Common Issues --------------------

    GitHub Repo Compile Error

    If you are using the example code from the GitHub repository for circuit 14 [ https://github.com/sparkfun/SIK-Guide-Code/blob/v33/SIK_circuit14_shiftRegister/SIK_circuit14_shiftRegister.ino#L90 ], there is a missing curly bracket { on line 90. Unfortunately, we are not able to correct the code since we released v4.0. We were unable to resolve the issue [ https://github.com/sparkfun/SIK-Guide-Code/issues/23 ]. This is a note for those are still using the example code.

  • UD_Dave / about 10 years ago / 1

    Ok, so the "Marquee" code doesn't run, LEDs 0 & 4 light up, and that's it. The "PingPong" code is exactly the same as "OneAtATime" code. I sort of see what you wanted there, but I'm not sure how to go about it. I guess, that's what these kits are about. At least I got the first and second options to run.

  • UD_Dave / about 10 years ago / 1

    Well, I solved my problem. The code string "for(index = 7; index >= 0; index = index --)" or "for(index = 7; index >= 0; index = index ++)" does not work. For the code to run the program properly the line MUST read "for(index = 7; index >= 0; index = index -1)" or "for(index = 7; index >= 0; index = index +1)"

    I changed it and it runs fine. I'm not sure why it doesn't like ++ (--) rather than +1 (-1).

  • UD_Dave / about 10 years ago / 1

    I am working through the SIK experiments and have come across a problem in #4: Driving Multiple LEDs. I have the wiring correct, checked it 4 times, ran the code on both a RedBoard and an Arduino UNO and I get the same result. The LED on pin #2 lights up, but nothing else happens. I checked to see if each LED was wire properly, no shorts, etc, and all was OK. I am a code Newbie, but since my wiring is OK, it's got to be the code, right? For some reason, it never gets past Pin 2 High (LED 0). I used the code from the SIK_Guide_Code_V3.3 and I also cut and paste it from this site.

    Thanks


If you've found an issue with this tutorial content, please send us your feedback!