MicroMod GNSS Function Board - NEO-M9N Hookup Guide

≡ Pages
Contributors: bboyho, Elias The Sparkiest

Introduction

The u-blox NEO-M9N is a powerful GPS unit that now comes populated on a MicroMod Function Board! In this tutorial, we will quickly get you set up using it with the MicroMod ecosystem and Arduino so that you can start reading the output.

SparkFun MicroMod GNSS Function Board - NEO-M9N

GPS-18378
$49.95 $34.97

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Reversible USB A to C Cable - 2m

CAB-15424
$10.50

SparkFun Mini Screwdriver

TOL-09146
$1.50

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

SparkFun MicroMod GNSS Function Board - NEO-M9N

GPS-18378
$49.95 $34.97

SparkFun MicroMod Main Board - Single

DEV-18575
Retired

MicroMod Main Board

To hold the processor board and function board, you will need one Main Board. Depending on your application, you may choose to have one or two additional function boards.

SparkFun MicroMod Main Board - Single

DEV-18575
Retired

SparkFun MicroMod Main Board - Double

DEV-18576
Retired

MicroMod Processor Board

There are a variety of MicroMod Processor Boards available to choose from. We recommend getting the ones that are Arduino compatible.

SparkFun MicroMod Teensy Processor

DEV-16402
$24.95

SparkFun MicroMod ESP32 Processor

WRL-16781
$19.95

SparkFun MicroMod SAMD51 Processor

DEV-16791
Retired

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

MicroMod Function Board

To add additional functionality to your Processor Board, you'll want to include one or two function boards when connecting them to the Main Board. Besides the NEO-M9N, you could add an additional function board for your project if you have the Main Board - Double.

SparkFun MicroMod GNSS Function Board - NEO-M9N

GPS-18378
$49.95 $34.97

SparkFun MicroMod WiFi Function Board - ESP32

WRL-18430
$14.95 $8.97

SparkFun MicroMod LoRa Function Board

WRL-18573
Retired

SparkFun MicroMod Environmental Function Board

SEN-18632
$149.95 $112.46

Tools

You will need a screw driver to secure the Processor and Function boards.

SparkFun Mini Screwdriver

TOL-09146
$1.50

Pocket Screwdriver Set

TOL-12891
$5.50

MicroMod Screwdriver

TOL-19012
$0.75

Suggested Reading

If you aren't familiar with the MicroMod ecosystem, we recommend reading here for an overview.

MicroMod Logo
MicroMod Ecosystem

If you aren’t familiar with the following concepts, we also recommend checking out a few of these tutorials before continuing. Make sure to check the respective hookup guides for your processor board and function board to ensure that you are installing the correct USB-to-serial converter. You may also need to follow additional instructions that are not outlined in this tutorial to install the appropriate software.

GPS Basics

The Global Positioning System (GPS) is an engineering marvel that we all have access to for a relatively low cost and no subscription fee. With the correct hardware and minimal effort, you can determine your position and time almost anywhere on the globe.

Serial Peripheral Interface (SPI)

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

Getting Started with U-Center for u-blox

Learn the tips and tricks to use the u-blox software tool to configure your GPS receiver.

Three Quick Tips About Using U.FL

Quick tips regarding how to connect, protect, and disconnect U.FL connectors.

Getting Started with MicroMod

Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

MicroMod Main Board Hookup Guide

The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single and Main Board - Double.

Hardware Overview

We've taken the u-blox NEO-M9N and broken the board out to a MicroMod Function Board! In this section, we will go over the main features of the Function Board.

u-blox NEO-M9N

For a detailed overview of the module, these integrated systems and how to use them, refer to the datasheet and integration manual linked in the Resources and Going Further.

Power

To power the board, you will need to apply power to a SparkFun Main Board. Power applied from the M.2 connector VCC line will be regulated down with the 3.3V/600mA AP2112K voltage regulator.

3.3V/600mA AP2112K Voltage regulator regulating voltage from the M.2 Edge pins

Communication Ports

The NEO-M9N has four communication ports. You can read NMEA data over I2C while you send configuration commands over the UART and vice/versa. The only limit is that the SPI pins are mapped onto the I2C and UART pins so it’s either SPI or I2C+UART. You will need select the port with the BUS SELECT jumper. The USB port is available at all times. There is a bilateral switch between the M.2 connector and the NEO-M9N's Serial, SPI, and I2C ports. The switch connects the appropriate port depending on the on the jumper position.

USB, Serial, SPI, I2C Ports

USB

The USB C connector is available for those that are interested in using the u-center software on a computer. There is a TVS diode between the USB port and NEO-M9N's USB data pins for protection.

USB Connector and TVS Diode IC

I2C (a.k.a DDC)

The u-blox NEO-M9N has a “DDC” port which is really just an I2C port (without all the fuss of trademark issues). These pins are shared with the SPI pins. Connecting the DSEL pin to the Serial/I2C with the 2-pin jumper disables the SPI data bus while keeping the UART and I2C interface available.

I2C

UART/Serial

The classic serial pins are available on the NEO-M9N but are shared with the SPI pins. Connecting the DSEL pin to the Serial/I2C with the 2-pin jumper disables the SPI data bus while keeping the UART and I2C interface available.

  • TXO/SDO = TX out from NEO-M9N
  • RXI/SDI = RX into NEO-M9N

Serial

SPI

The NEO-M9N can also be configured for SPI communication. Connecting the DSEL pin to the SPI with the 2-pin jumper enables the SPI data bus thus disabling the UART functions on those lines. This also disables I2C interface.

SPI

Backup Battery

The small metal disk is a small lithium battery. This battery does not provide power to the IC like the 3.3V system does, but to relevant systems inside the IC that allow for a quick reconnection to satellites. The time to first fix will about ~29 seconds, but after it has a lock, that battery will allow for a two second time to first fix. This is known as a hot start and lasts for four hours after the board is powered down. The battery provides over a years worth of power to the backup system and charges slowly when the board is powered. To charge it to full, leave your module plugged in for 48 hours.

backup battery

u.FL Connector

The MicroMod GNSS Function Board includes a u.FL connector for a secure connection with a patch antenna. Depending on the antenna, you may need a u.FL adapter to connect. The u.FL connector was added as a design choice for users that decide to place the MicroMod Main Board with the GNSS Function Board in an enclosure. With the u.FL adapter, the SMA connector can be mounted to the enclosure. For more information on working with u.FL connectors, we recommend checking out our tutorial about using u.FL connectors.

u.FL connector

EEPROM

The board includes an I2C EEPROM. Unfortunately, this is not available for the user and was meant to hold board specific information.

EEPROM

LEDs

The board includes two status LEDs.

  • 3V3: The 3V3 LED indicates when the board is powered. This LED is connected to the 3.3V line.
  • PPS: The PPS LED is connected to the Pulse Per Second line. When connected to a satellite, this line generates a pulse that is synchronized with a GPS or UTC time grid. By default, you'll see one pulse a second.

3.3V Power and PPS LEDs

Jumpers

The board includes a few jumpers to configure the NEO-M9N module. For more information, check out our tutorial on working with jumper pads and PCB traces.

  • I2C Pull-up Resistors - This three way jumper labeled I2C connects two pull-up resistors to the I2C data lines. If you have many devices on your I2C data lines, then you may consider cutting these.
  • WP - Adding solder to the jumper pad will disable write protect for the EEPROM.
  • 3V3 - The jumper on the opposite side of the board with the label 3V3 is connected to the 3V3 LED. Cutting this jumper will disable the LED.
  • PPS - The jumper on the opposite side of the board with the label PPS is connected to the PPS LED. Cutting this jumper will disable the LED.
  • Bus Select
    • SPI - Connecting the DSEL pin to the SPI with the 2-pin jumper enables the SPI data bus thus disabling the UART functions on those lines. This also disables I2C interface.
    • DSEL - This pin is connected to the NEO-M9N's D_SEL pin to select the interface. Connecting this pin to either side will select the communication protocol.
    • Serial/I2C - Connecting the DSEL pin to the Serial/I2C with the 2-pin jumper disables the SPI data bus while keeping the UART and I2C interface available. The UART and I2C can also be enabled if the DSEL pin is open and not connected to either side. We recommend keeping the 2-pin jumper connected to avoid misplacing the component.
  • SAFEBOOT - The PTH pads labeled as SAFEBOOT is used to start up the IC in safe boot mode, this could be useful if you somehow manage to corrupt the module's Flash memory. Breakaway a row of 2-pins from the header, solder the pins to the board, and connect a 2-pin jumper to enable the mode.
Jumpers (Top View) Jumpers (Bottom View)
Jumpers (Top View) Jumpers (Bottom View)

GPS Capabilities

The SparkFun GNSS Function Board NEO-M9N is able to connect to up to four different GNSS constellations at a time making it very accurate for its size. Below are the listed capabilities of the GPS unit when connecting to multiple GNSS constellations and when connecting to a single constellation.

Constellations GPS+GLO+GAL+BDS GPS+GLONASS+GAL GPS+GLO GPS+BDS GPS+GAL
Horizontal Position Accuracy 2m2m2m2m2m
Max Navigation Update Rate PVT 25Hz 25Hz 25Hz25Hz25Hz
Time-To-First-Fix Cold Start24s 25s 26s 28s29s
Hot Start 2s 2s 2s 2s 2s
SensitivityTracking and Navigation -167dBm -167dBm -167dBm -1667dBm -166dBm
Reacquisition -160dBm -160dBm -160dBm -160dBm -160dBm
Cold Start-148dBm -148dBm -148dBm -148dBm -148dBm
Hot Start -159dBm -159dBm -159dBm -159dBm-159dBm
Velocity Accuracy 0.05m/s 0.05m/s 0.05m/s 0.05m/s 0.05m/s
Heading Accuracy 0.3deg 0.3deg 0.3deg 0.3deg 0.3deg


When using a single GNSS constellation:

Constellation GPS GLONASS BEIDOU Galileo
Horizontal Position Accuracy 2m4m3m3m
Max Navigation Update Rate PVT 25Hz 25Hz 25Hz 25Hz
Time-To-First-Fix Cold Start 29s 27s 32s 42s
Hot Start 2s 2s 2s 2s
SensitivityTracking and Navigation -166dBm -164dBm -160dBm -159dBm
Reacquisition -160dBm -155dBm -157dBm -154dBm
Cold Start-148dBm -145dBm -145dBm -140dBm
Hot Start -159dBm -156dBm -159dBm -154dBm
Velocity Accuracy 0.05m/s 0.05m/s 0.05m/s 0.05m/s
Heading Accuracy 0.3deg 0.3deg 0.3deg 0.3deg

Hardware Pinout

Depending on your window size, you may need to use the horizontal scroll bar at the bottom of the table to view the additional pin functions. Note that the M.2 connector pins on opposing sides are offset from each other as indicated by the bottom pins where it says (Not Connected)*. There is no connection to pins that have a "-" under the primary function.

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Function Bottom
Pin
   Top   
Pin
Function
(Not Connected) 75 GND
3.3V 74 73 G5 / BUS5
RTC_3V_BATT 72 71 G6 / BUS6
SPI_CS1# SDIO_DATA3 (I/O) 70 69 G7 / BUS7
SDIO_DATA2 (I/O) 68 67 G8
SDIO_DATA1 (I/O) 66 65 G9 ADC_D- CAM_HSYNC
SPI_CIPO1 SDIO_DATA0 (I/O) 64 63 G10 ADC_D+ CAM_VSYNC
SPI COPI1 SDIO_CMD (I/O) 62 61 SPI_CIPO (I)
SPI SCK1 SDIO_SCK (O) 60 59 SPI_COPI (O) LED_DAT
AUD_MCLK (O) 58 57 SPI_SCK (O) LED_CLK
CAM_MCLK PCM_OUT I2S_OUT AUD_OUT 56 55 SPI_CS#
CAM_PCLK PCM_IN I2S_IN AUD_IN 54 53 I2C_SCL1 (I/O)
PDM_DATA PCM_SYNC I2S_WS AUD_LRCLK 52 51 I2C_SDA1 (I/O)
PDM_CLK PCM_CLK I2S_SCK AUD_BCLK 50 49 BATT_VIN / 3 (I - ADC) (0 to 3.3V)
G4 / BUS4 48 47 PWM1
G3 / BUS3 46 45 GND
G2 / BUS2 44 43 CAN_TX
G1 / BUS1 42 41 CAN_RX
G0 / BUS0 40 39 GND
A1 38 37 USBHOST_D-
GND 36 35 USBHOST_D+
A0 34 33 GND
PWM0 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 SWDIO
UART_TX2 (O) 22 21 SWDCK
UART_RX2 (I) 20 19 UART_RX1 (I)
CAM_TRIG D1 18 17 UART_TX1 (0)
I2C_INT# 16 15 UART_CTS1 (I)
I2C_SCL (I/0) 14 13 UART_RTS1 (O)
I2C_SDA (I/0) 12 11 BOOT (I - Open Drain)
D0 10 9 USB_VIN
SWO G11 8 7 GND
RESET# (I - Open Drain) 6 5 USB_D-
3.3V_EN 4 3 USB_D+
3.3V 2 1 GND
Function Bottom
Pin
   Top   
Pin
Function
(Not Connected) 75 GND
VIN 74 73 3.3V
VIN 72 71 Power EN
- 70 69 -
- 66 65 -
- 64 63 -
- 62 61 -
- 60 59 -
- 58 57 -
- 56 55 -
- 54 53 INT
- 52 51 RESET
- 50 49 SPI_CS0
- 48 47 PPS
- 46 45 GND
- 44 43 -
- 42 41 -
EEPROM_WP 40 39 GND
- 38 37 -
EEEPROM_A0 36 35 -
EEEPROM_A1 34 33 GND
EEEPROM_A2 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 -
- 22 21 I2C_SCL
- 20 19 I2C_SDA
- 18 17 -
- 16 15 UART_RX
- 14 13 UART_TX
- 12 11 -
- 10 9 -
- 8 7 SPI_SDO
- 6 5 SPI_SDI
- 4 3 SPI_SCK
- 2 1 GND
Signal Group Signal I/O Description Voltage
Power 3.3V I 3.3V Source 3.3V
GND Return current path 0V
USB_VIN I USB VIN compliant to USB 2.0 specification. Connect to pins on processor board that require 5V for USB functionality 4.8-5.2V
RTC_3V_BATT I 3V provided by external coin cell or mini battery. Max draw=100μA. Connect to pins maintaining an RTC during power loss. Can be left NC. 3V
3.3V_EN O Controls the carrier board's main voltage regulator. Voltage above 1V will enable 3.3V power path. 3.3V
BATT_VIN/3 I Carrier board raw voltage over 3. 1/3 resistor divider is implemented on carrier board. Amplify the analog signal as needed for full 0-3.3V range 3.3V
Reset Reset I Input to processor. Open drain with pullup on processor board. Pulling low resets processor. 3.3V
Boot I Input to processor. Open drain with pullup on processor board. Pulling low puts processor into special boot mode. Can be left NC. 3.3V
USB USB_D± I/O USB Data ±. Differential serial data interface compliant to USB 2.0 specification. If UART is required for programming, USB± must be routed to a USB-to-serial conversion IC on the processor board.
USB Host USBHOST_D± I/O For processors that support USB Host Mode. USB Data±. Differential serial data interface compliant to USB 2.0 specification. Can be left NC.
CAN CAN_RX I CAN Bus receive data. 3.3V
CAN_TX O CAN Bus transmit data. 3.3V
UART UART_RX1 I UART receive data. 3.3V
UART_TX1 O UART transmit data. 3.3V
UART_RTS1 O UART ready to send. 3.3V
UART_CTS1 I UART clear to send. 3.3V
UART_RX2 I 2nd UART receive data. 3.3V
UART_TX2 O 2nd UART transmit data. 3.3V
I2C I2C_SCL I/O I2C clock. Open drain with pullup on carrier board. 3.3V
I2C_SDA I/O I2C data. Open drain with pullup on carrier board 3.3V
I2C_INT# I Interrupt notification from carrier board to processor. Open drain with pullup on carrier board. Active LOW 3.3V
I2C_SCL1 I/O 2nd I2C clock. Open drain with pullup on carrier board. 3.3V
I2C_SDA1 I/O 2nd I2C data. Open drain with pullup on carrier board. 3.3V
SPI SPI_COPI O SPI Controller Output/Peripheral Input. 3.3V
SPI_CIPO I SPI Controller Input/Peripheral Output. 3.3V
SPI_SCK O SPI Clock. 3.3V
SPI_CS# O SPI Chip Select. Active LOW. Can be routed to GPIO if hardware CS is unused. 3.3V
SPI/SDIO SPI_SCK1/SDIO_CLK O 2nd SPI Clock. Secondary use is SDIO Clock. 3.3V
SPI_COPI1/SDIO_CMD I/O 2nd SPI Controller Output/Peripheral Input. Secondary use is SDIO command interface. 3.3V
SPI_CIPO1/SDIO_DATA0 I/O 2nd SPI Peripheral Input/Controller Output. Secondary use is SDIO data exchange bit 0. 3.3V
SDIO_DATA1 I/O SDIO data exchange bit 1. 3.3V
SDIO_DATA2 I/O SDIO data exchange bit 2. 3.3V
SPI_CS1/SDIO_DATA3 I/O 2nd SPI Chip Select. Secondary use is SDIO data exchange bit 3. 3.3V
Audio AUD_MCLK O Audio master clock. 3.3V
AUD_OUT/PCM_OUT/I2S_OUT/CAM_MCLK O Audio data output. PCM synchronous data output. I2S serial data out. Camera master clock. 3.3V
AUD_IN/PCM_IN/I2S_IN/CAM_PCLK I Audio data input. PCM syncrhonous data input. I2S serial data in. Camera periphperal clock. 3.3V
AUD_LRCLK/PCM_SYNC/I2S_WS/PDM_DATA I/O Audio left/right clock. PCM syncrhonous data SYNC. I2S word select. PDM data. 3.3V
AUD_BCLK/PCM_CLK/I2S_CLK/PDM_CLK O Audio bit clock. PCM clock. I2S continuous serial clock. PDM clock. 3.3V
SWD SWDIO I/O Serial Wire Debug I/O. Connect if processor board supports SWD. Can be left NC. 3.3V
SWDCK I Serial Wire Debug clock. Connect if processor board supports SWD. Can be left NC. 3.3V
ADC A0 I Analog to digital converter 0. Amplify the analog signal as needed to enable full 0-3.3V range. 3.3V
A1 I Analog to digital converter 1. Amplify the analog signal as needed to enable full 0-3.3V range. 3.3V
PWM PWM0 O Pulse width modulated output 0. 3.3V
PWM1 O Pulse width modulated output 1. 3.3V
Digital D0 I/O General digital input/output pin. 3.3V
D1/CAM_TRIG I/O General digital input/output pin. Camera trigger. 3.3V
General/Bus G0/BUS0 I/O General purpose pins. Any unused processor pins should be assigned to Gx with ADC + PWM capable pins given priority (0, 1, 2, etc.) positions. The intent is to guarantee PWM, ADC and Digital Pin functionality on respective ADC/PWM/Digital pins. Gx pins do not guarantee ADC/PWM function. Alternative use is pins can support a fast read/write 8-bit or 4-bit wide bus. 3.3V
G1/BUS1 I/O 3.3V
G2/BUS2 I/O 3.3V
G3/BUS3 I/O 3.3V
G4/BUS4 I/O 3.3V
G5/BUS5 I/O 3.3V
G6/BUS6 I/O 3.3V
G7/BUS7 I/O 3.3V
G8 I/O General purpose pin 3.3V
G9/ADC_D-/CAM_HSYNC I/O Differential ADC input if available. Camera horizontal sync. 3.3V
G10/ADC_D+/CAM_VSYNC I/O Differential ADC input if available. Camera vertical sync. 3.3V
G11/SWO I/O General purpose pin. Serial Wire Output 3.3V

Board Dimensions

The board uses the standard MicroMod Function Board size which measures about 1.50"x2.56".

Board Dimensions

Hardware Assembly

If you have not already, make sure to check out the Getting Started with MicroMod: Hardware Hookup for information on inserting your Processor and Function Boards to the Main Board.

Getting Started with MicroMod

October 21, 2020
Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

Insert your chosen Processor and GNSS Function board at an angle into the M.2 connector. The Processor Board will stick up at an angle (at around 25°).

alt text

Hold down each board, insert the screws, and to tighten.

alt text

After securing the Processor and Function Board to the Main Board, your setup should look like the image below.

alt text

Insert the u.FL adapter to the MicroMod GNSS Function Board. Connect the patch antenna to the other end of the u.FL adapter. The SMA connector just needs to be finger tight to secure the antenna to the adapter..

alt text

Connect a USB Type C Cable to power and program your Processor Board. In this case, we used the MicroMod Main Board - Single and MicroMod Artemis Processor. This will also power the MicroMod GNSS Function Board.

alt text

For users that want to connect the NEO-M9N to u-blox's u-center, insert a second USB Type C cable to the MicroMod GNSS Function Board's USB C connector.

alt text

Software Installation

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review the following tutorials.

Arduino Board Definitions and Driver

We'll assume that you installed the necessary board files and drivers for your Processor Board. In this case, we used the MicroMod Artemis Processor Board which uses the CH340 USB-to-serial converter. If you are using a Processor Board, make sure to check out its hookup guide for your Processor Board.

Installing Board Definitions in the Arduino IDE

September 9, 2020
How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

MicroMod Artemis Processor Board Hookup Guide

October 21, 2020
Get started with the Artemis MicroMod Processor Board in this tutorial!

How to Install CH340 Drivers

August 6, 2019
How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.

Arduino Library

All of our u-blox based GPS boards share the same library: this board, their predeccesors and the higher precision u-blox cousins. The SparkFun u-blox Arduino library can be downloaded with the Arduino library manager by searching 'SparkFun u-blox GNSS' or you can grab the zip here from the GitHub repository to manually install:

There are several example sketches provided that utilize the I2C bus to get you up and receiving messages from space. We'll go over one of the examples in this tutorial.

Main Board Example - Pin Connection Table

For NEO-M9N specific pins, here is the mapping between the function board and main board's processor pins. For the following examples, we are using the Artemis Processor Board.

AUDIO UART GPIO/BUS I2C SDIO SPI Dedicated
NEO-M9N Function Board
Pin Name
I/O
Direction
Main Board's
Processor Pin
Slot 0 Slot 1
VCC I VCC VCC
EN O PWR_EN0 PWR_EN1
GND - GND GND
SPI_SCK O SPI_SCK SPI_SCK
SPI_POCI I SPI_POCI SPI_POCI
SPI_PICO O SPI_PICO SPI_PICO
I2C_SCL I/O I2C_SCL I2C_SCL
I2C_SDA I/O I2C_SDA I2C_SDA
RX O TX1 TX2
TX I RX1 RX2
PPS I/O D0 D1
SPI_CS I/O CS0 CS1
RESET I/O PWM0 PWM1
INT I/O G0 G5
EEPROM_A0 I/O - -
EEPROM_A1 I/O - -
EEPROM_A2 I/O - -
EEPROM_WP I/O - -

Arduino Example

We're just going to look at example two (i.e. "Example2_NMEAParsing.ino") which in my opinion, makes it clear the awesomeness of these GPS receivers. That is to say, talking to satellites and finding out where in the world you are.

language:c
#include <Wire.h> //Needed for I2C to GPS

#include "SparkFun_u-blox_GNSS_Arduino_Library.h" //Click here to get the library: http://librarymanager/All#SparkFun_u-blox_GNSS
SFE_UBLOX_GNSS myGNSS;

void setup()
{
  Serial.begin(115200);
  Serial.println("SparkFun u-blox Example");

  Wire.begin();

  if (myGNSS.begin() == false)
  {
    Serial.println(F("u-blox GNSS module not detected at default I2C address. Please check wiring. Freezing."));
    while (1);
  }

  //This will pipe all NMEA sentences to the serial port so we can see them
  myGNSS.setNMEAOutputPort(Serial);
}

void loop()
{
  myGNSS.checkUblox(); //See if new data is available. Process bytes as they come in.

  delay(250); //Don't pound too hard on the I2C bus
}

When you upload this code you'll have to wait ~24s to get a lock onto any satellites. After that first lock, the backup battery on the board will provide power to some internal systems that will allow for a hot start the next time you turn on the board. The hot start only lasts four hours, but allows you to get a lock within one second. After you get a lock the serial terminal will start listing longitude and latitude coordinates, as seen below. Make sure to set the serial monitor to 115200 baud.

This image shows a screenshot of the Arduino Serial terminal spitting out latitude and longitude data.

These are the coordinates for SparkFun HQ

Troubleshooting

Resources and Going Further

Now that you've successfully got your MicroMod GNSS Function Board - NEO-M9N up and running, it's time to incorporate it into your own project! For more information, check out the resources below.

Hardware Documentation

MicroMod Documentation

Or check out other tutorials related to GPS and GNSS:

GPS Basics

The Global Positioning System (GPS) is an engineering marvel that we all have access to for a relatively low cost and no subscription fee. With the correct hardware and minimal effort, you can determine your position and time almost anywhere on the globe.

HX1 APRS Transmitter Hookup Guide

The HX1 is a low-power amateur radio transmitter that can be used to send data to the Automatic Packet Reporting System (APRS) network.

nRF9160 Thing Plus Hookup Guide

Getting started with the nRF9160 from Circuit Dojo and SparkFun!

How to Upgrade Firmware of a u-blox GNSS Receiver

A few steps and you'll upgrade to the latest features on a u-blox GNSS receiver.