Cryptographic Co-Processor ATECC508A (Qwiic) Hookup Guide

≡ Pages
Contributors: QCPete

Example 5: Random

This example shows how to use the Random Number Generator on the Sparkfun Cryptographic Co-processor. It will print random numbers once a second on the serial terminal at 115200.

This example only requires 1 Artemis and 1 co-processor. If you just completed example 4, you can choose to use Alice or Bob. This example helps set the stage for Example 6, so it's a good idea to check it out and see how the ATECC508A does random numbers - particularly its ability to create 32 bytes of random data!

Output in Serial Monitor
Output in the Arduino Serial Monitor.

Note, this chip is a bit more capable than the built-in Arduino function random().

  • random(max)
  • random(min, max)

It has a basic random(min, max). This will return a random number of type long. Note, it works very similarly to the built-in Arduino random() function, you can send it a single argument as a max, or you can send it two (as min and max).

It also has the following 3 other functions that can be useful in other applications.

  • getRandomByte()
  • getRandomInt()
  • getRandomLong()

Each of these functions return a random number of the type written into the name.

And lastly...

  • updateRandom32Bytes() will create 32 bytes of random data and store it in atecc.random32Bytes[].

After calling updateRandom32Bytes() then your random 32 bytes of data are available at a public variable within the library instance. If your instance was named atecc as in the SparkFun examples, this array would be atecc.random32Bytes[]. This can be useful as a challenge or time-to-live-token (aka NONCE) to send to another device.