AD8232 Heart Rate Monitor Hookup Guide

≡ Pages
Contributors: CaseyTheRobot

Resources and Going Further

Thanks for reading. For more resources on the AD8232 Heart Rate Monitor, check out the following links:

For more Electronics Fun, check out these other SparkFun tutorials:

MyoWare Muscle Sensor Kit

Line of products to work with the MyoWare muscle sensor from Advancer Technologies.

Fingerprint Scanner (GT-521Fxx) Hookup Guide

This tutorial provides information about how to connect to ADH-Tech's fingerprint scanner (GT-521F32) and how to use it with Hawley's FPS_GT511C3 library for Arduino.

Getting Started with Walabot

See through walls, track objects, monitor breathing patterns, and more using the power of radio frequency with the Walabot! In this tutorial, we will explore Walabot’s features using the Software Demo Kit (SDK) on Windows and the Application Programming Interface (API) on Linux-based distributions for embedded projects.

SparkFun Photodetector (MAX30101) Hookup Guide

The SparkFun Photodetector - MAX30101 (Qwiic) is the successor to the MAX30105 particle sensor, a highly sensitive optical sensor. This tutorial will get you started on retrieving the raw data from the MAX30101 sensor.

More Biometric products offered by SparkFun:

MyoWare 2 Muscle Sensor

DEV-27924
$42.95

SparkFun Air Quality PM1/PM2.5/PM10 Sensor - BMV080 (Qwiic)

SEN-26554
$59.95

SparkFun Pulse Oximeter and Heart Rate Sensor - MAX30101 & MAX32664 (Qwiic)

SEN-15219
$48.95

MyoWare 2 Muscle Sensor Wireless Kit

KIT-27922
$124.95