SparkFun Photodetector (MAX30101) Hookup Guide

≡ Pages
Contributors: santaimpersonator

Resources and Going Further

For more on the SparkFun Photodetector (MAX30101), check out the links below:

Application Notes

Note: Particle detection, heart rate measurement, and photoplethysmography (for pulse oximetry) are applications of the MAX30101. These applications are detailed in the notes below; however, they require an understanding of the operating principles of the sensor and a conceptual knowledge of the application(s). Although, we provided the information below for interested users and may provide some examples of the application in our software; these applications are, unfortunately, not supported by SparkFun and the examples are primarily for demonstration purposes only.

Here are additional resources on how the MAX30101 functions for HR detection and pulse oximetry:

For more information on particulate matter and their detection, check out these resources:

Maxim's Original Firmware for the MAX30102 adapted in our Arduino Library:

For more sensor action, check out these other great SparkFun tutorials.

Si7021 Humidity and Temperature Sensor Hookup Guide

The Si7021 humidity and temperature sensor is an easy to use, digital, low-cost sensor to aid you in all your environment sensing needs.

Gator:starter ProtoSnap Hookup Guide

Get started clipping sensors and lights to the micro:bit with the gator:starter gator:board from SparkFun!

SparkFun gator:soil Hookup Guide

The gator:soil is analog soil moisture sensor. This tutorial will get you started using the gator:soil with the micro:bit platform.

Tinker Kit Circuit Guide

This guide takes you through the basics of building 11 different circuits with the SparkFun Tinker Kit and how to program them using the Arduino IDE.

Or check out this blog post for ideas: