RedBoard Qwiic Hookup Guide

≡ Pages
Contributors: santaimpersonator

Resources and Going Further

Now that you've successfully got started with your SparkFun RedBoard Qwiic, it's time to incorporate it into your own project! For more information, check out the resources below:


Need some inspiration for your next project? Check out some of these related tutorials:

SparkFun Tutorials

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

What is an Arduino?

What is this 'Arduino' thing anyway? This tutorials dives into what an Arduino is and along with Arduino projects and widgets.

Installing Arduino IDE

A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

Arduino Tutorials

Arduino Board Comparison Guides

Choosing an Arduino for Your Project

Examining the diverse world of Arduino boards and understanding the differences between them before choosing one for a project.

Standard Arduino Comparison Guide

Arduino Comparison Guide Uno or Pro Mini? Bluetooth or wireless? When it comes to Arduinos, there are a lot of choices. We've compiled every Arduino development…

RedBoard vs. Uno

In this tutorial we discuss the differences and similarities between the RedBoard and the Arduino Uno (SMD and PTH). The development platforms

Arduino Shields

Arduino Shields v2

An update to our classic Arduino Shields Tutorial! All things Arduino shields. What they are and how to assemble them.
Beginner

Click the buttons above for tutorials relating to the board functionality based on topic difficulty.

Beginner

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

Analog to Digital Conversion

The world is analog. Use analog to digital conversion to help digital devices interpret the world.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

Analog vs. Digital

This tutorial covers the concept of analog and digital signals, as they relate to electronics.

Data Types in Arduino

Learn about the common data types and what they signify in the Arduino programming environment.

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

Intermediate

Serial Peripheral Interface (SPI)

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Processor Interrupts with Arduino

What is an interrupt? In a nutshell, there is a method by which a processor can execute its normal program while continuously monitoring for some kind of event, or interrupt. There are two types of interrupts: hardware and software interrupts. For the purposes of this tutorial, we will focus on hardware interrupts.

Advanced

Installing an Arduino Bootloader

This tutorial will teach you what a bootloader is and why you would need to install or reinstall it. We will also go over the process of burning a bootloader by flashing a hex file to an Arduino microcontroller.

Integrated Circuits

An introduction to integrated circuits (ICs). Electronics' ubiquitous black chips. Includes a focus on the variety of IC packages.

Reading and Writing Serial EEPROMs

EEPROM is a great way to add extra memory to your microcontroller project. Wait 'til you see how easy it is to use!

Example Projects

Assembly Guide for RedBot with Shadow Chassis

Assembly Guide for the RedBot Kit. This tutorial includes extra parts to follow to go along with the RedBot Inventor's Kit tutorial.

SparkFun Inventor's Kit Experiment Guide - v4.0

The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.0a.

RedBoard Edge Hookup Guide

The RedBoard Edge is a RedBoard that's been rebuilt around the idea that projects are eventually put into an enclosure to help clean up their look.