mbed Starter Kit Experiment Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: Shawn Hymel

Experiment 7: USB Device

This tutorial covers USB devices with the mbed LPC1768. Using a USB mini-B breakout and some buttons, we enumerate the mbed as a USB mouse and control the computer's pointer with the buttons.

mbed USB device circuit

Suggested Reading

The Circuit

This circuit can be made with parts in the SparkFun mbed Starter Kit. Also, keep in mind that the LPC1768 box contains a USB mini-B cable for programming and power.

Parts List

To follow this experiment, you would will need the following materials if you did not order the SparkFun mbed starter kit. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary. The experiment will be using 4x 10kOhm resistors.

Schematic

mbed usb device schematic

Click on schematic to view larger image.

Connections

Connect the LPC1768 to the USB mini-B breakout and buttons.

Fritzing Diagram

mbed USB Device fritzing

Hookup Table

Place the LPC1768 in the first breadboard with pin VOUT in position i1 and pin 20 in position b20.

Connect the rest of the components as follows:

Component Breadboard 1 Breadboard 2
Mini USB Breakout* h25 (GND) h27 (D+) h28 (D-) h29 (VCC)
Pushbutton d2 d4 g2 g4
Pushbutton d10 d12 g10 g12
Pushbutton d18 d20 g18 g20
Pushbutton d26 d28 g26 g28
10K Resistor i2 ( + )
10K Resistor i10 ( + )
10K Resistor i18 ( + )
10K Resistor i26 ( + )
Jumper Wire j1 ( + )
Jumper Wire a1 ( - )
Jumper Wire a2 f29
Jumper Wire f25 ( - )
Jumper Wire j9 f28
Jumper Wire j10 f27
Jumper Wire a5 h2
Jumper Wire a6 h10
Jumper Wire a7 h18
Jumper Wire a8 h26
Jumper Wire ( - ) h4
Jumper Wire ( - ) h12
Jumper Wire ( - ) h20
Jumper Wire ( - ) h28

* Pins not listed are not used.

The Code

In order to make the mbed act like a USB mouse for this walkthrough, we will rely on mbed's USBDevice library. This library contains all the necessary functions to enumerate as a USB device to a computer and function as a mouse.

Libraries

Navigate to the mbed.org, login, and navigate to your Compiler.

Create a new program with the "Blinky LED Hello World" template. Name it something like "usb_device."

Navigate to the following pages and import each library into your "usb_device" program.

The mbed library should already be imported if you used the "Blinky" template.

mbed USB Device libraries

Program

Click on "main.cpp" in your project, remove the template code, and copy in the following code.

language:c
// USB Device demo - control mouse pointer with buttons

#include "mbed.h"
#include "USBMouse.h"

// USB Mouse object
USBMouse mouse;

// Define buttons
DigitalIn button_up(p5);
DigitalIn button_down(p6);
DigitalIn button_left(p7);
DigitalIn button_right(p8);

DigitalOut myled(LED1);

int main() {
    int x = 0;
    int y = 0;


    while (1) {

        // Determine mouse pointer horizontal direction
        x = button_left ^ button_right;
        if ( button_right ) {
            x = -1 * x;
        }

        // Determine mouse pointer vertical direction
        y = button_up ^ button_down;
        if ( button_down ) {
            y = -1 * y;
        }

        // Move mouse
        mouse.move(x, y);

        // Wait for next cycle
        wait(0.001);
    }
}

Run

Compile the program and copy the downloaded file to the mbed. Disconnect the USB mini-B that you used to program your mbed and connect it into the USB mini-B breakout board.

USB cable plugged into breakout board

Make sure that the other end of the USB cable is plugged into your computer and press the mbed's restart button. Your computer should tell you that a USB input device has been detected. Start pressing the four buttons on the breadboard.

mbed running as a USB mouse

Your mouse pointer should start moving around!

moving mouse pointer

Concepts

We really only covered one important new concept in this tutorial: USB devices. Instead of acting as a USB host to accept peripherals, we turned the mbed into a USB peripheral. This allowed us to plug the mbed into a computer and control some functions normally assigned to dedicated accessories (a mouse, in this case).

USB Device

A lot of things need to happen to show up as a USB device on a computer. The process of attaching a device, getting assigned a unique identifier and a driver is called "USB enumeration." Luckily, the mbed USBDevice library handles all of the device-side enumeration details for us.

Being able to enumerate as a USB device opens up a world of possibilities for us. We can make the mbed act as a mouse, a keyboard, an audio device, a mass storage device, and so on. Note that the LPC1768 only supports USB Full-Speed, which means that the higher rates of USB 2.0 and 3.0 are not available to us. If you wanted to make your own mbed Flash Drive, it would be quite slow.

If you want to get really involved in USB device development, see Jan Axelson's USB Complete book.

Going Further

Becoming a USB device lets us interact with many different computers and mobile devices. You could even make your own keyboard and mouse!

Beyond the Tutorial

  • Make the buttons act as mouse clicks instead of moving the pointer
  • Make the buttons act as keyboard keys (Hint: see USBDevice Keyboard)
  • Create a program that automatically opens up a text editor and types out a message to the user whenever the mbed is plugged in as a USB device

Digging Deeper