mbed Starter Kit Experiment Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: Shawn Hymel

Experiment 10: Hardware Soundboard

In the final tutorial of our 10-part series, we will make a hardware soundboard using our mbed. We will store some .wav files on an SD card and play one whenever a button is pressed. You could use it to interject hilarious comments into any conversation!

mbed soundboard circuit

Suggested Reading

The Circuit

This circuit can be made with parts in the SparkFun mbed Starter Kit. Also, keep in mind that the LPC1768 box contains a USB mini-B cable for programming and power.

Parts List

To follow this experiment, you would will need the following materials if you did not order the SparkFun mbed starter kit. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary. The experiment will be using 1x 330Ohm resistor.

Schematic

mbed soundboard wave player schematic

Click on schematic to view larger image.

Connections

Connect a digital-to-analog (DAC) pin of the mbed (pin 18, in this case) to a 330 Ω resistor and connect that resistor to the base of an NPN transistor (2N3904). Connect the emitter of the transistor to ground and the collector to the negative (-) side of the speaker. The positive side of the speaker should be attached to +5V (the VU pin on the mbed). Note that the +/- markings can be found on the underside of the speaker (there are no wires on the speaker like in the Fritzing diagram).

To hook up the buttons, connect one side of each pushbutton to ground and the other to pins 11, 12, 13, and 14 of the mbed.

Polarized Components Pay special attention to the component’s markings indicating how to place it on the breadboard. Polarized components can only be connected to a circuit in one direction. Polarized components are highlighted with a yellow warning triangle in the table below.

Fritzing Diagram

mbed .wav player Fritzing

Hookup Table

Place the LPC1768 in the first breadboard with pin VOUT in position i1 and pin 20 in position b20.

Connect the rest of the components as follows:

Component Breadboard 1 Breadboard 2
MicroSD Transflash Breakout* h24 (CS) h25 (DI) h26 (VCC) h27 (SCK) h28 (GND) h29 (DO)
Transistor - NPN (2N3904) c27 (E) c28 (B) c29 (C)
330 Resistor b24 b28
Pushbutton d2 d4 g2 g4
Pushbutton d7 d9 g7 g9
Pushbutton d12 d14 g12 g14
Pushbutton d17 d19 g17 g19
Speaker f25 (+) e30 (-)
Jumper Wire j1 g26
Jumper Wire a1 ( - )
Jumper Wire a5 g25
Jumper Wire a6 g29
Jumper Wire a7 g27
Jumper Wire a8 g24
Jumper Wire g28 ( - )
Jumper Wire a18 a24
Jumper Wire a27 ( - )
Jumper Wire a29 a30
Jumper Wire j2 j25
Jumper Wire a11 j2
Jumper Wire ( - ) j4
Jumper Wire a12 j7
Jumper Wire ( - ) j9
Jumper Wire a13 j12
Jumper Wire ( - ) j14
Jumper Wire a14 j17
Jumper Wire ( - ) j19

* Pins not listed are not used.

Tips

Transistor

Make sure you are using the 2N3904 transistor and not the temperature sensor! Note that the flat edge of the transistor is facing down in the Fritzing diagram.

Speaker

Notice that the speaker has the positive (+) and negative (-) pins labeled on the underside. The speaker will fit directly on the breadboard, as the Fritzing diagram has been modified to show where the speaker should be plugged in (otherwise it would cover up the rest of the components in the picture!).

Place the positive (+) terminal of the speaker into hole f25 of the breadboard and the negative (-) terminal into hole e30. The speaker will be angled across the breadboard, but it will leave enough room for wires to be plugged into j25 and a30.

pcb speaker pin labels

The Code

For our soundboard, we need to read files from an SD card, which means using the SDFileSystem again. Additionally, we want to add another library that allows us to play .wav files.

Libraries

Navigate to the mbed.org, login, and navigate to your Compiler.

Create a new program with the "Blinky LED Hello World" template. Name it something like "soundboard."

Navigate to the following pages and import each library into your "soundboard" program.

The libraries should appear in your soundboard project.

mbed soundboard libraries

Program

Click on "main.cpp" in your project, remove the template code, and copy in the following code.

language:c
// Soundboard that plays 1 of 4 .wav files stored on the SD card based on 1 of
// 4 buttons pressed

#include "mbed.h"
#include "wave_player.h"
#include "SDFileSystem.h"

// .wav files to play
const char *filenames[4] = { "/sd/good_morning.wav", 
                             "/sd/questions.wav", 
                             "/sd/lack_discipline.wav", 
                             "/sd/stop_whining.wav"};

// Define buttons
DigitalIn button_1(p11);
DigitalIn button_2(p12);
DigitalIn button_3(p13);
DigitalIn button_4(p14);

// USB serial (tx, rx)
Serial pc(USBTX, USBRX);

// SD card
SDFileSystem sd(p5, p6, p7, p8, "sd");

// Audio out (DAC)
AnalogOut       DACout(p18);
wave_player     waver(&DACout);

// Play a .wav file
int playSound(int file_num) {

    FILE *file;

    // Open sound file for reading
    file = fopen(filenames[file_num], "r");
    if ( file == NULL ) {
        error("ERROR: Could not open file for reading!\n");
        return -1;
    }

    // Play the sound file
    pc.printf("Playing sound clip %i\r\n", (file_num + 1));
    waver.play(file);

    // Reset to beginning of file and close it
    fseek(file, 0, SEEK_SET);
    fclose(file);

    return 0;
}

int main() {

    // Use internal pull-up resistors
    button_1.mode(PullUp);
    button_2.mode(PullUp);
    button_3.mode(PullUp);
    button_4.mode(PullUp);

    pc.printf("\r\nHardware Soundboard\r\n");

    while(1) {

        // Figure out which button was pressed and play that file
        if ( button_1 == 0 ) {
            playSound(0);
        }
        if ( button_2 == 0 ) {
            playSound(1);
        }
        if ( button_3 == 0 ) {
            playSound(2);
        }
        if ( button_4 == 0 ) {
            playSound(3);
        }

        // Wait 10ms before sampling the buttons again
        wait(0.01);
    }
}

Run

Insert the micro SD card into the USB to micro SD card adapter and insert the USB adapter into your computer. Copy the following .wav files to the SD's root directory:

Wave files on SD card

Remove the SD card from your computer and plug it into the breakout board on the soundboard project.

Compile the program and copy the downloaded file to the mbed. Press the mbed's reset button to start running the program. Press one of the 4 buttons to hear a sound clip!

mbed running hardware soundboard

Concepts

This project was larger than the others before it. There are a number of things going on, but most of them we covered in previous tutorials.

Amplifier

In addition to adding a speaker to play sounds, we created a very simple amplifier to increase the signal strength (and the volume). We used an NPN transistor (specifically, a 2N3904) that converts a small current through its base into a larger current through its collector. If we tried to power the speaker directly from the mbed's pin, we would likely draw enough power to hurt the processor. Audio amplifiers can be quite complex. Read more about them here.

Internal Pull-ups

When we used buttons in previous tutorials, we used external pull-up resistors on the buttons to prevent a floating pin. In order to save board space for this project, we used mbed's internal pull-ups. These are resistors internal to the mbed processor and can be enabled for each of the pins with the following line of code:

pin_name.mode(PullUp);

Going Further

In this demo, we combined many concepts to create a fun project. We made a simple amplifier to play sounds and relied on the wave_player library to read .wav files. Adding sound to a project can add a layer of interactivity and bring it to life.

Beyond the Tutorial

  • Download or create your own .wav files and play them using our soundboard. Note: you might have to use an editing program like Audacity to convert sound clips into .wav files if they do not play on the mbed.
  • Add lights! Program some LEDs to flash whenever a clip is being played.
  • You might need some extra components not found in the kit, but can you get a sound recorder to work on the mbed? (Hint: see the Simple Wave Recorder & Player library)

Digging Deeper

The End!

This demo finishes up our 10-part series on the mbed. We covered a number of topics that are considered important to embedded systems: buttons, LEDs, GPIO, ADC, DAC, interrupts, SPI, I2C, UART, etc. You had the opportunity to search for libraries on mbed.org, import them into your program, and run some basic firmware on the LPC1768. By now, you have had a good exposure to the building blocks of embedded programming on the mbed and should be ready to tackle your first project.

Make something cool! Take a picture of it and tag @sparkfun or @mbedmicro on Twitter. Or, post your project to the mbed.org Cookbook.