LilyPad Development Board Activity Guide

≡ Pages
Contributors: Gella

3: Custom Color Mixing

In this program, you will continue mixing colors with the tri-color LED, but use a new function to change the brightness of each channel in relation to each other. Adjusting the brightness of the red, green, and blue LEDs within the LED will allow you to create a new range of values and color combinations.

LilyPad Boards Used in This Activity

  • LilyPad Arduino Simple
  • LilyPad Tri-Color LED

Parts Used

New Concepts Introduced in This Activity

Analog Output (Pulse Width Modulation)

Up until this point, you have been controlling LEDs by setting them to one of two states: HIGH (ON) or LOW (OFF). This is great for blinking, but what about adjusting the brightness of your LEDs? This is where analog output comes in handy. Your LilyPad Arduino Simple can mimic a range of brightness on the LEDs by using pulse width modulation. The microcontroller on the LilyPad Arduino Simple can switch voltage to the sew tabs on and off so quickly that it appears to your eyes as if more or less voltage is being provided to an LED. For example, by changing the percent of time that a pin is on, from 0 percent (always off) to 100 percent (always on), you can create the appearance of a range of brightnesses. This percentage is called a duty cycle.

Note: You may have noticed that some of the labels on the illustrations have a special symbol in front of them (~). This indicates that these pins on the LilyPad Arduino Simple are capable of Pulse Width Modulation. However, do not include the "~" symbol in your code. It is only provided to make it easy for you to check which pins can produce PWM (analog) output and is not used in addressing the pins on the LilyPad Arduino Simple in your program. If you try to use analog output commands on a tab without these capabilities, you will see unexpected results these are illustrated in Activity 4: Fading LEDs.

Color Mixing Continued

In the last example, you created basic primary and secondary colors by turning the red, green, and blue channels on or off with different combinations. In this activity, you'll create tertiary colors by combining the three color channels at 50% brightness levels. There are actually millions of color combinations available using RGB LEDs once you begin experimenting with adjusting the brightness/saturation of each. This example will cover a set of twelve tertiary colors.

Example Code

To open the code, go to:

File > Examples > LilyPadDevelopmentBoard_ActivityGuide > LPD_03_CustomColorMixing

You can also copy and paste the following code into the Arduino IDE. Hit upload, and see what happens!

language:c
/*
LilyPad Development Board Activity 3: Custom Color Mixing
SparkFun Electronics
https://www.sparkfun.com/products/11262

Expand your color options using analogWrite and the RGB (Red Green Blue) LED

Follow the tutorial at: 
https://learn.sparkfun.com/tutorials/lilypad-development-board-activity-guide/3-custom-color-mixing

This code is released under the MIT License (http://opensource.org/licenses/MIT)

******************************************************************************/
// The LilyPad Development Board has a RGB (Red / Green / Blue) LED attached to it.
// In this activity we'll use analogWrite to control the brightness of the three LEDs.
// Here we'll create a rainbow of tertiary colors by adding a 50%-brightness option.

// Create integer variables for our LED pins:

// The built-in LED:

int RGB_red = 9;
int RGB_green = 11;
int RGB_blue = 10;


void setup() {

// Make all of our LED pins outputs:

  pinMode(RGB_red, OUTPUT);
  pinMode(RGB_green, OUTPUT);
  pinMode(RGB_blue, OUTPUT);
}

void loop()
{
  // In this code we'll step through twelve rainbow colors (primary, secondary, tertiary).

  // Unlike digitalWrite, which can be only HIGH (on) or LOW (off),
  // analogWrite lets you smoothly change the brightness from 0 (off) to 255 (fully on).
  // When analogWrite is used with the RGB LED, you can create millions of colors!

  // In the analogWrite functions:
  // 0 is off
  // 128 is halfway on (used for the tertiary colors)
  // 255 is full brightness.
  // But because this particular LED is common anode, we will need to reverse these 
  // numbers to display correctly:
  // 255 is off
  // 128 remains halfway on
  // 0 is full brightness.

  // Red

  analogWrite(RGB_red,0);
  analogWrite(RGB_green,255);
  analogWrite(RGB_blue,255);
  delay(1000);

  // Orange

  analogWrite(RGB_red,0);
  analogWrite(RGB_green,128);
  analogWrite(RGB_blue,255);
  delay(1000);

  // Yellow

  analogWrite(RGB_red,0);
  analogWrite(RGB_green,0);
  analogWrite(RGB_blue,255);
  delay(1000);

  // Chartruese

  analogWrite(RGB_red,128);
  analogWrite(RGB_green,0);
  analogWrite(RGB_blue,255);
  delay(1000);

  // Green

  analogWrite(RGB_red,255);
  analogWrite(RGB_green,0);
  analogWrite(RGB_blue,255);
  delay(1000);

  // Spring Green

  analogWrite(RGB_red,255);
  analogWrite(RGB_green,0);
  analogWrite(RGB_blue,128);
  delay(1000);

  // Cyan

  analogWrite(RGB_red,255);
  analogWrite(RGB_green,0);
  analogWrite(RGB_blue,0);
  delay(1000);

  // Azure

  analogWrite(RGB_red,255);
  analogWrite(RGB_green,128);
  analogWrite(RGB_blue,0);
  delay(1000);

  // Blue

  analogWrite(RGB_red,255);
  analogWrite(RGB_green,255);
  analogWrite(RGB_blue,0);
  delay(1000);

  // Violet

  analogWrite(RGB_red,128);
  analogWrite(RGB_green,255);
  analogWrite(RGB_blue,0);
  delay(1000);

  // Magenta

  analogWrite(RGB_red,0);
  analogWrite(RGB_green,255);
  analogWrite(RGB_blue,0);
  delay(1000);

  // Rose

  analogWrite(RGB_red,0);
  analogWrite(RGB_green,255);
  analogWrite(RGB_blue,128);
  delay(1000);
}

What You Should See

After uploading your code the RGB LED will step through a rainbow sequence of red, orange, yellow, chartruese, green, spring green, cyan, azure, blue, violet, magenta, and rose, repeatedly.

By adjusting the brightness of each LED in the RGB LED individually, we open up a much wider range of color options to display than the previous activity. In fact, there are many more combinations than we show in the example code. The image below shows a chart of the tertiary colors the example program creates by stepping down the LEDs to half brightness, creating a rainbow with more color transitions than the Basic Color Mixing example. By using analog output to adjust the brightness of each color channel individually, the RGB LED can display almost any color you can choose from a color picker - if you are familiar with RGB sliders in a graphics program, you'll recognize the 0-255 values used in this code.

Tertiary Colors

Understanding Your Program

Program Overview

  1. Display red:
    R: 100%, G: 0%, B: 0%
    Wait 1 second.
  2. Display orange:
    R: 100%, G: 50%, B: 0%
    Wait 1 second.
  3. Display yellow:
    R: 100%, G: 100%, B: 0%
    Wait 1 second.
  4. Display chartruese:
    R: 50%, G: 100%, B: 0%
    Wait 1 second.
  5. Display green:
    R: 0%, G: 100%, B: 0%
    Wait 1 second.
  6. Display spring green:
    R: 0%, G: 100%, B: 50%
    Wait 1 second.
  7. Display cyan:
    R: 0%, G: 100%, B: 100%
    Wait 1 second.
  8. Display azure:
    R: 0%, G: 50%, B: 100%
    Wait 1 second.
  9. Display blue:
    R: 0%, G: 0%, B: 100%
    Wait 1 second.
  10. Display violet:
    R: 50%, G: 0%, B: 100%
    Wait 1 second.
  11. Display magenta:
    R: 100%, G: 0%, B: 100%
    Wait 1 second.
  12. Display rose:
    R: 100%, G: 0%, B: 50%
    Wait 1 second.
  13. Repeat.

Code to Note

CodeDescription
analogWrite(RGB_red,255);
analogWrite(RGB_green,0);
analogWrite(RGB_blue,0);

Analog Write:
Notice that like digitalWrite(), the analog function takes two pieces of information - the pin it is controlling and a state to set that pin to. The analogWrite() function outputs a voltage between 0 and 3.3V on a pin, with this range divided into 255 steps, where digital output only had HIGH or LOW. This example uses three values to mix the rainbow of tertiary colors: 255 (OFF), 128 (50% brightness), and 0 (100% brightness). You can use any value between 0 and 255 when you begin to experiment with mixing your own colors.

Note that for the tri-color LED, 0 turns the LEDs on and 255 turns them off.

Coding Challenges

  • Try using a color picker to find the R, G, and B values for an interesting color and use that in your program. In order to translate them for use on the tri-color LED, you will need to do some math to reverse them.

  • Try creating your own rainbow light patterns using different values for the color mixes.