IoT Power Relay

≡ Pages
Contributors: SFUptownMaker

ESP32 Example Code

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

With Arduino installed, please make sure you also download and install the ESP32 software support package.

And lastly, download the IoT_Power_Relay GitHub repo which contains the firmware you'll be uploading to the ESP32.

Now that we have our basics, let's go over the code that will be programmed onto the ESP32!

Core Code

This is the core code, in the TeleSitter.ino main file.

The includes section holds all the library references needed for this project. time.h is the ESP32 native time library, while TimeLib.h is the Arduino time library. We use both of them because time.h does graceful NTP server synchronization, while TimeLib.h is better for tracking current time and reacting to it.

Preferences.h is the ESP32 non-volatile memory support module.

language:c
#include <WiFi.h>
#include "PageContent.h"
#include "time.h"
#include <Preferences.h>
#include "TimeLib.h"
#include "SFE_MicroOLED.h"
#include <Wire.h>

Next, we set up a few constant strings: SSID, WiFi password, and the address of the ntpServer we wish to use. "pool.ntp.org" is an open NTP project great for things like this.

language:c
const char* ssid      = "ssid_goes_here";
const char* password  = "wifi_password_goes_here";
const char* ntpServer = "pool.ntp.org";

We use global variables to track the times that we turn on and off our power switch. In the full code, there are four variables for each day. Only Monday's variables are shown here.

language:c
int mHoursOn = 8;
int mMinutesOn = 0;
int mHoursOff = 0;
int mMinutesOff = 0;

Here we set up defines for our project. We use pin 5 for controlling the switch because it has an LED on it, making testing easy. The MicroOLED library requires a reset pin to be defined, even if it isn't used, and requires a note on the status of the jumper on the back of the MicroOLED board. We leave the jumper set to '1', which is the default that it ships with.

language:c
#define CTRL_PIN 5
#define OLED_RESET 10 // Not used, but needed for initialization
#define DC_JUMPER 1   // Default value. If you didn't change the jumper
                      //  on the PCB, this is what you want.

Next we create objects that will be used throughout the code. The port number for the server is passed to the constructor; 80 is the default port for http requests and that number shouldn't be changed.

language:c
WiFiServer server(80);
MicroOLED oled(OLED_RESET, DC_JUMPER);
Preferences alarmTimes; 

setup(). Does typical setup-y things like printing debugging messages during startup, configuring the serial port and pins, etc.

language:c
void setup()
{
  Serial.begin(115200);
  pinMode(CTRL_PIN, OUTPUT);  // Also has a blue LED on the ESP32 Thing

  // We start by connecting to a WiFi network
  Serial.println();
  Serial.println();
  Serial.print("Connecting to ");
  Serial.println(ssid);

  WiFi.begin(ssid, password);

During setup, we try to connect to WiFi. It's been my experience that if the WiFi doesn't connect within 10-15 seconds, it's probably not going to, and the smartest thing to do is reset the ESP32. This section of the code handles that.

language:c
  int wifiCounter = 0;
  while (WiFi.status() != WL_CONNECTED) 
  {
    delay(500);
    Serial.print(".");
    if (++wifiCounter > 30) ESP.restart();
  }

  Serial.println("");
  Serial.println("WiFi connected.");
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());

During normal operation, we can't count on the user to have a computer attached to the ESP32. Thus, we provide the OLED to tell the user what the current IP address is.

  // Initialize the OLED and display the IP address
  oled.begin();
  oled.clear(PAGE);
  oled.setCursor(0,0);
  oled.print(WiFi.localIP());
  oled.display();

The ESP32 has an odd way of storing data in non-volatile memory. You must create a region ("TeleSitter", here), and then issue a begin() call to the library. Note that the second parameter to begin() must, per the documentation, always be false.

language:c
  // Initialize the NVM storage handler and fetch the cached
  //  alarm time information.
  alarmTimes.begin("TeleSitter", false);
  getAlarmTimes();

  // Enable the server functionality.
  server.begin();

Timekeeping initialization. Read the comments for more information on how and why the timekeeping is done the way it is.

language:c
  // We use two different timekeeping services, the ESP32 built-in
  //  and the one from the Arduino TimeLib. Why? Because the ESP32
  //  based one gets its time from an NTP server and it's unclear
  //  which functions it uses that ping the NTP server, so we want
  //  to avoid excessive NTP checks.

  // Preeeetty sure configTime() pings the NTP server. Parameters
  //  are GMT offset in seconds, DST offset in seconds, and NTP
  //  server address.
  configTime((-7*3600), 0, ntpServer);
  // A tm struct holds time info. It can be current local time, as
  //  here, or an arbitrary time, as used elsewhere.
  struct tm timeinfo;
  // Unclear as to whether getLocalTime() populates the tm struct
  //  solely from the local clock or from the NTP server. Thus, we
  //  avoid calling it too often by setting the Arduino timekeeping
  //  with it at boot time, then using the Arduino timekeeping for
  //  most of our timekeeping duties.
  getLocalTime(&timeinfo);
  // Set the Arduino library timekeeping to currrent time derived
  //  from the NTP server. We have to add 1 to the month as returned by
  //  the ESP32 module, as Arduino numbers months starting from 1 and ESP
  //  numbers starting from 0. Also, add 1900 to the year, as Arduino stores
  //  the full year number and ESP stores it as an offset from year 1900.
  setTime(timeinfo.tm_hour, timeinfo.tm_min, timeinfo.tm_sec, 
          timeinfo.tm_mday, timeinfo.tm_mon+1, timeinfo.tm_year + 1900);
  // Check to see if DST is in effect. This function relies upon
  //  having the Arduino timekeeping set. We'll repeat this check
  //  once a day at 3am and reset the Arduino clock accordingly.
  if (dstCheck()) configTime((-7*3600), 3600, ntpServer);
  else configTime((-7*3600), 0, ntpServer);
  // Fetch the current time into timeInfo again. This is now DST
  //  correct local time.
  getLocalTime(&timeinfo);
  // Set the Arduino clock to DST correct local time.
  setTime(timeinfo.tm_hour, timeinfo.tm_min, timeinfo.tm_sec, 
          timeinfo.tm_mday, timeinfo.tm_mon+1, timeinfo.tm_year + 1900);
}

loop(). Starts out by doing a health check on the WiFi connection. IF the WiFi connection is lost, the ESP32 will reboot.

language:c
void loop(){

  // Health check. If we've lost our wifi connection, restart
  //  the ESP to (hopefully) reconnect without user noticing.
  if (WiFi.status() != WL_CONNECTED) 
  {
    Serial.println("WiFi dropped; rebooting");
    delay(100);
    ESP.restart();
  }

Every pass through loop, we check our alarm status to see if we should turn the output on or off. We'll talk about what exactly is involved in the alarm checking later.

language:c
  checkAlarm();

Check if it's 0300 local time or not. If it is, we go through the clock setting process again. We only do this once a day because our clock is good enough to keep time over 24 hours fairly accurately and because we don't want to accidentally activate rate limiting on the NTP server. We do it at 0300 because that is a good time to catch the DST shift.

language:c
  if (hour() == 3 && minute() == 0 && second() == 0)
  {
    struct tm timeinfo;
    getLocalTime(&timeinfo);
    setTime(timeinfo.tm_hour, timeinfo.tm_min, timeinfo.tm_sec, 
            timeinfo.tm_mday, timeinfo.tm_mon + 1, timeinfo.tm_year + 1900);
    // Check to see if DST is in effect. 
    if (dstCheck()) configTime((-7*3600), 3600, ntpServer);
    else configTime((-7*3600), 0, ntpServer);
    getLocalTime(&timeinfo);
    setTime(timeinfo.tm_hour, timeinfo.tm_min, timeinfo.tm_sec, 
            timeinfo.tm_mday, timeinfo.tm_mon + 1, timeinfo.tm_year + 1900);
  }

This code was taken more or less directly from the example code provided with the ESP32 library. It handles incoming requests by serving up the webpage that we will create later, then checking what the nature of the request is and taking some action based on that. Note that, regardless of the request, the webpage is served back.

language:c
  WiFiClient client = server.available();   // listen for incoming clients
  if (client) {                             // if you get a client,
    Serial.println("New Client.");          // print a message out the serial port
    String currentLine = "";                // make a String to hold incoming data from the client
    while (client.connected())              // loop while the client's connected
    {            
      if (client.available())               // if there's bytes to read from the client,
      {             
        char c = client.read();             // read a byte, then
        Serial.write(c);                    // print it out the serial monitor
        if (c == '\n')                      // if the byte is a newline character
        {                    
          // if the current line is blank, you got two newline characters in a row.
          // that's the end of the client HTTP request, so send a response:
          if (currentLine.length() == 0) 
          {

We split the response into several blocks, to make editing easier, and unlike the original example, we make our webpage in constants defined elsewhere. Note the use of printf() in the body printing section. That allows us to push variables from our code to the webpage.

language:c
           client.print(pageContentHead);
            client.printf(pageContentBody, mHoursOn, mMinutesOn, mHoursOff, mMinutesOff,
                                           tHoursOn, tMinutesOn, tHoursOff, tMinutesOff,
                                           wHoursOn, wMinutesOn, wHoursOff, wMinutesOff,
                                           rHoursOn, rMinutesOn, rHoursOff, rMinutesOff,
                                           fHoursOn, fMinutesOn, fHoursOff, fMinutesOff,
                                           sHoursOn, sMinutesOn, sHoursOff, sMinutesOff,
                                           nHoursOn, nMinutesOn, nHoursOff, nMinutesOff);
            // Print out the current time and date. This is useful for debugging
            //  as it's the only way to check the internal server clock.
            client.printf("%d:%02d:%02d<br>", hour(), minute(), second());
            client.printf("%d/%d/%d %d<br>", day(), month(), year(), weekday());
            client.print(pageContentFoot);
            break;
          } 
          else                // if you got a newline, then clear currentLine:
          {    
            currentLine = "";
          }
        } 
        else if (c != '\r')   // if you got anything else but a carriage return character,
        {
          currentLine += c;      // add it to the end of the currentLine
        }

We expect to get a few types of response from the client that connects to this device. These can be differentiated by the text in the response. For instance, a request for the path reset should trigger a reset of the alarm times, and an HTTP get request that starts with a question mark indicates an incoming string of data that is to be parsed into alarm times.

language:c
        if (currentLine.endsWith("GET /reset"))
        {
          resetAlarmTimes();
        }
        if (currentLine.endsWith("HTTP/1.1"))
        {
          if (currentLine.startsWith("GET /?"))
          {
            parseIncomingString(currentLine);
            storeAlarmTimes();
          }
        }
      }
    }
    // close the connection:
    client.stop();
    Serial.println("Client Disconnected.");
  }
}

Lastly, we have a few chunks of code that don't really belong anywhere else, so we stick them at the end of the main code.

language:c
void turnOn()
{
  digitalWrite(CTRL_PIN, HIGH);
}

void turnOff()
{
  digitalWrite(CTRL_PIN, LOW);
}

void printTitle(String title, int font)
{
  int middleX = oled.getLCDWidth() / 2;
  int middleY = oled.getLCDHeight() / 2;

  oled.clear(PAGE);
  oled.setFontType(font);
  // Try to set the cursor in the middle of the screen
  oled.setCursor(middleX - (oled.getFontWidth() * (title.length()/2)),
                 middleY - (oled.getFontWidth() / 2));
  // Print the title:
  oled.print(title);
  oled.display();
  delay(1500);
  oled.clear(PAGE);
}

Alarm Handling Code

Alarms.ino handles the checking of the alarm times: whether or not the output should be turned on. It calculates the time of the day, in seconds, then calculates the times the output should be on or off depending upon the day of the week. It then does a comparison of those times and takes the appropriate action.

language:c
void checkAlarm()
    {
      int dow = weekday();
      int secsOfDay = hour()*3600 + minute()*60 + second();
      int timeOn, timeOff;
      switch(dow)
      {
        case 1: // Sundays
          timeOn = nHoursOn*3600 + nMinutesOn*60;
          timeOff = nHoursOff*3600 + nMinutesOff*60;
          break;
        case 2: // Mondays
          timeOn = mHoursOn*3600 + mMinutesOn*60;
          timeOff = mHoursOff*3600 + mMinutesOff*60;
          break;
        case 3: // Tuesdays
          timeOn = tHoursOn*3600 + tMinutesOn*60;
          timeOff = tHoursOff*3600 + tMinutesOff*60;
          break;
        case 4: // Wednesdays
          timeOn = wHoursOn*3600 + wMinutesOn*60;
          timeOff = wHoursOff*3600 + wMinutesOff*60;
          break;
        case 5: // Thursdays
          timeOn = rHoursOn*3600 + rMinutesOn*60;
          timeOff = rHoursOff*3600 + rMinutesOff*60;
          break;
        case 6: // Fridays
          timeOn = fHoursOn*3600 + fMinutesOn*60;
          timeOff = fHoursOff*3600 + fMinutesOff*60;
          break;
        case 7: // Saturdays
          timeOn = sHoursOn*3600 + sMinutesOn*60;
          timeOff = sHoursOff*3600 + sMinutesOff*60;
          break;
      }
      if (timeOn > timeOff)
      {
        if (secsOfDay > timeOn) turnOn();
        else if (secsOfDay > timeOff) turnOff();
      }
      else
      {
        if (secsOfDay > timeOff) turnOff();
        else if (secsOfDay > timeOn) turnOn();
      }
    }

Non-Volatile Memory Functionality

NVM.ino handles the various accesses to non-volatile memory that must be managed. This includes setting and resetting the alarm times and loading the alarm times into memory upon startup.

Again, I've removed redundant code for the additional days of the week to make things a little simpler to follow.

resetAlarmTimes() simply sets the on time to 0800 and the off time to 0000 and then stores it to NVM.

language:c
void resetAlarmTimes()
    {
      mHoursOn = 8;
      mMinutesOn = 0;
      mHoursOff = 0;
      mMinutesOff = 0;
      storeAlarmTimes();
    }

storeAlarmTimes() takes the current global alarm time variables and stores them into NVM. Note that storage into NVM is dependent upon data type; we use putInt() because our time data is of type int.

language:c
void storeAlarmTimes()
{
  alarmTimes.putInt("mHoursOn", mHoursOn);
  alarmTimes.putInt("mMinutesOn", mMinutesOn);
  alarmTimes.putInt("mHoursOff", mHoursOff);
  alarmTimes.putInt("mMinutesOff", mMinutesOff);
}

getAlarmTimes() is the opposite of storeAlarmTimes(). Note the use of getInt() here to correspond to putInt() earlier.

language:c
void getAlarmTimes()
{
  mHoursOn = alarmTimes.getInt("mHoursOn", 8);
  mMinutesOn = alarmTimes.getInt("mMinutesOn", 0);
  mHoursOff = alarmTimes.getInt("mHoursOff", 0);
  mMinutesOff = alarmTimes.getInt("mMinutesOff", 0);
}

Parse Input from Client

The client responds to a button press by sending a large string of values to the ESP32 Thing. We need to parse those values out into their appropriate hour and minute times. The code in ParseInput.ino does just that.

language:c
void parseIncomingString(String str)
    {
      String str0 = "mHoursOn=";
      String str1 = "&mMinutesOn=";
      mHoursOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&mHoursOff=";
      mMinutesOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&mMinutesOff=";
      mHoursOff = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&tHoursOn=";
      mMinutesOff = extractInteger(str, str0, str1);

      str0 = str1;
      str1 = "&tMinutesOn=";
      tHoursOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&tHoursOff=";
      tMinutesOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&tMinutesOff=";
      tHoursOff = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&wHoursOn=";
      tMinutesOff = extractInteger(str, str0, str1);

      str0 = str1;
      str1 = "&wMinutesOn=";
      wHoursOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&wHoursOff=";
      wMinutesOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&wMinutesOff=";
      wHoursOff = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&rHoursOn=";
      wMinutesOff = extractInteger(str, str0, str1);

      str0 = str1;
      str1 = "&rMinutesOn=";
      rHoursOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&rHoursOff=";
      rMinutesOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&rMinutesOff=";
      rHoursOff = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&fHoursOn=";
      rMinutesOff = extractInteger(str, str0, str1);

      str0 = str1;
      str1 = "&fMinutesOn=";
      fHoursOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&fHoursOff=";
      fMinutesOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&fMinutesOff=";
      fHoursOff = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&sHoursOn=";
      fMinutesOff = extractInteger(str, str0, str1);

      str0 = str1;
      str1 = "&sMinutesOn=";
      sHoursOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&sHoursOff=";
      sMinutesOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&sMinutesOff=";
      sHoursOff = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&nHoursOn=";
      sMinutesOff = extractInteger(str, str0, str1);

      str0 = str1;
      str1 = "&nMinutesOn=";
      nHoursOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&nHoursOff=";
      nMinutesOn = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = "&nMinutesOff=";
      nHoursOff = extractInteger(str, str0, str1);
      str0 = str1;
      str1 = " HTTP/1.1";
      nMinutesOff = extractInteger(str, str0, str1);
    }

    int extractInteger(String str, String sub0, String sub1)
    {
      int index0 = 0;
      int index1 = 0;
      index0 = str.indexOf(sub0) + sub0.length();
      index1 = str.indexOf(sub1);
      return str.substring(index0, index1).toInt();
    }

Check for Daylight Saving Time

In much of the world clocks are set back by one hour and forward by one hour once per year. In most of the US, this is done (forward) on the second Sunday in March and (back) on the first Sunday in November. dstCheck.ino contains code I wrote for SparkFun's Big GPS clock to automate handling of DST changes.

language:c
// This code was lifted more or less whole-hog from the SparkFun Big GPS Clock
//  project. I wrote that too.

bool dstCheck()
{
  //Serial.println("DST Check");
  // As of 2007, most of the US observes DST between the 2nd Sunday morning in
  //  March and the 1st Sunday morning in November. DST in the US changes by
  //  time zone, so at 2am local time on the 2nd Sunday in March, we increase
  //  the offset from UTC by one hour.

  // We can bail out if month is < 3 or > 11.
  if ( (month() < 3) || (month() > 11) )
  {
    return false;
  }

  // We can also bail out if month is > 3 and < 11.
  if ( (month() > 3) && (month() < 11) )
  {
    return true;
  }

  // Okay, edge cases, March and November. We can do a couple more low-math
  //  checks to quickly decide whether the date is a possible one.
  // For November, the date of the first Sunday *must* be less than 8, so if
  //  the date is greater than 8, we can return false.
  if (month() == 11)
  {
    if (day() > 7)
    {
      return false;
    }
    // Otherwise, we need to figure out whether we've seen the first Sunday
    //  yet.
    TimeElements firstOfNovTE;
    firstOfNovTE.Day = 1;
    firstOfNovTE.Month = 3;
    firstOfNovTE.Year = year();
    firstOfNovTE.Hour = 0;
    firstOfNovTE.Minute = 0;
    firstOfNovTE.Second = 0;
    time_t firstOfNov = makeTime(firstOfNovTE);
    int8_t firstDayOfNov = weekday(firstOfNov);
    int8_t firstSundayOfNov = (9 - firstDayOfNov) % 7;
    // If we *haven't* seen the first Sunday yet, we are in DST still.
    if (day() < firstSundayOfNov)
    {
      return true;
    }

    // If it's *after* the first Sunday, we aren't in DST anymore.
    if (day() > firstSundayOfNov)
    {
      return false;
    }

    // If we're here, it's the first Sunday of November right now, and we only
    //  need to know if the current hour is < 2; at 0200 MST, DST ends.
    if (hour() < 2)
    {
      return true;
    }
    return false;
  }

  // For March, dates less than 8, or greater than 13 are automatically out.
  if (month() == 3)
  {
    if (day() < 8)
    {
      return false;
    }
    if (day() > 13)
    {
      return true;
    }

    // Otherwise, we need to figure out whether we've see the second Sunday
    //  yet. 
    // TimeElements is a struct, but we have to initialize it in the long-form, due
    //  to limitations of the compiler used by the Arduino IDE.
    TimeElements firstOfMarTE;
    firstOfMarTE.Day = 1;
    firstOfMarTE.Month = 3;
    firstOfMarTE.Year = year();
    firstOfMarTE.Hour = 0;
    firstOfMarTE.Minute = 0;
    firstOfMarTE.Second = 0;
    time_t firstOfMar = makeTime(firstOfMarTE);
    int8_t firstDayOfMar = weekday(firstOfMar);
    int8_t secondSundayOfMar = ((9 - firstDayOfMar) % 7) + 7;

    // If we *haven't* seen the second Sunday yet, we aren't in DST yet.
    if (day() < secondSundayOfMar)
    {
      return false;
    }

    // If it's *after* the second Sunday, we are in DST now.
    if (day() > secondSundayOfMar)
    {
      return true;
    }

    // If we're here, it's the second Sunday of November right now, and we only
    //  need to know if the current hour is < 2; at 0200 MST, DST starts.
    if (hour() < 2)
    {
      return false;
    }
    return true;
  }
  return false; // We *should* never get here, but we need to return something
                //  or chaos ensues.
}