GNSS Correction Data Receiver (NEO-D9S) Hookup Guide

≡ Pages
Contributors: bboyho, PaulZC

Resources and Going Further

Now that you've successfully got your NEO-D9S up and running, it's time to incorporate it into your own project! Need more information? Check out some of the links below:

SparkFun Resources

u-blox Resources

If you are looking for a more integrated solution, try checking out the RTK Facet L-Band! The RTK Facet L-Band includes the NEO-D9S, ZED-F9P, and ESP32 WROOM in a sweet enclosure. Additionally, the product includes several hardware features such as a built-in LiPo battery, charging circuit, microOLED, L1/L2/L-Band antenna, microSD card socket for datalogging, fuel gauge, accelerometer, and serial ports. The build in software features also make it user friendly. It does not require copy and pasting of keys, certificates, or any other materials. By connecting the RTK Facet L-Band to a WiFi network, the keys will be automatically be updated and stored. There are also five different modes available. Everything is built into one unit and it was made to be as easy as possible to use.

SparkFun RTK Facet L-Band Hookup Guide

June 9, 2022
Setup the RTK Facet L-Band in minutes to begin gathering millimeter level geospatial coordinates.

Need some inspiration for your next project? Check out some of these related tutorials related to GNSS.

Building an Autonomous Vehicle: The Batmobile

Documenting a six-month project to race autonomous Power Wheels at the SparkFun Autonomous Vehicle Competition (AVC) in 2016.

GPS-RTK2 Hookup Guide

Get precision down to the diameter of a dime with the new ZED-F9P from u-blox.

SparkFun GPS Dead Reckoning NEO-M8U Hookup Guide

The u-blox NEO-M8U is a powerful GPS units that takes advantage of untethered dead reckoning (UDR) technology for navigation. The module provides continuous positioning for vehicles in urban environments and during complete signal loss (e.g. short tunnels and parking garages). We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!

SparkFun RTK Express Hookup Guide

Learn how to use the enclosed RTK Express product to achieve millimeter level geospatial coordinates.