GNSS Chip Antenna Hookup Guide

≡ Pages
Contributors: Nate

Introduction

GPS is common but what if you need to pack your GPS receiver into a small space such as a wearable? Standard GPS antennas are much too large to strap to your wrist so what do you do? You use one of the SparkFun GNSS Chip Antennas!

SparkFun GNSS Chip Antenna Evaluation Board

GPS-15247
Retired

The SparkFun GNSS Chip Antenna Evaluation Board makes it easy to test out various sized GPS antennas and geometries. These individual antennas can even be separated and installed permanently into a project once you select the best one for your application.

Required Materials

The GNSS Chip Antenna Evaluation Board (we’ll call it the eval board from here on out for your tongues’ sake) is possible because we have designed each antenna to have a 50-ohm microstrip. To connect, you’ll need a U.FL cable and a GPS receiver capable of connecting to a U.FL cable. You may not need everything though depending on what you have. Add it to your cart, read through the guides, and adjust the cart as necessary.

U.FL to U.FL Mini Coax Cable - 200mm

WRL-15114
$2.75

Below is a list of SparkFun GPS receivers that have a U.FL connector for its antenna. These are the easiest products to get working with the eval board.

SparkFun GPS Breakout - ZOE-M8Q (Qwiic)

GPS-15193
$50.95

SparkFun GPS Breakout - XA1110 (Qwiic)

GPS-14414
$35.95

One of the most common setups is shown below. The ZOE-M8Q has a U.FL connector and can be attached to any of the six chip-scale GPS antennas.

SparkFun Qwiic ZOE connected to the GNSS antenna eval board

Suggested Reading

If you’re unfamiliar with working with GPS receivers or U.FL connectors, be sure to checkout some of these foundational tutorials. You'll also need to check out the respective tutorials for your GPS receiver.

GPS Basics

The Global Positioning System (GPS) is an engineering marvel that we all have access to for a relatively low cost and no subscription fee. With the correct hardware and minimal effort, you can determine your position and time almost anywhere on the globe.

Three Quick Tips About Using U.FL

Quick tips regarding how to connect, protect, and disconnect U.FL connectors.

Hardware Overview

The SparkFun GNSS Chip Antenna Evaluation Board is composed of six ‘blocks’. Each one is capable of obtaining a GPS lock but the reception quality depends on the size and shape of the antenna.

SparkFun GNSS Chip Antenna Evaluation Board

Antenna Technologies

There are six different antennas on the GNSS Chip Antenna Evaluation Board.

Six highlighted antennas

You can find the datasheet and technical information for each, in order from top left to lower right:

The gain is printed on each antenna block but take this gain with a grain of salt. Antenna manufacturers tend to report the theoretical gain of an antenna, or the gain achieved from a more-than-ideal setup (i.e., using a ground plane the size of your head).

Individual Antenna Blocks

Each of the six antennas has its own U.FL connector, mounting holes, U.FL stress relief holes, and an isolated ground plane.

Single antenna block with U.FL, mounting holes, and stress relief pins highlighted

The board comes as a single unit but can be snapped apart so that any one antenna block can be mounted into a project. In theory the antennas should perform better separated but we found no measurable performance difference between the antennas as a whole or broken apart.

Antenna blocks snapped apart

U.FL Connectors and Stress Relief

U.FL connectors are generally pretty resilient but if you’ve got a particularly wearable project or harsh antenna environment, you can reinforce the U.FL connection by soldering a piece of wire over the cable to hold it in place. We recommend you do this after you’ve selected the antenna that best suits your project.

U.FL cable with attached stress relief

How Well Do the Antennas Perform?

Here’s our preliminary findings:

Antenna Name SIV[1] PDOP[2] HDOP[3]
Molex Molded 5 2.2 1
W3011 9 1.47 0.69
W3062A 6 2.48 1.16
Molex Chip 5 2.27 1.18
Molex Cube 10 1.16 0.63
TE Puck 9 1.27 0.68
Molex Flexible[4] 10 1.14 0.62


1 - Satellites in view: The number of satellites an antenna was able to detect after 60 seconds of searching. Higher is generally better.

2 - Position Dilution of Precision: The accuracy of the 3D solution being output by the receiver. A lower number is better. Meaning of numbers can be found on Wikipedia.

3 - Horizontal Dilution of Precision: The accuracy of the horizontal location solution being output by the receiver. A lower number is better. Meaning of numbers can be found on Wikipedia.

4 - The Flexible Adhesive GPS Antenna is not on the GNSS Chip Antenna Evaluation Board but performed impressively.

These results are provided for illustration only. Testing was done using a Ublox ZED-F9P on the RTK2 with 60 seconds to obtain satellites from a cold start. Your results will vary greatly based on how clear your view is of the sky, where you are located, and the type of GPS receiver used.

As you can see, the larger antennas tend to pick up more satellites. The interesting outliers are the flexible antenna (arguably the largest of all the antennas) and the Pulse W3011 (arguably one of the smallest, best performing antennas).

FAQ and Troubleshooting

What’s the Difference Between GPS and GNSS?

GPS refers to the collection of satellites put into space by the USA. Other countries have their own collection of navigation satellites include Russia (their constellation is called GLONASS), the EU (Galileo), and China (BeiDou). GNSS refers to all navigation constellations as a whole. The GNSS Chip Antenna Evaluation Board is capable of receiving signals from any GPS/GLONASS/BeiDou/Galileo satellite transmitting on band 1 (the most common civilian frequency). If your GPS receiver was purchased after 2015 it will probably be capable of picking up most GNSS satellites.

I’m Not Getting a Lock?!

Are you outside? Do you have a clear, unobstructed view of the sky? These antennas are small and require a very clear view of the sky. They can not get a lock indoors.

Have you moved outside and are still having problems? Double check that your U.FL connections are seated nicely and orthogonal. You should feel a nice click when the connector is seated properly. Be sure to checkout our tutorial on using U.FL connectors for more info.

Three Quick Tips About Using U.FL

December 28, 2018
Quick tips regarding how to connect, protect, and disconnect U.FL connectors.

Resources and Going Further

We hope you have fun experimenting with your chip antennas. We find the variance in design and geometries fascinating as is the art of antenna design. Remember, all our designs are open source so you are welcome to use the footprints and layouts from our board in your own design. That’s the real power of this eval board - try out various antennas and if you like one you can implement it in your own tiny GPS receiver design!

For more information, check out the resources below:

Be sure to check out some of the other tutorials we have around GPS:

Alphanumeric GPS Wall Clock

This is a GPS controlled clock - a clock you truly never have to set! Using GPS and some formulas, we figure out what day of the week and if we are in or out of daylight savings time.

What is GPS RTK?

Learn about the latest generation of GPS and GNSS receivers to get 14mm positional accuracy!

Basic Autonomous Kit for Sphero RVR Assembly Guide

Get your Basic Autonomous Kit for Sphero RVR all hooked up with this guide!

SparkFun GPS Dead Reckoning NEO-M8U Hookup Guide

The u-blox NEO-M8U is a powerful GPS units that takes advantage of untethered dead reckoning (UDR) technology for navigation. The module provides continuous positioning for vehicles in urban environments and during complete signal loss (e.g. short tunnels and parking garages). We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!