GNSS Correction Data Receiver (NEO-D9S) Hookup Guide

≡ Pages
Contributors: bboyho, PaulZC

Arduino Library Overview

We will be highlighting a few parts of the SparkFun u-blox Arduino GNSS Library below for the NEO-D9S and the ZED-F9P.

NEO-D9S Configuration

The first step is to declare the SFE_UBLOX_GNSS object. Like most Arduino sketches, this is done at a global scope (after the include file declaration), not within the setup() or loop() functions.

language:c
#include <SparkFun_u-blox_GNSS_v3.h> //http://librarymanager/All#SparkFun_u-blox_GNSS_v3
SFE_UBLOX_GNSS myLBand; // NEO-D9S

Within setup() we then need to start (initialize) communiation with the NEO-D9S. The NEO-D9S has a default I2C address of 0x43 and so we need to provide that when calling the begin method:

language:c
Wire.begin(); //Start I2C

while (myLBand.begin(Wire, 0x43) == false) //Connect to the u-blox NEO-D9S using Wire port. The D9S default I2C address is 0x43 (not 0x42)
{
    Serial.println(F("u-blox NEO-D9S not detected at default I2C address. Please check wiring."));
    delay(2000);
}
Serial.println(F("u-blox NEO-D9S connected"));

The NEO-D9S needs to be configured so it can receive the PointPerfect correction stream. The configuration items are:

Configuration item Default value
CFG-PMP-CENTER_FREQUENCY 1539812500 Hz
CFG-PMP-SEARCH_WINDOW 2200 Hz
CFG-PMP-USE_SERVICE_ID 1 (true)
CFG-PMP-SERVICE_ID 50821
CFG-PMP-DATA_RATE 2400 (B2400) bps
CFG-PMP-USE_DESCRAMBLER 1 (true)
CFG-PMP-DESCRAMBLER_INIT 23560
CFG-PMP-USE_PRESCRAMBLING 0 (false)
CFG-PMP-UNIQUE_WORD 0xe15ae893e15ae893

The centre frequency varies depending on which satellite is broadcasting corrections for your geographical area.

The up-to-date frequencies are distributed via the MQTT /pp/frequencies/Lb topic. At the time of writing, they are (in MHz):

language:c
{
  "frequencies": {
    "us": {
      "current": {
        "value": "1556.29"
      }
    }
  }
}

We can add that to the code as follows:

language:c
const uint32_t myLBandFreq = 1556290000; // Uncomment this line to use the US SPARTN 1.8 service

The code to configure the NEO-D9S is as follows. Note that the UBLOX_CFG_PMP_USE_SERVICE_ID, UBLOX_CFG_PMP_SERVICE_ID and UBLOX_CFG_PMP_DESCRAMBLER_INIT also need to be changed.

language:c
  uint8_t ok = myLBand.setVal32(UBLOX_CFG_PMP_CENTER_FREQUENCY,   myLBandFreq); // Default 1539812500 Hz
  if (ok) ok = myLBand.setVal16(UBLOX_CFG_PMP_SEARCH_WINDOW,      2200);        // Default 2200 Hz
  if (ok) ok = myLBand.setVal8(UBLOX_CFG_PMP_USE_SERVICE_ID,      0);           // Default 1 
  if (ok) ok = myLBand.setVal16(UBLOX_CFG_PMP_SERVICE_ID,         21845);       // Default 50821
  if (ok) ok = myLBand.setVal16(UBLOX_CFG_PMP_DATA_RATE,          2400);        // Default 2400 bps
  if (ok) ok = myLBand.setVal8(UBLOX_CFG_PMP_USE_DESCRAMBLER,     1);           // Default 1
  if (ok) ok = myLBand.setVal16(UBLOX_CFG_PMP_DESCRAMBLER_INIT,   26969);       // Default 23560
  if (ok) ok = myLBand.setVal8(UBLOX_CFG_PMP_USE_PRESCRAMBLING,   0);           // Default 0
  if (ok) ok = myLBand.setVal64(UBLOX_CFG_PMP_UNIQUE_WORD,        16238547128276412563ull); // 0xE15AE893E15AE893

Finally, we need to ensure that the communication port is set correctly. Let's configure the UART2 port. In order to do that, we need to:

  • Change the baud rate to 38400 - to match the ZED-F9P's baud rate
  • Ensure that the UBX protocol is enabled for output on UART2
  • Enable the RXM PMP message on UART2
    • The RXM PMP message contains the SPARTN correction data in UBX format
  • Perform a restart (software reset) so that the NEO-D9S starts using the new configuration items

Of course, you could set the NEO-D9S to output the correction data to the other communication ports as well (e.g. in the Arduino Library, correction data was sent via the I2C, UART1, and UART2 ports for example 19). The sample code below configures the NEO-D9S module's UART2 port to pass the correction data.

language:c
  if (ok) ok = myLBand.setVal32(UBLOX_CFG_UART2_BAUDRATE,          38400); // match baudrate with ZED default
  if (ok) ok = myLBand.setVal8(UBLOX_CFG_UART2OUTPROT_UBX,         1);     // Enable UBX output on UART2
  if (ok) ok = myLBand.setVal8(UBLOX_CFG_MSGOUT_UBX_RXM_PMP_UART2, 1);     // Output UBX-RXM-PMP on UART2

  Serial.print(F("L-Band configuration: "));
  if (ok)
    Serial.println(F("OK"));
  else
    Serial.println(F("NOT OK!"));

  myLBand.softwareResetGNSSOnly(); // Do a restart

Once the NEO-D9S has aquired the signal from the satellite, it will start outputting PMP correction messages to the ZED-F9P on UART2.

ZED-F9P Configuration

We need to declare a second SFE_UBLOX_GNSS object for the ZED-F9P. Again, this is done at a global scope (after the include file declaration), not within the setup() or loop() functions.

language:c
SFE_UBLOX_GNSS myGNSS; // ZED-F9P

Within setup() we need to start (initialize) communication with the ZED-F9P:

language:c
  while (myGNSS.begin() == false) //Connect to the u-blox module using Wire port and the default I2C address (0x42)
  {
    Serial.println(F("u-blox GNSS module not detected at default I2C address. Please check wiring."));
    delay(2000);
  }
  Serial.println(F("u-blox GNSS module connected"));

We then need to:

  • Make sure the ZED-F9P's UART2 port is configured to accept the PMP correction data
  • Tell the ZED-F9P to use FIXED carrier solutions when possible (this is the default setting)
  • Tell the ZED-F9P to accept L-band PMP as a correction source

The sample code below configures the ZED-F9P module's UART2 port to accept correction data. Again, you could use the other communication ports as well. Just make sure that the communication ports match the settings that were configured on the NEO-D9S.

language:c
          ok = myGNSS.setUART2Input(COM_TYPE_UBX | COM_TYPE_NMEA | COM_TYPE_SPARTN); //Be sure SPARTN input is enabled
  if (ok) ok = myGNSS.setDGNSSConfiguration(SFE_UBLOX_DGNSS_MODE_FIXED); // Set the differential mode - ambiguities are fixed whenever possible
  if (ok) ok = myGNSS.setVal8(UBLOX_CFG_SPARTN_USE_SOURCE, 1); // use LBAND PMP message

The final piece of the puzzle is to provide the ZED-F9P with the keys it needs to decrypt the encrypted SPARTN (PMP) corrections.

The ZED-F9P can hold two dynamic keys: the current key; and the next key. We also need to tell it when each key is valid from, so it knows when to switch to the next key.

You can find the current and next keys in the Location Services \ Location Things \ Thing Details \ Credentials tab in Thingstream:

L-band Dynamic Keys

PointPerfect L-band dynamic keys. (Click to enlarge)

The ZED-F9P actually needs to know when the keys are valid from, rather than when they expire. Each key is valid for four weeks, so we need to work backwards 4 weeks from the expiry date.

The current key expires at midnight (UTC) at the end of Friday, September 23rd, 2022. This means it became valid 4 weeks earlier at midnight (UTC) on August 27th:

Current Dynamic Key Valid 4 Weeks from Expiry Date Next Dynamic Key Valid from Expiry Date

Dynamic Key: Expiry and Valid From dates. (Click to enlarge)

Using the website recommended in the u-blox Application Note:

we can see that the key became valid during GPS week 2224, at time-of-week 518400.

We can use the Arduino Library setDynamicSPARTNKey method to configure a single key:

language:c
  if (ok) ok = myGNSS.setDynamicSPARTNKey(16, 2224, 518400, "500--------------------------177");

  Serial.print(F("GNSS: configuration "));
  if (ok)
    Serial.println(F("OK"));
  else
    Serial.println(F("NOT OK!"));

Alternately, we can set both the current key and the next key together using setDynamicSPARTNKeys. The next key becomes valid during GPS week 2228:

language:c
  if (ok) ok = myGNSS.setDynamicSPARTNKeys(16, 2224, 518400, "500--------------------------177", 16, 2228, 518400, "582--------------------------a7d");

The keys can also be retrieved using MQTT. We have an Arduino Library example which shows how to retrieve the keys from the L-band + IP key distribution topic /pp/ubx/0236/Lb. That topic provides the keys in UBX (binary) format, ready to be pushed to the ZED.

The keys are also available in human-readable JSON format from the MQTT topic /pp/key/Lb . But note that that topic provides the valid from in Unix epoch format, in milliseconds, excluding the 18 leap seconds since GPS time started!

language:c
{
  "dynamickeys": {
    "current": {
      "start": "1661558382000",
      "duration": "2419199999",
      "value": "500--------------------------177"
    },
    "next": {
      "start": "1663977582000",
      "duration": "2419199999",
      "value": "582--------------------------a7d"
    }
  }
}