Getting Started with the SparkFun Blynk Board

≡ Pages
Contributors: jimblom

RGB Status Codes

During setup, the RGB LED on the Blynk Board will be your window into its soul. The board uses this multi-colored LED to indicate all sorts of status modes. If you're ever unclear of what the RGB color-code means, consult the table below:

RGB ColorBlink SpeedStatusNotes
Purple●Medium (2Hz)Device connected to Blynk BoardVerifies that your phone (or possibly someone else's) is connected to the Blynk Board.
Blue●Fast (4Hz)Connecting to Wi-Fi networkAfter sending it the info, the Blynk Board will attempt to connect to your Wi-Fi network for up to 30 seconds.
Blynk Green●Slow (1Hz)Connecting to Blynk CloudAfter connecting to your Wi-Fi network, the Blynk Board will establish a connection with the Blynk server.
Blynk Green●Smoothly fading in/outConnected to BlynkAfter successfully connecting to Wi-Fi and Blynk, this is the sign that everything is working! The LED will continue to "breathe" until you tell it to do something else.
Yellow●Slow (1Hz)Re-connecting to BlynkConnection issues should resolve themselves, but the Blynk board will likely be unresponsive while blinking yellow. If it continues to Blynk yellow for over a minute, try cycling power to the Blynk Board.
White●Medium (2Hz)Blynk Board waiting for configIf your Blynk Board was unable to connect to either Wi-Fi or Blynk, it'll sit in this mode – waiting for you to press a button. More on this in the Reconfiguring a Blynk Board section