Getting Started with the DA16200 FreeRTOS SDK

≡ Pages
Contributors: santaimpersonator

Software Setup

Note: The minimum system requirements for the DA16200 FreeRTOS SDK are: *For more information on the required software, please refer to the DA16200 FreeRTOS Getting Started Guide.

Users should have already familiarized themselves with the DA16200 FreeRTOS Getting Started Guide. While a majority of the information in this section is already covered in the DA16200 FreeRTOS Getting Started Guide, we have included a few additional details specific to the DA16200 boards in our catalog. Below, are a complete set of instructions for users to download, install, and setup the various programs required for the DA16200 FreeRTOS SDK.

Serial-to-UART Driver

Depending on the board and/or adapter being utilized, users will need to install the appropriate driver for their computer to recognize the serial-to-UART chip on their board/adapter. Most of the latest operating systems will recognize serial-to-UART chip on the board and automatically install the required driver.

To manually install the CH340 driver on their computer, users can download it from the WCH website. For more information, check out our How to Install CH340 Drivers Tutorial.

How to Install CH340 Drivers

August 6, 2019
How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.

Terminal Emulator (with Y-Modem)

In order to program their board through the USB-C connection and access the serial debug interface, users will need a serial terminal installed on their computer. We have verified that these emulators, below, support Y-Modem to upload the SDK bootloader and firmware. Users are welcome to use their preferred serial terminal, but we will only provide support with these applications for this tutorial.

Once installed, users will need to configure the serial terminal with the following settings for the COM port they are utilizing:

  • Baud Rate: 230400 bps
  • Data Bits: 8 (8-N-1)
  • Parity: None
  • Stop Bits: 1
  • Flow Control (HW/SW): None

Download the DA16200 FreeRTOS SDK Image

In order to utilize the DA16200 FreeRTOS SDK, users should to program their board with the latest DA16200 FreeRTOS SDK firmware. To download the DA16200 FreeRTOS SDK Image, users will need to register an account first. Then, from the Design & Development tab of the DA16200MOD product page, users can download the:

  • DA16200 DA16600 FreeRTOS SDK Image v3.2.4.0 (8.47 MB) 08/17/2022
  • There are two firmware images for the DA16200 FreeRTOS SDK:
    • FBOOT is the bootloader image which is used to initialize the DA16200 and launch the main firmware.
      • File Name: DA16200_FBOOT-GEN01-01-XXXXXXXXX_W25Q32JW.img
      • The bootloader image must be the first thing loaded into flash for a new device.
      • Since the bootloader image contains SFDP (flash specific) information, the bootloader must be loaded into flash before other images are loaded.
      • When the SDK is updated, always load the bootloader image first.
    • FRTOS is the main firmware image which includes the RTOS and user applications.
      • File Name: DA16200_FRTOS-GEN01-01-XXXXXXXXX-XXXXXX.img

Download firmware
Download the latest DA16200 FreeRTOS SDK firmware from the DA16200MOD product page. (Click to enlarge)

Download the DA16200 FreeRTOS SDK

Note: The Windows operating system has a path length limitation of 260 characters. Therefore, it is recommended that users extract the SDK into the root directory of the disk drive and rename the folder (i.e. C:/dialog_sdk).

To download the DA16200 FreeRTOS SDK, users will need to register an account first. Then, from the Design & Development tab of the DA16200MOD product page, users can download the:

Download SDK
Download the latest DA16200 FreeRTOS SDK from the DA16200MOD product page. (Click to enlarge)

For more information on the content of the DA16200 FreeRTOS SDK (i.e. file organization, API, example applications, etc.), please refer to the DA16200 FreeRTOS SDK Programmer Guide.

xPack Project Manager

Note: A recent version of Node.js (12.x or later) is required to install the following software.

Users will need to install the xPack Project Manager (xpm), to install the following xPack development tools required to utilize the SDK. Follow the instructions on the xPack website to install the software.

To install the xPack Project Manager (xpm) through Node.js, open a Windows command line or a Linux terminal and enter the following command:

language:bash
npm install --global xpm@latest

GCC Toolchain

In order to compile the code from the SDK, users will need to install the GNU Arm GCC (v10.2.1) cross compiler.

This development tool can be installed as an xPack package through the xPack Project Manager. Once users have installed the xpm, from the section above, open a Windows command line or a Linux terminal and enter the following command:

language:bash
xpm install --global @xpack-dev-tools/arm-none-eabi-gcc@10.2.1-1.1.2

Windows Build Tools

Note: Only for Windows operating systems.

Windows does not include any build tools (i.e. make) by default; therefore, users should install the Windows Build Tools xPack package.

This development tool can be installed as an xPack package through the xPack Project Manager. Once users have installed the xpm, from the section above, open a Windows command line and enter the following command:

language:bash
xpm install --global @xpack-dev-tools/windows-build-tools

Install and Setup Eclipse

The Eclipse IDE (integrated development environment) is a free and open source development platform that is released under the Eclipse Public License (EPL). The Eclipse IDE will be used to import the DA16200 FreeRTOS SDK into a workspace and build/compile the example projects using xPack development tools.

For more documentation on the Eclipse IDE, please refer to the resources below:

Installation

Installation of the Eclipse IDE is simple:

  1. Download the installer for the Eclipse IDE. (Users can also download the installation software from the Download or Getting Started pages.)
  2. Run the downloaded executable to launch the Eclipse Installer.

    • On Linux platforms, use the following commands to extract and execute to Eclipse Installer:

      language:bash
      tar -xvzf eclipse-inst-jre-linux64.tar.gz
      cd eclipse-installer
      ./eclipse-inst
      
    • Select the Eclipse IDE for Embedded C/C++ Developers from the installation options.
      installation options
      Installation menu from Eclipse Installer. (Click to enlarge)
  3. Select the program's installation location and accept the software agreements.

Configuration

The first time users launch the Eclipse IDE, they be prompted to select a folder for the program's workspace. However, before users can proceed to working on a project, they will need to setup DA16200 FreeRTOS SDK and link the xPack development tools.

Configure the Development Tools:

In order to build the DA16200 FreeRTOS SDK, users will need to configure the Eclipse IDE and link the necessary development tools.

  • To setup the GCC Toolchain, users need to provide the file path to the compiler:
    1. Open the Window > Preferences dialog box.
      open the preferences dialog box
      Open the Preferences dialog box from the Window drop down menu. (Click to enlarge)
    2. In the preferences dialog, select MCU > Global Arm Toolchain Paths and verify the Toolchain folder points to the where the GNU Arm GCC 10.2.1 toolchain is installed.
      compiler file path
      Link the compiler to the GCC toolchain. (Click to enlarge)
      • If the GNU Arm GCC 10.2.1 xPack was installed, users should find it with a file path similar to the following:
        • C:/Users/<username>/AppData/Roaming/xPacks/@xpack-dev-tools/arm-none-eabi-gcc/<gcc version>/.content/bin
      • If the toolchain folder is empty or incorrect, press the xPack button and select the correct Version.
        verify xPack version
        Verify the xPack version. (Click to enlarge)
  • To setup the build tool (i.e. make; only on Windows), users need to provide the file path to the build tool:
    1. Open the Window > Preferences dialog box.
      open the preferences dialog box
      Open the Preferences dialog box from the Windows drop down menu. (Click to enlarge)
    2. In the preferences dialog, check the MCU > Global Build Tools path and verify it points to where the Windows Build Tools xPack has been installed.
      build tools file path
      Link the Windows build tools to the Eclipse IDE. (Click to enlarge)
      • If the Windows Build Tools xPack was installed, users should find it with a file path similar to the following:
        • C:/Users/<username>/AppData/Roaming/xPacks/@xpack-dev-tools/windows-build-tools/<Window Build Tools version>/.content/bin

Import the DA16200 FreeRTOS SDK:

Note: The Windows operating system has a path length limitation of 260 characters. The <sdk_root_directory> path length must be less than 70 characters.

Users will also need to import the DA16200 FreeRTOS SDK into the Eclipse IDE:

  1. Download the DA16200 FreeRTOS SDK. (Users will need to register an account.)
  2. Extract the SDK zip file; this directory of this folder will be known as the <sdk_root_directory>.

    • The Windows operating system has a path length limitation of 260 characters. Therefore, the <sdk_root_directory> path length must be less than 70 characters.
      • We recommended that users extract the SDK into the root directory of a disk drive and rename the folder to shorten the file path length (i.e. C:/dialog_sdk).
        root directory example
        An example of a shortened <sdk_root_directory> file path. (Click to enlarge)
    • For Linux systems, certain files used during the build process need to be set as executable. After extracting the SDK files, the <sdk_root_directory>/tools/util file permissions must be changed by running the set_linux_perm.sh script in that directory:

      language:bash
      cd <sdk_root_diretory>/tools/util
      chmod 755 set_linux_perm.sh
      sh ./set_linux_perm.sh
      
  3. To setup the SDK in Eclipse, the top-level project contained in the <sdk_root_directory> should be imported. This will provide a view into the full SDK source code and will set up the launch and debug configurations required by the SDK.
    • Under the File menu select Import
      open import dialog box
      Open the Import dialog box from the Files drop down menu. (Click to enlarge)
    • In the Import dialog box, select General > Existing Projects into Workspace and press the Next button.
      import dialog box
      Select the Existing Projects into Workspace option. (Click to enlarge)
    • In the Import dialog box, select the Select root directory option and press the Browse button.
      select root directory option to import project
      Select the Select root directory option. (Click to enlarge)
    • Use the file manager to navigate to the <sdk_root_directory> directory and then press the Select Folder button.
      select folder for SDK
      Select the folder of the the <sdk_root_directory>. (Click to enlarge)
    • A project should appear in the Projects list which matches the name of the <sdk_root_directory>. Select that project and then press the Finish button.
      select project
      Select the project from the list. (Click to enlarge)
    • The project will appear in the Eclipse Project Explorer.
      SDK in project explorer
      The DA16200 FreeRTOS SDK imported into the Eclipse Project Explorer. (Click to enlarge)

Segger J-Link Software

Note: In order to program and debug the DA16200MOD, a J-Link Lite (or higher) programmer is required. Users may also be interested in these J-Link programmers and accessories.


Straight Header - Male (PTH, 0.05in., 2x5-Pin)

PRT-15362
$1.95

J-Link EDU Mini Programmer

PGM-15345
Retired

J-Link BASE Compact Programmer

PGM-15347
Retired
JTAG 20 Pin 0.1 In. To 10 Pin 0.05 In. Adapter

JTAG 20 Pin 0.1 In. To 10 Pin 0.05 In. Adapter

PGM-18421
Retired

For a comparison of the different J-Link programmer models, please refer to the Segger website.

Below are the minimum requirements to setup the J-Link programmer to be used in the Eclipse IDE for the DA16200 FreeRTOS SDK:

In order to use the J-Link flash loader with the DA16200MOD, users will need to add it to the J-Link software:

  1. With the J-Link software already installed, find the installation directory and locate the JLinkDevices.xml file.
    • Example: C:\Program Files (x86)\SEGGER\JLink\JLinkDevices.xml
  2. Open JLinkDevices.xml in a text editor and add device entries for the DA16200 to the <DataBase> section as follows:

    language:xml
    <DataBase>
    <!-- ->
    <!-- Dialog Semiconductor ->
    <!-- ->
    <Device>
     <ChipInfo Vendor="Dialog Semiconductor" Name="DA16200_W25Q32JW" Core="JLINK_CORE_CORTEX_M4"
    WorkRAMAddr="0x80000" WorkRAMSize="0x00040000" />
     <FlashBankInfo Name="QSPI Flash" BaseAddr="0x100000" MaxSize="0x400000"
    Loader="Devices/Dialog/DA16200_W25Q32JW.elf" LoaderType="FLASH_ALGO_TYPE_OPEN" />
    </Device>
    <Device>
     <ChipInfo Vendor="Dialog Semiconductor" Name="DA16200.SeggerES.4MB" Core="JLINK_CORE_CORTEX_M4" WorkRAMAddr="0x83000" WorkRAMSize="0x00020000" />
     <FlashBankInfo Name="QSPI Flash" BaseAddr="0x10000000" MaxSize="0x400000" Loader="Devices/Dialog/ES_DA16200_4MB.elf" LoaderType="FLASH_ALGO_TYPE_OPEN" />
    </Device>
    <Device>
     <ChipInfo Vendor="Dialog Semiconductor" Name="DA16200.SeggerES.2MB" Core="JLINK_CORE_CORTEX_M4" WorkRAMAddr="0x83000" WorkRAMSize="0x00020000" />
     <FlashBankInfo Name="QSPI Flash" BaseAddr="0x10000000" MaxSize="0x200000" Loader="Devices/Dialog/ES_DA16200_2MB.elf" LoaderType="FLASH_ALGO_TYPE_OPEN" />
    </Device>
    <Device>
     <ChipInfo Vendor="Dialog Semiconductor" Name="DA16200.eclipse.4MB" Core="JLINK_CORE_CORTEX_M4" WorkRAMAddr="0x83000" WorkRAMSize="0x00020000" />
     <FlashBankInfo Name="QSPI Flash" BaseAddr="0x10000000" MaxSize="0x400000" Loader="Devices/Dialog/DA16200_4MB.elf" LoaderType="FLASH_ALGO_TYPE_OPEN" />
    </Device>
    <Device>
     <ChipInfo Vendor="Dialog Semiconductor" Name="DA16200.eclipse.2MB" Core="JLINK_CORE_CORTEX_M4" WorkRAMAddr="0x83000" WorkRAMSize="0x00020000" />
     <FlashBankInfo Name="QSPI Flash" BaseAddr="0x10000000" MaxSize="0x200000" Loader="Devices/Dialog/DA16200_2MB.elf" LoaderType="FLASH_ALGO_TYPE_OPEN" />
    </Device>
    </DataBase>
    

    add new devices
    Device entries added to the JLinkDevices.xml file. (Click to enlarge)

  3. Copy the flash loader files from the <sdk_root_directory>/utility/j-link/scripts/flashloader/Devices/Dialog directory into the directory where the JLinkDevices.xml is located.
    flash loader files
    Flash loader files in the C:\Program Files (x86)\SEGGER\JLink\Devices\Dialog directory. (Click to enlarge)
  4. Configure the file path of the J-Link software in the Eclipse IDE
    1. In the Eclipse IDE, open the Window > Preferences dialog box.
      open preferences window
      Open the Preferences dialog box from the Window drop down menu in the Eclipse IDE. (Click to enlarge)
    2. In the preferences dialog box, select Run/Debug > String Substitution and press the New button.
      String Substitution menu
      Create a new variable. (Click to enlarge)
    3. Enter jlink_path as the variable name and set the value as the file path to the J-Link software:
      • C:\Program Files (x86)\SEGGER\JLink
      • C:\Users\<USER>\AppData\Roaming\SEGGER\JLinkDevices
        new variable
        Add the jlink_path variable linking to the J-Link software. (Click to enlarge)
    4. Click the OK and then the Apply and Close buttons to save the setting.

Note: If users are having trouble locating the flash loader files or modifying the JLinkDevices.xml file, please feel free to utilize this archived version of the files. These files are meant to be used with:

  • DA16200 FreeRTOS SDK v3.2.4.0
  • J-Link v7.80b
Download Archived Files (ZIP)

Follow the instructions below, to utilize the archived files:

  1. Extract the archived files from the j-link_files.zip zip folder.
  2. Replace the JLinkDevices.xml file in the C:\Program Files (x86)\SEGGER\JLink directory with the extracted file.
  3. Add the flash loader files by moving the extracted Dialog folder into the C:\Program Files (x86)\SEGGER\JLink\Devices directory.

Once the users have linked the J-Link software to the Eclipse IDE, they will need to import the j-link project to provide an absolute path for the SDK scripts to use. The project can be imported using the Eclipse Project Explorer by navigating to the <sdk_top_directory>/utility/j-link/project/ and then right click on that directory and select Import as Project.

import j-link scripts
Importing the J-Link scripts. (Click to enlarge)

For more information on utilizing J-Link with the DA16200 FreeRTOS SDK, please refer to the instructions in the <sdk_root_directory>\utility\j-link\scripts\ReadMe.txt file.