Getting Started with the DA16200 FreeRTOS SDK

≡ Pages
Contributors: santaimpersonator

Example: I2C

In the DA16200 FreeRTOS SDK, there is an I2C example project (apps > common > examples > Peripheral > I2C) that will write to and read from an EEPROM. This project is compatible with the Qwiic EEPROM. Below are the prebuilt images for the I2C example project, using version 3.2.4.0 of the SDK:

Build Project

After users have imported and built the project from the SDK, they can connect the Qwiic EEPROM and program their board. (No code modifications are necessary for this example project.)

harware connection
The Qwiic EEPROM connected to the DA16200 Thing Plus. (Click to enlarge)

If connected properly, users should see a success message in the serial debug interface after the FRTOS image has been uploaded. The DA16200MOD will write 32 bytes to the EEPROM and then read the EEPROM to verify the data. The success message is displayed upon verification of the data.

success message
The success message of the example project in the serial debug interface. (Click to enlarge)