Audio Codec Breakout - WM8960 Hookup Guide

≡ Pages
Contributors: QCPete, bboyho

Hardware Hookup

There are a number of ways to connect to the input and output pins of the WM8960. We will go over each .

Soldering

Header pins were left off the Audio Codec Breakout to allow users the flexibility of connecting any type of 0.1"-spaced header to the board. Depending on your connections, you may need to solder additional breakout boards and adapters. For temporary connections to the I/O pins, you could use IC hooks to test out the pins. However, you'll need to solder headers or wires of your choice to the board for a secure connection. For the scope of this tutorial, we will be soldering male header pins on the board and wiring the circuit on a breadboard. Here are a few tutorials to connect to the pads depending on your personal preference.

How to Solder: Through-Hole Soldering

September 19, 2013
This tutorial covers everything you need to know about through-hole soldering.

Working with Wire

February 8, 2013
How to strip, crimp, and work with wire.

Power

To power the WM8960 appropriately, you will just need to provide power to VIN and the 3V3 pins. As stated in the Hardware Overview: Power, you can take advantage of your development board's voltages without adjusting jumpers. We recommend making the following connection listed in the table.

Audio Codec - WM8960 IoT RedBoard - ESP32
VIN 5V
GND GND
(Additional Ground, optional)
Qwiic Cable's 3.3V pin
(or 3.3V)
Qwiic Cable's 3.3V pin
(or 3.3V)
Qwiic Cable's GND pin
(or GND)
Qwiic Cable's GND pin
(or GND)

Using wires and the Qwiic cable to power VIN and 3V3, your circuit should look similar to the circuit diagram below. We will use this method to power the audio codec for the proceeding circuit diagrams.

Power Input and Power from Qwiic Cable

Depending on your setup, you could provide a separate input voltage to the SPKVDD and VDD. Just make sure to adjust the jumpers on the back as necessary.

Qwiic and I2C

To configure the I2S settings or signal path, you will need to connect to the I2C port. Users can save some time wiring this part of the circuit up by adding a Qwiic cable between the audio codec breakout and the IoT RedBoard ESP32. As an alternative, users could also solder to the PTH as well. We recommend making the following connection listed in the table.

Audio Codec - WM8960 IoT RedBoard - ESP32
Qwiic Cable's SCL pin
(or SCL)
Qwiic Cable's SCL pin
(or SCL)
Qwiic Cable's SDA pin
(or SDA)
Qwiic Cable's SDA pin
(or SDA)
Qwiic Cable's 3.3V pin
(or 3.3V)
Qwiic Cable's 3.3V pin
(or 3.3V)
Qwiic Cable's GND pin
(or GND)
Qwiic Cable's GND pin
(or GND)

Surprise! Your connection is basically the same as the circuit diagram in the previous section. We just highlighted the circuit connection for I2C data and clock lines here.

Power and I2C

Line Input 3

The following connection is for a line level input 3. For simplicity, the table does not include the power and I2C pins.

Audio Codec - WM8960 TRS Connector
LINPUT3 Tip
RINPUT3 Ring
GND Sleeve

Your circuit should look similar to the circuit diagram below.

Power, I2C, and Line Input 3

Line Input 2

The following connection is for a line level input 2. For simplicity, the table does not include the power and I2C pins.

Audio Codec - WM8960 TRS Connector
LINPUT2 Tip
RINPUT2 Ring
GND Sleeve

Your circuit should look similar to the circuit diagram below.

Power, I2C, and Line Input 2

Line Input 1

The following connection is for a line level input 1. For simplicity, the table does not include the power and I2C pins.

Audio Codec - WM8960 TRS Connector
LINPUT1 Tip
RINPUT1 Ring
GND Sleeve

Your circuit should look similar to the circuit diagram below.

Power, I2C, and Line Input 1

I2S Passthrough

The following connection is for passing an audio source through the ADC and immediately back to the DAC. For simplicity, the table does not include the power and I2C pins. Note that this is for setting the codec as a I2S peripheral.

Audio Codec - WM8960 IoT RedBoard - ESP32
DACDAT 4
BCLK 16
ADCDAT 17
DACLRC 25
ADCLRC 25

Your circuit should look similar to the circuit diagram below.

Power, I2C, and I2S Passthrough

I2S Decoder

The following connection is for decoding audio. One example is if users connect an audio Bluetooth® device (such as your phone or laptop) to the ESP32 and stream music wirelessly. For simplicity, the table does not include the power and I2C pins. Note that this is for setting the codec as a I2S peripheral.

Audio Codec - WM8960 IoT RedBoard - ESP32
DACDAT 4
BCLK 16
DACLRC 25

Your circuit should look similar to the circuit diagram below.

Power, I2C, and I2S Decoder

Differential Microphone Input

The following connection is for connecting differential microphones to the audio codec. When using a pseudo-differential microphone configuration, make sure to include a 2.2kΩ resistor between the MICBIAS and the + terminals of each differential microphone. You will also need to set voltage on the MICBIAS pin. For simplicity, the table does not include the power and I2C pins.

Audio Codec - WM8960 Resistor Electret Microphone
GND Left Mic -
LINPUT1 Left Mic -
LINPUT2 Left Mic +
MICBIAS 2.2kΩ Right Mic +
GND Right Mic -
LINPUT1 Right Mic -
LINPUT2 Right Mic +
MICBIAS 2.2kΩ Right Mic +

Your circuit should look similar to the circuit diagram below.

Psuedo-Differential Microphone Configuration

Single Ended Microphone Input

The following connection is for connecting single ended microphones to the audio codec. Instead of using a line level input from the TRS connector, users can also connect unbalanced microphones (these are usually microphones with an amplifier on the breakout boards and have one audio output pin) to the left and right pins of INPUT1. Make sure to also connect power and GND to the boards. For simplicity, the table does not include the power and I2C pins between the ESP32 and WM8960.

Audio Codec - WM8960 Single Ended Microphone (Left) Single Ended Microphone (Right) IoT RedBoard - ESP32
Qwiic Cable's
GND pin
(or GND)
GND GND GND
LINPUT1 AUD
RINPUT1 AUD
Qwiic Cable's
3.3V pin
(or 3.3V)
3.3V 3.3V 3.3V

Your circuit should look similar to the circuit diagram below.

Single Ended Microphone Circuit

Headphone Output

Based on the recommended output configuration from the datasheet, we will be using a capless headphone output in this tutorial.

alt text

Recommended headphone output configuration from the WM8960 Datasheet (v4.2) on page 41.

The following connection is for connecting headphones to the audio codec's headphone output. For simplicity, the table does not include the power and I2C pins.

Audio Codec - WM8960 TRS Connector
HPL Tip
HPR Ring
OUT3 Sleeve

Power, I2C, and Headphone Output

Differential Speaker Output

There are a few recommended speaker output configurations from the datasheet to minimize the speaker connection losses due to series resistance and EMI. For a basic setup, we will be using a short wire connection between the audio codec's breakout board and each differential speaker. For those that require long exposed track and want to go the extra mile, users can build an LC filter circuit, add ferrite beads, or shield the wires using PCB ground plane (or Vdd).

alt text

Recommended speaker output configuration from the WM8960 Datasheet (v4.2) on page 88.

The following connection is for connecting speakers to the audio codec's speaker output channels. For simplicity, the table does not include the power and I2C pins.

Audio Codec - WM8960 Speakers
SL+ Speaker Left +
SL- Speaker Left -
SR+ Speaker Right +
SR+ Speaker Right -

Power, I2C, and Speakers