Audio Codec Breakout - WM8960 Hookup Guide

≡ Pages
Contributors: QCPete, bboyho

Example 11: Volume Plotter

This example is similar to example 3. However, we will be connecting to reading I2S audio from the ADC and plotting the audio samples on the Arduino Serial Plotter.

Hardware Hookup

Connect power, I2C, I2S, line input 1, and the headphone output. Your circuit should look similar to the circuit diagram below.

alt text

If you have not already, insert a USB cable into your IoT RedBoard ESP32 and a TRS cable from your audio source (e.g. MP3 player, smartphone, or computer) into the audio connector. Then connect your headphones to the output. For those that are sensitive to sounds, you may want to hear the example output before inserting the headphones into your ears.

Upload Code

From the menu, select the following: File > Examples > SparkFun WM8960 Arduino Library > Example_11_VolumePlotter. If you have not already, select your Board (in this case the SparkFun ESP32 IoT RedBoard), and associated COM port. Then hit the upload button.

Open the Arduino Serial Plotter and set it to 115200 baud to view the output. Then hit the play button on your audio source. Make sure that the volume from the audio source is turned up. You should hear some music from the headphones and view the audio samples on the Serial Plotter.