ReconBot with the Tessel 2

≡ Pages
Contributors: rwaldron

Resources and Going Further

For some extra fun, you could implement the following.

  • Instead of relying on an existing Wireless LAN, use the Tessel 2's built-in Access Point support. Remember that your control device will have to connect to the Tessel 2's Access Point network in order to access the controller application in the browser.
  • Deploy your software to the Tessel 2's flash memory with the following command:

    t2 push index.js

this way your program will be automatically started when the Tessel 2 boots.

You can find all the files for the Reconbot at the GitHub repository.

For more Tessel fun, check out these other great SparkFun tutorials.

Experiment Guide for the Johnny-Five Inventor's Kit

Use the Tessel 2 and the Johnny Five Inventors kit to explore the world of JavaScript enabled hardware through 14 awesome experiments!

Environmental Monitoring with the Tessel 2

Build an air-conditioner monitoring device to collect environment information and store it in the cloud.

Sunrise Machine with the Tessel 2

Are you to sleepy to enjoy a sunrise on a brisk morning? Yeah...us too! No worries, with a Webcam, a Tessel 2 and a bit of code you can sleep in and catch the sunrise at your leisure with the Sunrise Machine.