Qwiic Kit for Raspberry Pi V2 Hookup Guide

≡ Pages
Contributors: M-Short, bboyho

Hardware Overview

Revision Changes: With the revision from the initial release of the the SparkFun Qwiic Starter Kit for Raspberry Pi, we have swapped out an individual board inside the kit, listed below. At the time of writing we used the Qwiic pHAT v1.0. The Qwiic pHAT v2.0 is functionally the same with additional features. Unfortunately, the CCS811 is EOL so the Environmental Combo Breakout CCS811/BME280 was removed from V2. Thus, a similar sensor (SGP40) was added. Since the BME280 is also broken out on the Atmospheric Sensor Breakout, it was also included in the kit.

Qwiic Kit for Raspberry Pi Kit SKU Revision History
KIT-21285 - Add Air Quality Sensor SGP40 (Qwiic).
- Add Environmental Sensor Breakout - BME280 (Qwiic)
- Add Additional Qwiic Cable
- Remove Environmental Combo Breakout (CCS811/BME280).
- Kit version number bumped up to V2.
KIT-16841 - Switch to Qwiic pHAT v2.0
KIT-15367 - Initial release with the Qwiic pHAT
Please refer to the following pictures if you are unsure.

KIT-21285 KIT-16841 KIT-21285
KIT-21285 KIT-16841 KIT-15367

The hardware we are using for this kit (other than the Pi) is the Qwiic pHAT V2.0 which provides a Qwiic connector to your Raspberry Pi. This enables you to easily connect a variety of Qwiic-enabled Devices easily such as the Proximity Sensor Breakout- VCNL4040, Atmospheric Sensor Breakout - BME280, Air Quality Sensor - SGP40, and Qwiic micro OLED breakout.

Proximity and Light Sensor (VCNL4040) Temperature, Humidity, and Barometric Pressure Sensor (BME280)  Air Quality Sensor (SGP40) MicroOLED Display
Proximity and Light Sensor
(VCNL4040)
Temperature, Humidity, and Barometric Pressure Sensor
(BME280)
Air Quality Sensor
(SGP40)
MicroOLED Display