Qwiic Digital Desk Sign with MicroMod

≡ Pages
Contributors: bboyho

Arduino Example Code

Note: If this is your first time using Arduino IDE or board add-on, please review the following tutorials.

The example code can be found in the following GitHub repository. The example includes the original host keyboard code from Arduino. The code was modified to work with a 20x4 SerLCD and eventually the 16x2. To save power and the screen, the code was further modified to be used with the Qwiic PIR motion sensor in order to toggle the RGB LED and screen. For the scope of this project tutorial, we will be using examples 1b and 2.

Arduino SAMD Board Add-Ons

Since we are using the SAMD51, you will need to install the board add-on. Head over to the tutorial for instructions on installing the board definitions.

MicroMod SAMD51 Processor Board Hookup Guide

October 21, 2020
This tutorial covers the basic functionality of the MicroMod SAMD51 and highlights the features of the ARM Cortex-M4F development board.

Additional Libraries

If you are using the Qwiic PIR motion sensor, make sure to download and install the library as stated in its tutorial.

Qwiic PIR Hookup Guide

March 25, 2021
Get started passively monitoring motion using the Panasonic EKMC and EKMB sensors with the SparkFun Qwiic PIR.

The Arduino Library Manager is the easiest way to install the library. Open the Library Manager, search for "SparkFun Qwiic PIR Arduino Library" and click the "Install" button to download the latest version. If you prefer manually installing the library from the GitHub repository, you can download it here: