Qwiic Digital Desk Sign with MicroMod

≡ Pages
Contributors: bboyho

Resources and Going Further

For more information, check out the resources below regarding this project!

Looking for more inspiration related to USB host? Try switching out the MicroMod SAMD51 Processor with another processor board that is capable of USB host. Of course, you'll need to check the processor's specifications and hookup guide to see if the feature is available. To name a few, the Teensy, STM32, and RP2040 are capable of USB host. However, you'll need to adjust the code with the USB host library depending on the processor board. Or try using mbed's USB host library with the mbed Starter Kit!

MicroMod Teensy Processor Hookup Guide

Add the processing power and versatility of the Teensy to your MicroMod project following this guide for the SparkFun MicroMod Teensy Processor.

MicroMod RP2040 Processor Board Hookup Guide

This tutorial covers the basic functionality of the MicroMod RP2040 Processor Board and highlights the features of the dual-core ARM Cortex-M0+ processors development board. Get started with the first microcontroller from the Raspberry Pi Foundation!

MicroMod STM32 Processor Hookup Guide

Get started with the MicroMod Ecosystem and the STM32 Processor Board!