Qwiic Digital Desk Sign with MicroMod

≡ Pages
Contributors: bboyho

Hardware Assembly

If you have not already, make sure to check out the Getting Started with MicroMod: Hardware Hookup for information on inserting your Processor Board to your Carrier Board.

Getting Started with MicroMod

October 21, 2020
Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

Your board should look like the image below after connecting the MicroMod SAMD51 Processor Board to the MicroMod ATP. To program, insert the USB-C cable.

Processor Board inserted into Carrier Board

Since the SAMD51 uses the USB connector for USB host, we'll strip and solder wires to the board to connect an external 5V wall adapter.

Solder Wire to 5V and GND

Then we'll strip the other end of the wires and insert them into a female barrel jack adapters with "+" to VIN and "−" to GND. We'll secure the wires by twisting them together.

Wires Inserted into Barrel Jack with Screw Terminals

Due to the design of the MicroMod SAMD51's host pins, we'll need to solder another USB Type A connector breakout to the ATP's host pins using male headers. If you have an adapter to convert the USB Type C to Type A, you can also use that as well.

Solder Header Pins to USB Breakout Board

While I could solder the breakout directly to the ATP's host pins, I decided to solder female headers to the board to be able to easily disconnect the USB keyboard.

Solder Female Header Pins to ATP Carrier Board's USB Pins

Add a Qwiic cable between the Qwiic SerLCD and MicroMod's Qwiic connector labeled as I2C

Qwiic Cable Between ATP Carrier Board and 20x4 RGB Character LCD

Insert a keyboard to the USB breakout board.

Insert Keyboard into USB breakout board

When you have finished programming the SAMD51, you can insert a 5V wall adapter for power.

5V Wall Adapter connected to Barrel Jack for Power

To save power and the screen, you can also add a PIR motion sensor or distance sensor to toggle the screen on and off. An additional Qwiic cable and Qwiic PIR motion sensor was added between the MicroMod ATP and Qwiic SerLCD.

Qwiic PIR Motion Sensor Added to Setup

The 20x40 SerLCD was hard to see any messages with it flat on a table so a panel was eventually cut out from a SparkFun cardboard box to mount the project. for the scope of this tutorial, won't go over the specifics of cutting the cardboard in this tutorial or mounting the electronics to the panel.

Cardboard panel to mount the electronics