MicroMod Single Pair Ethernet Function Board - ADIN1110 Hookup Guide

≡ Pages
Contributors: QCPete, El Duderino

Introduction

The SparkFun MicroMod Single Pair Ethernet Function Board - ADIN1110 introduces 10Base-T1L Single Pair Ethernet protocol into the SparkFun MicroMod ecosystem. Using the ADIN1110 Ethernet transceiver from Analog Devices Inc., this Function Board provides a development tool for long-range, 10Mb/s single-pair 10BASE-T1L Ethernet applications. The 10BASE-T1L Ethernet supported by the ADIN1110 is compatible with the 802.3cg IEEE® standard, supports high bandwidth up to 10Mb/s and can send and receive data on connections over 1 kilometer long! We also have the MicroMod Single Pair Ethernet Kit that includes nearly everything you need to get started prototyping a MicroMod Single Pair Ethernet connection. Just make sure to grab a pair of MicroMod Processor Boards.

SparkFun MicroMod Single Pair Ethernet Function Board - ADIN1110

COM-19038
$49.95 $26.47

SparkFun MicroMod Single Pair Ethernet Kit

KIT-24804
Retired

In this guide we'll cover the basics of 10BASE-T1L Single-Pair Ethernet (SPE), what to expect from the ADIN1110 and other hardware present on this Function Board, how to assemble a SPE circuit and use it with our ADIN1110 Arduino Library.

Required Materials

The following materials are necessary for following along with this guide. All Function Boards require a Main Board and Processor to connect to each other. Depending on your application, you may need a Single or Dual Main Board:

SparkFun MicroMod Main Board - Single

DEV-20748
$18.50

SparkFun MicroMod Main Board - Double

DEV-20595
$22.95

A Processor Board is needed to act as a host controller for the Function Board:

SparkFun MicroMod Teensy Processor

DEV-16402
$24.95

SparkFun MicroMod ESP32 Processor

WRL-16781
$19.95

SparkFun MicroMod SAMD51 Processor

DEV-16791
Retired

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

Finally, a Single Pair Ethernet cable is required to connect the two MicroMod assemblies to each other:

Single Pair Ethernet Cable - 0.5m (Shielded)

CAB-19312
$21.75
Single Pair Ethernet Cable - 20m (Shielded)

Single Pair Ethernet Cable - 20m (Shielded)

CAB-19364
Retired

Suggested Reading

The MicroMod ecosystem is a unique way to allow users to customize their project to their needs. If you aren't familiar with the MicroMod system, click on the banner below for more information.

MicroMod Logo


You may also want to read the tutorials below if you are not familiar with the concepts covered in them:

Serial Peripheral Interface (SPI)

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.

What is an Arduino?

What is this 'Arduino' thing anyway? This tutorials dives into what an Arduino is and along with Arduino projects and widgets.

Installing Arduino IDE

A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

Getting Started with MicroMod

Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!