MicroMod Single Pair Ethernet Function Board - ADIN1110 Hookup Guide

≡ Pages
Contributors: QCPete, El Duderino

Troubleshooting

Here are a couple of quick troubleshooting tips to use if you run into issues creating a link between ADIN1110's.

Check Board/Library Versions

If you have any issues with the Arduino Library and a SparkFun MicroMod Processor, make sure you have the latest versions of both the Processor Board definitions and the Arduino Library.

Reset Sequence

If the boards do not establish a link when running the example sets from the Arduino library, hold the RESET buttons on the Main Boards down at the same time. Release the RESET button on the receiving board (eg. the LCD circuit for the demo example) first and then release the RESET button on the transmitting after.

General Troubleshooting