MicroMod Single Pair Ethernet Function Board - ADIN1110 Hookup Guide

≡ Pages
Contributors: QCPete, El Duderino

Software Setup

Note: This library assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino or if you need a refresher, please review the following tutorials.

SparkFun ADIN1110 Arduino Library

The SparkFun ADIN1110 Arduino Library includes several examples to get started communicating between two ADIN1110 Function Boards. The library is hosted on GitHub. Install the library through the Arduino Library Manager tool by searching for "SparkFun ADIN1110 Arduino Library". Users who prefer to manually install it can grab it from the repository or download it directly by clicking the button below:

The SparkFun ADIN1110 Arduino Library includes a wide set of examples to demonstrate different ways to configure and use the ADIN1110. They include basic examples to get up and running as well as advanced examples for users who prefer to customize the performance and memory use in transmissions.

Processor Arduino Board Definitions and Driver

Make sure you go through the Hookup Guide for your chosen Processor Board to install the latest Arduino board definitions and any necessary drivers:

MicroMod ESP32 Processor Board Hookup Guide

October 21, 2020
A short hookup guide to get started with the SparkFun MicroMod ESP32 Processor Board.

MicroMod STM32 Processor Hookup Guide

May 13, 2021
Get started with the MicroMod Ecosystem and the STM32 Processor Board!

MicroMod Teensy Processor Hookup Guide

July 1, 2021
Add the processing power and versatility of the Teensy to your MicroMod project following this guide for the SparkFun MicroMod Teensy Processor.

Pin Connection Table

The table below helps show which pins the Function Board connects to depending on the slot it is connected to on a Main Board (Note: The Single Main Board connection is Slot 0):

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Function Board
Pin Name
I/O
Direction
Main Board's
Processor Pin
Slot 0 Slot 1
VCC Input -
3.3V Input -
GND - -
INT D0 D1
CS CS0 CS1