Getting Started with MicroPython and the SparkFun Inventor's Kit for micro:bit

≡ Pages
Contributors: LightningHawk

Experiment 4: Driving an RGB LED

Introduction

You know what’s even more fun than a blinking LED? Changing colors with one LED! In this circuit you’ll learn how to use an RGB LED to create unique color combinations. Depending on how bright each diode is, nearly any color is possible!

Parts Needed

You will need the following parts:

  • 1x Breadboard
  • 1x micro:bit
  • 1x micro:bit Breakout with Headers
  • 1x micro-b USB Cable
  • 1x Common Cathode RGB LED
  • 3x 100Ω Resistors
  • 5x Jumper Wires

Didn't Get the SIK for micro:bit?

If you are conducting this experiment and didn't get the Inventor's Kit, we suggest using these parts:

Jumper Wires - Connected 6" (M/M, 20 pack)

PRT-12795
$2.95

micro:bit v2 Board

DEV-17287
$16.50

Breadboard - Self-Adhesive (White)

PRT-12002
$6.25

LED - RGB Diffused Common Cathode

COM-09264
$2.30

SparkFun Qwiic micro:bit Breakout (with Headers)

BOB-16446
$6.25

USB Micro-B Cable - 6 Foot

CAB-10215
$6.50

Suggested Reading

Before continuing with this experiment, we recommend you be familiar with the concepts in the following tutorial:

Pulse Width Modulation

February 27, 2013
An introduction to the concept of Pulse Width Modulation.

Introducing the Red/Green/Blue (RGB) LED

RGB Diffused Common Cathode LED

The Red/Green/Blue (RGB) LED is three LEDs in one. The RGB has four pins with each of the three shorter pins controlling an individual color: red, green or blue. The longer pin of the RGB is the common ground pin. You can create a custom-colored LED by turning different colors on and off to combine them. For example, if you turn on the red pin and green pin, the RGB will light up as yellow.

But which pin is which color? Pick up the RGB so that the longest pin (common ground) is aligned to the left as shown in the graphic below. The pins are Red, Ground, Green and Blue --- starting from the far left.

RGB LED pinout

Note: When wiring the RGB, each colored pin still needs a current-limiting resistor in line with the micro:bit's I/O pin that you plan to use to control it, as with any standard LED.

Hardware Hookup

Ready to start hooking everything up? Check out the wiring diagram and hookup table below to see how everything is connected.

Polarized Components Pay special attention to the component’s markings indicating how to place it on the breadboard. Polarized components can only be connected to a circuit in one direction.

Wiring Diagram for the Experiment

Fritzing Diagram

Having a hard time seeing the circuit? Click on the wiring diagram for a closer look.

Run Your Script

Let's drive an RGB LED. Type (or copy) the program into your Mu editor, or download all the programs from this GitHub Repository and open the Ex4_drivingRGB.py program. Save it, then click the Flash icon to program your micro:bit.

language:python
# SparkFun Electronics
# Experiment 4.0
# Driving an RGB LED

from microbit import *
from random import randint

redVal = randint(0, 255)
greenVal = 0
blueVal = 0

while True:
    if button_a.is_pressed():
        redVal = 0
        blueVal = 0
        greenVal = randint(0, 255)
        pin0.write_analog(redVal)
        pin1.write_analog(greenVal)
        pin2.write_analog(blueVal)
    elif button_b.is_pressed():
        redVal = 0
        blueVal = randint(0, 255)
        greenVal = 0
        pin0.write_analog(redVal)
        pin1.write_analog(greenVal)
        pin2.write_analog(blueVal)
    else:
        pin0.write_analog(redVal)
        pin1.write_analog(greenVal)
        pin2.write_analog(blueVal)

code image for drivingRGB

Code to Note

Using the random module

MicroPython comes with a random module to introduce a little unknown into your programs. There are a few ways you can use the random module beyond using it as a random number generator the way it is used in this experiment. To see the documentation, read the official docs on the random module.

In this experiment we are using random to generate a random number between 0 and 255

button_a.is_pressed() and button_b.is_pressed()

button_a and button_b represent the left and right buttons on the micro:bit respectively. There are three built-in functions that can be attached to button_a or button_b:

  • is_pressed() --- Will return True if the button specified is pressed. If the specified button is not pressed, it will return False.
  • was_pressed() --- Will return True or False depending on whether the specified button was pressed since start-up or since the last time this statement (method) was called.
  • get_pressed() --- Will return the number of times the specified button has been pressed since the device started or since the last time the statement (method) was used. Once the method is used, it will reset to zero.

elif

The elif statement lets you check for multiple expressions that might be True. In this experiment we want to do different things whether button A pressed is True or button B pressed is True.

What You Should See

You should see your LED turn on red. If you press the A button on the micro:bit, the color will change to green, and if you press the B button, the color will change to blue. Try modifying the code to mix all three colors and display a white.

Exp 4 RGB LED

Troubleshooting

LED Remains Dark or Shows Incorrect Color

With the four pins of the LED so close together, it’s sometimes easy to misplace one. Double check that each pin is where it should be.

Seeing Red

The red diode within the RGB LED may be a bit brighter than the other two. To make your colors more balanced, use a higher ohm resistor.