Getting Started with MicroPython and the SparkFun Inventor's Kit for micro:bit

≡ Pages
Contributors: LightningHawk

Experiment 2: Reading a Potentiometer

Introduction

In this circuit you will work with a potentiometer. You will learn how to use a potentiometer to control the brightness of an LED by reading a sensor and storing its 0--1023 value as a variable, then using it as a brightness level for the LED.

Parts Needed

You will need the following parts:

  • 1x Breadboard
  • 1x micro:bit
  • 1x micro:bit Breakout with Headers
  • 1x micro-b USB Cable
  • 1x LED
  • 1x 100Ω Resistor
  • 7x Jumper Wires
  • 1x 10kΩ Potentiometer

Didn't Get the SIK for micro:bit?

If you are conducting this experiment and didn't get the Inventor's Kit, we suggest using these parts:

Jumper Wires - Connected 6" (M/M, 20 pack)

PRT-12795
$2.95

Trimpot 10K Ohm with Knob

COM-09806
$1.25

micro:bit v2 Board

DEV-17287
$16.50

Breadboard - Self-Adhesive (White)

PRT-12002
$6.25

SparkFun Qwiic micro:bit Breakout (with Headers)

BOB-16446
$6.25

USB Micro-B Cable - 6 Foot

CAB-10215
$6.50

LED - Basic Red 5mm

COM-09590
$0.50

Resistor 100 Ohm 1/4 Watt PTH - 20 pack (Thick Leads)

PRT-14493
$1.50

Suggested Reading

Before continuing with this experiment, we recommend you be familiar with the concepts in the following tutorial:

Analog to Digital Conversion

February 7, 2013
The world is analog. Use analog to digital conversion to help digital devices interpret the world.

Introducing the Potentiometer

Potentiometer next to Quarter

A potentiometer is a resistance-based analog sensor that changes its internal resistance based on the rotation of its knob. The potentiometer has an internal voltage divider enabling you to read the change in voltage on the center pin with a microcontroller (the micro:bit). To hook up the potentiometer, attach the two outside pins to a supply voltage (5V in this circuit) and ground. It doesn’t matter which is connected where, as long as one is connected to power, and the other to ground. The center pin is then connected to an analog input pin so the micro:bit can measure the change in voltage. When you twist the knob, the sensor reading will change!

Note: The potentiometer included in the kit has three marks on it that will help you figure out which breadboard rows the pins are plugged into.

Hardware Hookup

Ready to start hooking everything up? Check out the wiring diagram and hookup table below to see how everything is connected.

Polarized Components Pay special attention to the component’s markings indicating how to place it on the breadboard. Polarized components can only be connected to a circuit in one direction.

Wiring Diagram for the Experiment

alt text

Having a hard time seeing the circuit? Click on the wiring diagram for a closer look.

Note: The full-sized breadboard power rails have a break down the middle. If you end up using the lower half of the power rail, you will need to jump between the upper end and lower end.

Running Your Script

Let's read a potentiometer and control the brightness of an LED. Type (or copy) the program into your Mu editor, or download all the programs from this GitHub Repository and open the Ex2_readPot.py program. Save it, then click the Flash icon to program your micro:bit.

language:python
# SparkFun Electronics
# Experiment 2.0
# Reading a Potentiometer

from microbit import *

while True:
    potVal = pin2.read_analog()
    pin0.write_analog(potVal)
    sleep(25)

code for reading a pot

Code to Note

pin2.read_analog()

In this program you are reading the voltage from the potentiometer, which is 0 to 3.3 volts on pin 2. The micro:bit reads that value as a 10-bit number, which is a value range from 0 to 1023 using the call pin2.read_analog(). We are saving that number to a variable called potVal.

pin0.write_analog()

As with the analog read, the analog write deals with a range of values, but instead of reading a pin as an input, the line pin0.write_analog() outputs an analog value to a pin. We see this as a brightness range with this LED, but it could be a tone from a buzzer, a motor speed, etc. We set our analog output to the variable we stored the potentiometer value in.

A “variable” is a placeholder for values that may change in your code. You can create a variable by simply typing a name and setting it equal to what you want. Python is a dynamically typed language. This means the type of variable is determined at runtime. So you do not need to worry about declaring your variable type.

What You Should See

You should twist the potentiometer. You will notice that the LED will get brighter or dimmer based on the position of the potentiometer. If you turn the potentiometer all the way one direction, it will be fully on, and the other end will be fully off.

LED Dimmer with Potentiometer

Troubleshooting

Sporadically Working

This is most likely due to a slightly dodgy connection with the potentiometer's pins. This can usually be conquered by holding the potentiometer down or moving the potentiometer circuit somewhere else on your breadboard.

Not Working

Make sure you haven’t accidentally connected the wiper (center pin), the resistive element in the potentiometer, to a wrong pin!

LED Not Lighting Up

LEDs will only work in one direction. Double check your connections.