1W LoRa MicroMod Function Board Hookup Guide

≡ Pages
Contributors: Nate, santaimpersonator

Introduction

Frequency Operation

This LoRa module can only be used in the 915MHz LoRaWAN frequency band (i.e. 902 to 928 MHz). It is not compatible with other frequency bands; double check the frequency band used in your region. Check out these resources from The Things Network for an unofficial summary of regional radio regulations and list of the regional frequency plans.

The 1W LoRa MicroMod Function Board adds LoRa capabilities to your MicroMod project. It is intended to be used in conjunction with a MicroMod processor board and a MicroMod main board, which provides the electrical interface between a processor board and the function board(s).

SparkFun MicroMod LoRa Function Board

WRL-18573
Retired

Match up the board's M.2 edge connector to the slot of the M.2 connector and secure the function board with the screws provided with the main board.

Utilizing the 915M30S LoRa module from EBYTE, which is a 1W (30dBm) transceiver based around the SX1276 from Semtech. There is a robust edge mount RP-SMA connector for large LoRa (915MHz) antennas; with modification, a U.FL connector is also available. We've successfully tested a 12 miles line-of-sight transmission with this module (user results may vary).

With the MicroMod standardization, users no longer need to cross-reference schematics with datasheets, while fumbling around with jumper wires. Simply, match up the function board's M.2 edge connector to the slot of the M.2 connector on the main board and secure the function board with screws. All connections are hardwired to compatible pins of the processor board and the pin connections are standardized for the processor boards.

Required Materials

To get started, users will need a few of the items listed below. (You may already have a some of these items; read through the guide and modify your cart accordingly.)

MicroMod Processor Board

A processor board is required for the MicroMod system to operate. Users can choose a processor board, based upon their needs, to attach to the MicroMod M.2 connector of the main board. Below, are few options:

SparkFun MicroMod ESP32 Processor

WRL-16781
$19.95

SparkFun MicroMod mikroBUS Starter Kit

KIT-19935
$79.95 $59.95

SparkFun MicroMod STM32 Processor

DEV-21326
$20.50

SparkFun Arduino IoT Weather Station

KIT-22636
$129.95

MicroMod Main Board

A main board provides the electrical connections between the function and processor boards to operate. Users can choose a main board based upon their needs. Below, are few options:

SparkFun MicroMod Main Board - Double

DEV-20595
$22.95

SparkFun MicroMod Main Board - Single

DEV-20748
$18.50

Required Hardware

A Phillips screw driver is necessary to attach the processor board and function board(s) to the main board. Additionally, a USB-C cable is needed to connect the main board to a computer. The LoRa function board also requires a LoRa antenna for the transceiver to operate.

SparkFun Mini Screwdriver

TOL-09146
$1.50

USB 3.1 Cable A to C - 3 Foot

CAB-14743
$7.95

Below, is a selection of our 915MHz frequency band RP-SMA antennas.

915MHz LoRa Antenna RP-SMA - 1/2 Wave 2dBi

WRL-14876
$21.95

915MHz LoRa Antenna RP-SMA - 1/4 Wave 2dBi

WRL-14875
$18.95

Pycom LoRa and Sigfox Antenna Kit - 915MHz

WRL-14676
Retired

Optional Hardware

A LoRa gateway provides internet connection for LoRaWAN network. Below are a few options from our LoRa product category.

LoRa Raspberry Pi 4 Gateway with Enclosure

WRL-16447
Retired

Nebra Indoor HNT Hotspot Miner (915MHz)

WRL-17843
Retired

Nebra Outdoor HNT Hotspot Miner (915MHz)

WRL-17844
Retired

Users can also use other LoRa boards for peer-to-peer communication. Below are a few options from our LoRa product category.

SparkFun LoRa Thing Plus - expLoRaBLE

WRL-17506
$54.95

SparkFun Pro RF - LoRa, 915MHz (SAMD21)

WRL-15836
$36.95

915MHz LoRa Antenna RP-SMA - 1/4 Wave 2dBi

WRL-14875
$18.95

Interface Cable RP-SMA to U.FL - 100mm

WRL-00662
$3.50

To modify the jumpers, users will need soldering equipment and/or a knife.

Solder Lead Free - 100-gram Spool

TOL-09325
$24.95

Chip Quik No-Clean Flux Pen - 10mL

TOL-14579
$8.50

Hobby Knife

TOL-09200
$3.75

Weller WLC100 Soldering Station

TOL-14228
Retired

Suggested Reading

The MicroMod ecosystem is a unique way to allow users to customize their project to their needs. Click on the banner below for more information.

MicroMod Logo


For users who aren't familiar with the following concepts, we also recommend reading the following tutorials before continuing.

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

Serial Peripheral Interface (SPI)

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.

Pulse Width Modulation

An introduction to the concept of Pulse Width Modulation.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Analog vs. Digital

This tutorial covers the concept of analog and digital signals, as they relate to electronics.

Processor Interrupts with Arduino

What is an interrupt? In a nutshell, there is a method by which a processor can execute its normal program while continuously monitoring for some kind of event, or interrupt. There are two types of interrupts: hardware and software interrupts. For the purposes of this tutorial, we will focus on hardware interrupts.

SparkFun expLoRaBLE Hookup Guide

Check out our latest LoRaWAN development board with Bluetooth capabilities! With this guide, we'll get you passing data to The Things Network in no time.

Getting Started with MicroMod

Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

Designing with MicroMod

This tutorial will walk you through the specs of the MicroMod processor and carrier board as well as the basics of incorporating the MicroMod form factor into your own PCB designs!

MicroMod Main Board Hookup Guide

The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single and Main Board - Double.

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

Installing Arduino IDE

A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

Installing Board Definitions in the Arduino IDE

How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

Hardware Overview

Board Dimensions

The overall board dimensions are roughly 65 x 35 mm with an approximate 6 mm protrusion of the RP-SMA antenna connector.

board dimensions
The dimensions for the LoRa MicroMod Function Board. (Click to enlarge)

M.2 Edge Connector and Screw Slots

Like other function and processor boards, there is a polarized M.2 edge connector, which provides a standardized electrical connection. The attachment points for the screws prevent users from connecting a processor board into a function board slot and vice-versa.

function board attachment points
The Micromod M.2 edge connector and screw slots on the LoRa Function Board. (Click to enlarge)

Power

There is a power status LED to help make sure that your LoRa function board is getting (5V) power. Power is provided through the (MicroMod) M.2 edge connector. The LoRa module is meant to run on 5V with 3.3V logic levels. A jumper is available on the back of the board to remove power to the LED for low-power applications (see the Jumpers section below).

power led
Power LED on the LoRa MicroMod Function Board. (Click to enlarge)

E19-915M30S LoRa Module

Note: The range verification was performed in a clear and open area (direct line-of-sight) with a 5dBi antenna gain, height of 2.5m, and data rate 0.3 kbps. Users results may vary.

The Chengdu Ebyte E19-915M30S RF transceiver module is a 1W 915MHz LoRa module, based on the SX1276 from Semtech. It is FCC, CE, and RoHS certified and has been tested up to a range of 10km by the manufacturer. PLease refer to the datasheet for more details.

  • Global license free ISM 915MHz band
  • 1W maximum transmission power
    • Software multi-level adjustable
  • 256Byte FIFO data buffer

SX1276

The E19-915M30S transceiver is based on the SX1276 chip from Semtech. Please refer to the datasheet for more details.

Part Number SX1276
Frequency Range 137 - 1020 MHz
Spreading Factor 6 - 12
Bandwidth 7.8 - 500 kHz
Effective Bitrate .018 - 37.5 kbps
Est. Sensitivity -111 to -148 dBm
Characteristic Description
Operating Voltage 3.3 - 5.5 V
Current Consumption 630 mA (TX)) 23 mA (RX)) 3 µA (Sleep)
Operating Temperature -40 - 85 °C
Operating Humidity[1] 10 - 90%
Communication Interface SPI (0 - 10 Mbps)
Logic Level 3.3 V
Frequency Range 900 - 931 MHz
Transmit Power 28.5 - 30 dBm (max)
Modulation LoRa, FSK, GFSK, MSK, GMSK, OOK
Data Rate FSK: 1.2 - 300 kbps
LoRa: 0.018 - 37.5 kbps
Antenna Impedance 50 Ω

LoRa module
The E19-915M30S RF transceiver module on the LoRa MicroMod Function Board. (Click to enlarge)

Pin Connections

Below is a table of the pin connections available on the E19-915M30S RF transceiver module. However, not all the pins listed are utilized by the LoRa function board (see the Function Board Pinout Table section below).

Pin # Pin Name I/O Direction Pin Description
1 GND Ground
2 DIO5 Input/Output Configurable IO port(Please refer to the SX1276 datasheet).
3 DIO4 Input/Output Configurable IO port(Please refer to the SX1276 datasheet).
4 DIO3 Input/Output Configurable IO port(Please refer to the SX1276 datasheet).
5 DIO2 Input/Output Configurable IO port(Please refer to the SX1276 datasheet).
6 DIO1 Input/Output Configurable IO port(Please refer to the SX1276 datasheet).
7 DIO0 Input/Output Configurable IO port(Please refer to the SX1276 datasheet).
8 RST Input Reset
9 GND Ground
10 GND Ground
11 VCC Input Power supply: 4.75~5.5V (Ceramic filter capacitoris advised to add)
12 SCK Input SPI - Clock Signal
13 MISO Output SPI - Data from Peripheral Device
14 MOSI Input SPI - Data to Peripheral Device
15 NSS Input SPI - Chip Select
16 TXEN Input Radio frequency switch control, make sure the TXEN pin is in high level, RXEN pin is in low level when transmitting.
17 RXEN Input Radio frequency switch control, make sure the RXEN pin is in high level, TXEN pin is in low level when receiving.
18 GND Ground
19 ANT Antenna
20 GND Ground
21 GND Ground
22 GND Ground

MicroMod Edge Connector

The MicroMod M.2 edge connector provides a standardized interface for the pin connection of a function board.

function board edge connector
The Micromod M.2 edge connector on the LoRa Function Board. (Click to enlarge)

Function Board Pinout Table

The tables below outline the pin on the M2. edge connector and their functions.

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Functions Bottom
Pin
   Top   
Pin
Functions
(Not Connected) 75 GND
3.3V 74 73 G5 / BUS5
RTC_3V_BATT 72 71 G6 / BUS6
SPI_CS1# SDIO_DATA3 (I/O) 70 69 G7 / BUS7
SDIO_DATA2 (I/O) 68 67 G8
SDIO_DATA1 (I/O) 66 65 G9 ADC_D- CAM_HSYNC
SPI_CIPO1 SDIO_DATA0 (I/O) 64 63 G10 ADC_D+ CAM_VSYNC
SPI COPI1 SDIO_CMD (I/O) 62 61 SPI_CIPO (I)
SPI SCK1 SDIO_SCK (O) 60 59 SPI_COPI (O) LED_DAT
AUD_MCLK (O) 58 57 SPI_SCK (O) LED_CLK
CAM_MCLK PCM_OUT I2S_OUT AUD_OUT 56 55 SPI_CS#
CAM_PCLK PCM_IN I2S_IN AUD_IN 54 53 I2C_SCL1 (I/O)
PDM_DATA PCM_SYNC I2S_WS AUD_LRCLK 52 51 I2C_SDA1 (I/O)
PDM_CLK PCM_CLK I2S_SCK AUD_BCLK 50 49 BATT_VIN / 3 (I - ADC) (0 to 3.3V)
G4 / BUS4 48 47 PWM1
G3 / BUS3 46 45 GND
G2 / BUS2 44 43 CAN_TX
G1 / BUS1 42 41 CAN_RX
G0 / BUS0 40 39 GND
A1 38 37 USBHOST_D-
GND 36 35 USBHOST_D+
A0 34 33 GND
PWM0 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 SWDIO
UART_TX2 (O) 22 21 SWDCK
UART_RX2 (I) 20 19 UART_RX1 (I)
CAM_TRIG D1 18 17 UART_TX1 (0)
I2C_INT# 16 15 UART_CTS1 (I)
I2C_SCL (I/0) 14 13 UART_RTS1 (O)
I2C_SDA (I/0) 12 11 BOOT (I - Open Drain)
D0 10 9 USB_VIN
SWO G11 8 7 GND
RESET# (I - Open Drain) 6 5 USB_D-
3.3V_EN 4 3 USB_D+
3.3V 2 1 GND
LoRa Func. Board Pin Function Bottom
Pin
   Top   
Pin
Functions LoRa Func. Board Pin
(Not Connected) - 75 GND
VIN 74 73 3.3V 3.3V IN
VCC IN VIN 72 71 Power EN Power EN
- 70 69 -
- 66 65 -
- 64 63 -
- 62 61 F7
- 60 59 F6 LoRa DIO2
- 58 57 F5 LoRa DIO1
- 56 55 F4 LoRa RST
- 54 53 F3 LoRa RX EN
- 52 51 F2 PWM LoRa TX EN
- 50 49 F1 SPI_CS0 LoRa NSS (CS)
- 48 47 F0 INT LoRa DIO0
- 46 45 GND
- 44 43 -
- 42 41 -
EEPROM WP - 40 39 GND
A0 38 37 USBHOST_D-
EEPROM A0 EEPROM_A0 36 35 USBHOST_D+
EEPROM A1 EEPROM_A1 34 33 GND
EEPROM A2 EEPROM_A2 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 I2C_INT
22 21 I2C_SCL EEPROM SCL
20 19 I2C_SDA EEPROM SDA
UART_CTS 18 17
UART_RTS 16 15 UART_RX
14 13 UART_TX
12 11 GND
10 9
8 7 SPI_CIPO LoRa SDO
6 5 SPI_COPI LoRa SDI
4 3 SPI_SCK LoRa SCK
2 1 GND
Signal
Group
Signal I/O Description Voltage
Power 3.3V I 3.3V Source 3.3V
GND Return current path 0V
USB_VIN I USB VIN compliant to USB 2.0 specification. Connect to pins on processor board that require 5V for USB functionality 4.8-5.2V
RTC_3V_BATT I 3V provided by external coin cell or mini battery. Max draw=100μA. Connect to pins maintaining an RTC during power loss. Can be left NC. 3V
3.3V_EN O Controls the carrier board's main voltage regulator. Voltage above 1V will enable 3.3V power path. 3.3V
BATT_VIN/3 I Carrier board raw voltage over 3. 1/3 resistor divider is implemented on carrier board. Amplify the analog signal as needed for full 0-3.3V range 3.3V
Reset Reset I Input to processor. Open drain with pullup on processor board. Pulling low resets processor. 3.3V
Boot I Input to processor. Open drain with pullup on processor board. Pulling low puts processor into special boot mode. Can be left NC. 3.3V
USB USB_D± I/O USB Data ±. Differential serial data interface compliant to USB 2.0 specification. If UART is required for programming, USB± must be routed to a USB-to-serial conversion IC on the processor board.
USB Host USBHOST_D± I/O For processors that support USB Host Mode. USB Data±. Differential serial data interface compliant to USB 2.0 specification. Can be left NC.
CAN CAN_RX I CAN Bus receive data. 3.3V
CAN_TX O CAN Bus transmit data. 3.3V
UART UART_RX1 I UART receive data. 3.3V
UART_TX1 O UART transmit data. 3.3V
UART_RTS1 O UART ready to send. 3.3V
UART_CTS1 I UART clear to send. 3.3V
UART_RX2 I 2nd UART receive data. 3.3V
UART_TX2 O 2nd UART transmit data. 3.3V
I2C I2C_SCL I/O I2C clock. Open drain with pullup on carrier board. 3.3V
I2C_SDA I/O I2C data. Open drain with pullup on carrier board 3.3V
I2C_INT# I Interrupt notification from carrier board to processor. Open drain with pullup on carrier board. Active LOW 3.3V
I2C_SCL1 I/O 2nd I2C clock. Open drain with pullup on carrier board. 3.3V
I2C_SDA1 I/O 2nd I2C data. Open drain with pullup on carrier board. 3.3V
SPI SPI_COPI O SPI Controller Output/Peripheral Input. 3.3V
SPI_CIPO I SPI Controller Input/Peripheral Output. 3.3V
SPI_SCK O SPI Clock. 3.3V
SPI_CS# O SPI Chip Select. Active LOW. Can be routed to GPIO if hardware CS is unused. 3.3V
SPI/SDIO SPI_SCK1/SDIO_CLK O 2nd SPI Clock. Secondary use is SDIO Clock. 3.3V
SPI_COPI1/SDIO_CMD I/O 2nd SPI Controller Output/Peripheral Input. Secondary use is SDIO command interface. 3.3V
SPI_CIPO1/SDIO_DATA0 I/O 2nd SPI Peripheral Input/Controller Output. Secondary use is SDIO data exchange bit 0. 3.3V
SDIO_DATA1 I/O SDIO data exchange bit 1. 3.3V
SDIO_DATA2 I/O SDIO data exchange bit 2. 3.3V
SPI_CS1/SDIO_DATA3 I/O 2nd SPI Chip Select. Secondary use is SDIO data exchange bit 3. 3.3V
Audio AUD_MCLK O Audio master clock. 3.3V
AUD_OUT/PCM_OUT
I2S_OUT/CAM_MCLK
O Audio data output. PCM synchronous data output. I2S serial data out. Camera master clock. 3.3V
AUD_IN/PCM_IN
I2S_IN/CAM_PCLK
I Audio data input. PCM syncrhonous data input. I2S serial data in. Camera periphperal clock. 3.3V
AUD_LRCLK/PCM_SYNC
I2S_WS/PDM_DATA
I/O Audio left/right clock. PCM syncrhonous data SYNC. I2S word select. PDM data. 3.3V
AUD_BCLK/PCM_CLK
I2S_CLK/PDM_CLK
O Audio bit clock. PCM clock. I2S continuous serial clock. PDM clock. 3.3V
SWD SWDIO I/O Serial Wire Debug I/O. Connect if processor board supports SWD. Can be left NC. 3.3V
SWDCK I Serial Wire Debug clock. Connect if processor board supports SWD. Can be left NC. 3.3V
ADC A0 I Analog to digital converter 0. Amplify the analog signal as needed to enable full 0-3.3V range. 3.3V
A1 I Analog to digital converter 1. Amplify the analog signal as needed to enable full 0-3.3V range. 3.3V
PWM PWM0 O Pulse width modulated output 0. 3.3V
PWM1 O Pulse width modulated output 1. 3.3V
Digital D0 I/O General digital input/output pin. 3.3V
D1/CAM_TRIG I/O General digital input/output pin. Camera trigger. 3.3V
General
Bus
G0/BUS0 I/O General purpose pins. Any unused processor pins should be assigned to Gx with ADC + PWM capable pins given priority (0, 1, 2, etc.) positions. The intent is to guarantee PWM, ADC and Digital Pin functionality on respective ADC/PWM/Digital pins. Gx pins do not guarantee ADC/PWM function. Alternative use is pins can support a fast read/write 8-bit or 4-bit wide bus. 3.3V
G1/BUS1 I/O 3.3V
G2/BUS2 I/O 3.3V
G3/BUS3 I/O 3.3V
G4/BUS4 I/O 3.3V
G5/BUS5 I/O 3.3V
G6/BUS6 I/O 3.3V
G7/BUS7 I/O 3.3V
G8 I/O General purpose pin 3.3V
G9/ADC_D-
CAM_HSYNC
I/O Differential ADC input if available. Camera horizontal sync. 3.3V
G10/ADC_D+
CAM_VSYNC
I/O Differential ADC input if available. Camera vertical sync. 3.3V
G11/SWO I/O General purpose pin. Serial Wire Output 3.3V

EEPROM

There is an I2C serial EEPROM on the LoRa function board. It has been reserved for future use, but users have access to it. A jumper is available on the back of the board to write protect the EEPROM (see the Jumpers section below).

EEPROM
EEPROM on the LoRa MicroMod Function Board. (Click to enlarge)

RP-SMA Antenna Connector

Warning: Users should attach the antenna before powering their LoRa function board. Transmitting without an antenna connected may potentially damage the transceiver module.

The LoRa function board features a sturdy RP-SMA antenna connector for users to attach an antenna of their choice. While this antenna connector is fairly robust, users should not expect to leverage a lot of weight off of it.

The edge-type antenna connector allows for the threads to protrude just beyond the edge of the board. Along with the dimensions of the LoRa function board, this feature is designed so that the connection also extends past the edge of the main board that the function board interfaces with; and is therefore, well suited to be used with an enclosure.

Antenna Connector
RP-SMA antenna connector on the LoRa MicroMod Function Board. (Click to enlarge)

Note: Users who wish to use the u.FL connector can modify the position of this 0Ω resistor. Due to the size and position of the resistor, we only recommended for highly experience soldering experts attempt this modification. More novice users could potentially damage their LoRa function board if they attempt this modification.

antenna jumper
Antenna select jumper on the E19-915M30S RF transceiver module. (Click to enlarge)

Jumpers

There are three jumpers available on the LoRa function board.

LED Power

For more low power projects, the PWR jumper can be cut to remove power from the red power LED.

LED power jumper
LED power jumper on the LoRa MicroMod Function Board. (Click to enlarge)

Current Measurement

For users who would like to measure the current going to LoRa function board, the MEAS jumper can be cut and used for measurements. This jumper is only connected to the 5V power, which is used by only the E19-915M30S RF transceiver module and power LED.

Current measurement jumper
Current measurement jumper on the LoRa MicroMod Function Board. (Click to enlarge)

EEPROM Write Protection

To permanently write protect the EEPROM on the LoRa function board, users can bridge the WP jumper.

EEPROM WP jumper
EEPROM WP jumper on the LoRa MicroMod Function Board. (Click to enlarge)

Software Overview

Getting Started with MicroMod

For those unfamiliar with the MicroMod ecosystem, be sure to review the Getting Started with MicroMod guide. Also, make sure that the correct board definitions are installed in the Arduino IDE, for the associated processor board.

Getting Started with MicroMod

October 21, 2020
Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

Programming

Note: Make sure that the correct board definitions are installed in the Arduino IDE, for the connected processor board. Depending on the processor board, users may need to install drivers (if they have not done so already). For help installing board definitions, use the MicroMod processor boards landing page and review the associated hookup guide for that hardware.

Installing Board Definitions in the Arduino IDE

September 9, 2020
How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

Arduino Library

Note: The example for this tutorial assumes users have the latest version of the Arduino IDE installed. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide:

Installing an Arduino Library

January 11, 2013
How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

SparkFun External EEPROM Arduino Library

We've written a library to easily get setup and read/write data on the EEPROM. You can install this library through the Arduino Library Manager. Search for SparkFun External EEPROM Arduino Library and you should be able to install the latest version. If you prefer manually downloading the libraries from the GitHub repository, you can grab them here:

For more details on this Arduino library and its use, please refer to the Serial EEPROM hookup guide:

Reading and Writing Serial EEPROMs

August 11, 2017
EEPROM is a great way to add extra memory to your microcontroller project. Wait 'til you see how easy it is to use!

RadioLib Arduino Library

The RadioLib library provides support for peer-to-peer RF communication with the 1W LoRa MicroMod Function Board. Users can install this library through the Arduino Library Manager. Search for RadioLib and you should be able to install the latest version. If you prefer manually downloading the libraries from the GitHub repository, you can grab them here:

Note: Peer-to-peer refers to direct RF communication using a specific modulation protocol (similar to a 2-way walkie talkie); and is not to be confused with a mesh network or LoRaWAN network integration.

For more details on this Arduino library, check out the Arduino reference page, the API refernce page, and GitHub repository. Additional specifics of the library that users may be interested in can be found in the links below:

LoRaWAN Library

The MCCI LoRaWAN LMIC Library library provides support for an end node/device (i.e. 1W LoRa MicroMod Function Board) integration into a LoRaWAN network and communication with a LoRaWAN server. Users can install this library through the Arduino Library Manager. Search for MCCI LoRaWAN LMIC and you should be able to install the latest version. If you prefer manually downloading the libraries from the GitHub repository, you can grab them here:

Notes:
  • Initially we were inclined to utilize the Arduino-LMIC library. However, we followed the repository's recommendation and chose to utilize the MCCI LoRaWAN LMIC Library instead.
  • Support for this library has only been confirmed with The Things Stack - Community Edition's (i.e. V3 or previously TTN) and Helium's servers.
  • To utilize this library, users are expected to be able to modify various files for regional configuration and compatibility with specific processor boards.
  • We assume that users are familiar with the device registration process for each LoRaWAN server. For more information, please refer to the LoRaWAN server's documentation:
    • Helium Device Registration
      • Usage Cost: 1 Data Credit (1 DC = 0.001¢ in USD) per packet (up to 24 bytes)
      • After a device is first added/registered to an account, it takes approx. 20 min for it to get added to the blockchain. Until then, hotspots will not recognize the device and relay its data packets.
    • The Things Stack Device Registration:
      • The information below also assumes that users have migrated to and are currently using The Things Stack Community Edition (or V3).
      • When manually registering a device on The Things Stack, users will need to set the LoRaWAN version to MAC V1.0.3 (per the library specifications).
      • Devices registered with the V3 console will only work with gateways on the V3 console. (i.e. Data transmissions from a device registered on the V3 console will not be passed to the server, if its transmissions are only received by a gateway on registered to the V2 console.)
Warning: The Helium network is a pay-to-use 3rd party service, which does involve the use of cryptocurrency. Please, use at your own discretion.
  • We have no control over its service.
  • We are not liable for any customer's choice to utilize the network.
  • The cryptocurrency market valuation can be volitile.
  • There may be legal and financial implications for digital wallets.
  • etc.

To be able to utilize this library with the 1W LoRa function board and various MicroMod processor boards, users will need to make the following modifications to the library's files:

Regional Configuration

In the lmic_project_config.h file make sure that #define CFG_us915 1 and #define CFG_sx1276_radio 1 are uncommented.

language:c
// project-specific definitions
//#define CFG_eu868 1
#define CFG_us915 1
//#define CFG_au915 1
//#define CFG_as923 1
// #define LMIC_COUNTRY_CODE LMIC_COUNTRY_CODE_JP      /* for as923-JP; also define CFG_as923 */
//#define CFG_kr920 1
//#define CFG_in866 1
#define CFG_sx1276_radio 1
//#define LMIC_USE_INTERRUPTS
Processor Board Compatibility
nRF52840 Processor Board

In the hal.cpp file, users will need to modify lines 368-370 (based on the default code) to provide compatibility with the nRF52840 processor board to the library:

language:c
#if !defined(ARDUINO_ARDUINO_NANO33BLE)
void hal_sleep () {
    // Not implemented
}
#endif // !defined(ARDUINO_ARDUINO_NANO33BLE)
Artemis Processor Board
Note: Currently, the Apollo3 Arduino core does not support the use of the noInterrupts() and Interrupts() functions. There is already an issue filed with the GitHub repository. Once this issue has been resolved, the modifications below will no longer be necessary.

In the hal.cpp file, users will need to modify lines 339-347 (based on the default code) to provide compatibility with the Artemis processor board to the library:

language:c
void hal_disableIRQs () {
    #if !defined(ARDUINO_APOLLO3_SFE_ARTEMIS_MM_PB)
        noInterrupts();
    #endif // !defined(ARDUINO_APOLLO3_SFE_ARTEMIS_MM_PB)

    irqlevel++;
}

void hal_enableIRQs () {
    if(--irqlevel == 0) {
        #if !defined(ARDUINO_APOLLO3_SFE_ARTEMIS_MM_PB)
            interrupts();
        #endif // !defined(ARDUINO_APOLLO3_SFE_ARTEMIS_MM_PB)
ES32 Processor Board

In reference to issue #714 for the library, users will need to add the following lines to the end of lmic_project_config.h file, which is the same file used for the regional configuration.

language:c
#if defined(ARDUINO_ESP32_MICROMOD)
    #define hal_init LMICHAL_init  // ESP32: https://github.com/mcci-catena/arduino-lmic/issues/714
#endif // defined(ARDUINO_ESP32_MICROMOD)

Hadware Assembly

For those unfamiliar with the MicroMod ecosystem, be sure to review the Getting Started with MicroMod guide.

Getting Started with MicroMod

October 21, 2020
Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

Processor Board and Main Board

To get started users will need a compatible processor and main board. Insert the MicroMod processor board into the M.2 socket for the processor board at an angle, with its edge connector aligned to the matching slots.

Note: The dimensions of the processor board's edge connector prevents it from mating with the slots of the M.2 socket in reverse. As an extra safeguard, the screw insert is spaced to only match the screw key of MicroMod processor boards.

When inserted properly, the processor board will rest at an angle:

MicroMod processor board inserted into the carrier board
Inserting a processor board into the M.2 socket. (Click to enlarge)

To secure the processor board, gently hold down on the board and attach the M.2 screw with a Phillip's head (PH0 or PH1) screw driver. Below, is an example of an assembled MicroMod system:

MicroMod processor board attached to the Qwiic carrier board
A processor board attached to the MicroMod Qwiic Carrier Board. (Click to enlarge)

Function Board and Main Board

Warning: The LoRa module is susceptible to electrostatic discharge. Therefore, it is recommended that users a static discharge strap, like the one included in the iFixit Pro Tech Toolkit.


Static discharge strap in the upper righthand corner. (Click to enlarge)

Users should also address any humidity and temperature concerns, when utilizing the LoRa function board.

Note: The dimensions of the function board's edge connector prevents it from mating with the slots of the M.2 socket in reverse. As an extra safeguard, the screw inserts are spaced to only match the screw key of MicroMod function board.

Similarly to the processor board, insert the MicroMod function board into the M.2 socket for the function board at an angle, with its edge connector aligned to the matching slots.

When inserted properly, the function board will rest at an angle:

MicroMod function board inserted into the main board
Inserting a function board into the M.2 socket. (Click to enlarge)

To secure the function board, gently hold down on the board and attach the M.2 screw with a Phillip's head (PH0 or PH1) screw driver. Below, is an example of an assembled MicroMod system:

MicroMod function board attached to the main board
A function board attached to the MicroMod Main Board. (Click to enlarge)

Don't forget to attach the antenna for the LoRa function board. Transmitting or powering the LoRa module without an attached antenna has the potential to permanently damage the transceiver.

Fully assembled main board with processor board and function board
Fully assembled main board with processor board and function board. (Click to enlarge)

Main Board Example - Pin Connection Table

This table summarizes the pins utilized on the LoRa function board's MicroMod edge connector and their connections to the main board's processor pins; based on the slot that the LoRa function board is inserted to.

Function Board
Pin Name
MicroMod
Pin Number
I/O
Direction
Description Main Board's
Processor Pin
Slot 0 Slot 1
VCC 72 Input Power supply: 4.75~5.5V
  • Power LED
  • Transceiver's Power
-
3.3V 73 Input Power supply: 3.3V
  • EEPROM's Power
  • Logc-level conversion
-
GND 11 - Ground -
Power Enable 71 Input Controls the 3.3V power 68 66
SCK 3 Input SPI - Clock signal for transceiver SCK (57)
CIPO 7 Output SPI - Data from transceiver CIPO (59)
COPI 5 Input SPI - Data to transceiver COPI (61)
NSS 49 (F1) Input SPI - Chip select for transceiver CS0 (55) CS1 (70)
RST 55 (F4) Input Resets transceiver G1 (42) G6 (71)
DIO0 47 (F0) Input
Output
Transceiver's configurable IO(Please refer to the SX1276 datasheet). D0 (10) D1 (18)
DIO1 57 (F5) Input
Output
Transceiver's configurable IO(Please refer to the SX1276 datasheet). G2 (44) G7 (69)
DIO2 59 (F6) Input
Output
Transceiver's configurable IO(Please refer to the SX1276 datasheet). G3 (46) G8 (62)
TXEN 51 (F2) Input Transceiver's RF control switch: The TXEN pin is in high level, RXEN pin is in low level when transmitting. PWM0 (32) PWM1 (47)
RXEN 53 (F3) Input Transceiver's RF control switch: The RXEN pin is in high level, TXEN pin is in low level when receiving. G0 (40) G5 (73)
SCL 21 Input I2C - Clock signal for EEPROM SCL (14)
SDA 19 Input
Output
I2C - Data signal for EEPROM SDA (12)
EEPROM WP 40 Input Controls the write protection pin for the EEPROM. Pull low to enable. -
EEPROM A0 6 Input Controls EEPROM's I2C address configuration. -
EEPROM A1 4 Input Controls EEPROM's I2C address configuration. -
EEPROM A2 2 Input Controls EEPROM's I2C address configuration. -

Programming

To program the processor board utilized on the Main Board; connect the board to a computer with a USB-C cable. Depending on the processor board, users may need to install drivers (if they have not done so already).

Note: Make sure that the correct board definitions are installed in the Arduino IDE, for the selected processor board. For help installing board definitions, use the MicroMod processor boards landing page and review the associated hookup guide for that hardware.

Installing Board Definitions in the Arduino IDE

September 9, 2020
How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

Peer-to-Peer Example

Note: The example codes assume that the LoRa function board is inserted into the 0 function board slot of the main board.

The example codes below, allow users to communicate between two LoRa function boards. Simply download, extract the files, and upload the code the main board with associated processor and function boards.

Additional examples have also been provided for users who would like to use their expLoRable (LoRa Thing Plus) board to communicate with a LoRa function board.

The example codes were tested under the following parameters:
  • Arduino IDE version: 1.8.16
    • If not using the Teensy - Windows App Store version 1.8.51.0
  • RadioLib Library version: 4.6.0
  • MicroMod Processor Boards and Arduino Cores:
    Processor Board Definition
    RP2040 Arduino Mbed OS RP2040 Boards version: 2.5.2
    ESP32 esp32 version: 2.0.0
    STM32 SparkFun STM32 Boards version: 2.0.0
    Artemis SparkFun Apollo3 Boards version: 2.1.1
    SAMD51 SparkFun SAMD Boards (dependency Arduino SAMD Boards version 1.8.1) version: 1.8.5
    • Requires - Arduino SAMD Boards (32-bit ARM Cortex-M0+) version: 1.8.11
    nRF52840 [DEPRECATED - Please install standalone packages] Arduino Mbed OS Boards version: 1.3.1
    Teensy Teensyduino version: 1.55

Once uploaded, users can open the serial monitor to view the progress of the data transmission or reception. When using the RP2040 processor board, the example code will wait until the Serial Monitor is opened to execute the code and transmit/receive data.

peer-to-peer data transmission example
An example of the data transmission between an expLoRaBLE board and the LoRa MicroMod Function Board in the Serial Monitor. (Click to enlarge)

Code Breakdown

In order to get the built-in example for the RadioLib library working, a few changes needed to be made. Below, is a short explanation of the modifications made to the example code that we provide (see above), to include compatibility with all the available processor boards.

CS Pin Definition

The SPI library for the Arduino IDE, by default expects the chip select pin to be defined as PIN_SPI_SS. However, this pin definition is different for the ESP32 and Artemis (Apollo3) Arduino cores. Therefore, the code below was inserted to allow the code to compile for all the various processor boards.

language:c
// Redefine CS Pin Name
// SPI_CS0:     ESP32
// SS:          ESP32, nRF, RP2040
// SPI_CS:      Artemis
// PIN_SPI_SS:  STM32, SAMD51, nRF, RP2040

#ifndef PIN_SPI_SS
    // For Artemis
    #ifdef SS
        #define PIN_SPI_SS SPI_CS
    #endif
    // For ESP32
    #ifdef SPI_CS0
        #define PIN_SPI_SS SS
    #endif
#endif

MicroMod Pin Names

Unfortunately, for the RP2040 MicroMod processor board hasn't been included in the MbedOS Arduino core; current progress is on hold (please refer to this issue in the GitHub repository). However, with the modifications below, the RP2040 Pico board definition can be used.

By using the RP2040 Pico board definition, the generic MicroMod processor board's pin names obviously can't be used. Therefore, all the pins must be declared by their GPIO pin numbers. In addition, the default pin connections for the SPI bus on the RP2040 MicroMod processor board differs from the RP2040 Pico. To accommodate for the different pin connections, a custom SPI object was created and passed into the library.

language:c
// SX1276 pin connections:
//       | SLOT 0 | SLOT 1 |
//==========================
// cs    |   CS0  |   CS1  |
// dio0  |   D0   |   D1   |
// dio1  |   G2   |   G7   |
// dio2  |   G3   |   G8   |
// rst   |   G1   |   G6   |
// tx_en |  PWM0  |  PWM1  |
// rx_en |   G0   |   G5   |

#if defined(ARDUINO_RASPBERRY_PI_PICO)
    // MM RP2040 Processor Board (Using RP2040 Pico board definition)
    int pin_cs = 21;
    int pin_dio0 = 6;
    int pin_tx_enable = 13;
    int pin_rx_enable = 16;
    int pin_nrst = 17;
    int pin_dio1 = 18;

    // Redefine SPI pins
    int miso = 20;
    int mosi = 23;
    int sck = 22;

    // Custom SPI object
    MbedSPI SPI_mm(miso, mosi, sck);

    SX1276 radio = new Module(pin_cs, pin_dio0, pin_nrst, pin_dio1, SPI_mm);

#else

Similarly to the RP2040, the Teensy MicroMod processor board definition doesn't include the generic MicroMod processor board pin names yet (we are currently working on this update). Therefore, all the pins must be declared by their pin numbers.

language:c
    #if defined(ARDUINO_TEENSY_MICROMOD)
        // MM Teensy Processor Board
        int pin_cs = 10;
        int pin_dio0 = 4;
        int pin_tx_enable = 3;
        int pin_rx_enable = 40;
        int pin_nrst = 41;
        int pin_dio1 = 42;

    #else

RP2040 Special Consideration

As mentioned above, a custom SPI object was created and passed into the library for the RP2040 MicroMod processor board. However, the library doesn't initialize the SPI bus when it is passed in. Therefore, the setup() loop includes a modification to start the SPI bus operation.

In our testing, the RP2040 MicroMod processor board had issues with the printouts on the serial port. Adding a while() statement to wait for the serial port to be accessed by the Serial Monitor, resolved the issue.

language:c
#if defined(ARDUINO_RASPBERRY_PI_PICO)
    // Wait for serial monitor/port to open
    while (!Serial){
        ; // wait for serial port
    }

    // Start SPI bus
    SPI_mm.begin();
#endif

Enabling the STM32 Serial Port

When uploading to the provided example code (see above) to the STM32 MicroMod processor board, users will need to enable the serial port on the processor board. Otherwise, when the Serial Monitor is opened, nothing will appear. The following settings must be used in the in the Tools drop down menu:

STM32 serial port configuration
The STM32 MicroMod processor board settings in the Tools drop-down menu to enable the microcontroller's serial port. (Click to enlarge)

LoRaWAN Examples

Important Notes:
  • The example below assumes that the LoRa function board is inserted into the 0 function board slot of the main board.
  • While there are sketch examples built into the MCCI LoRaWAN LMIC Arduino library for both the Helium and The Things Network (TTN) servers, users should use the example code that we provide below (click the Download buttons). Otherwise, users will run into various issues.
  • The examples below, require a user account and device registration on whichever server you decide to utilize.
    • Click here to setup an account on Helium
      • Usage Cost: 1 Data Credit (1 DC = 0.001¢ in USD) per packet (up to 24 bytes)
      • After a device is first added/registered to an account, it takes approx. 20 min for it to get added to the blockchain. Until then, hotspots will not recognize the device and relay its data packets.
    • Click here to setup an account on The Things Stack
      • The information below also assumes that users have migrated to and are currently using The Things Stack Community Edition (or V3).
      • Devices registered with the V3 console will only work with gateways on the V3 console. (i.e. Data transmissions from a device registered on the V3 console will not be passed to the server, if its transmissions are only received by a gateway on registered to the V2 console.)
      • When manually registering a device on The Things Stack, users will need to set the LoRaWAN version to MAC V1.0.3 (per the library specifications).
Warning: The Helium network is a pay-to-use 3rd party service, which does involve the use of cryptocurrency. Please, use at your own discretion.
  • We have no control over its service.
  • We are not liable for any customer's choice to utilize the network.
  • The cryptocurrency market valuation can be volitile.
  • There may be legal and financial implications for digital wallets.
  • etc.

Our example codes below, allow users to communicate with a LoRaWAN server (through a connected gateway) with the LoRa function board. Simply download, extract the file, modify the sketch to include a registered device's EUIs and application key, and then upload the code the main board with associated processor and function board.

The example codes were tested under the following parameters:
  • Arduino IDE version: 1.8.16
    • If not using the Teensy - Windows App Store version 1.8.51.0
  • MCCI LoRaWAN LMIC Library version: 4.1.0
  • MicroMod Processor Boards and Arduino Cores:
    Processor Board Definition
    RP2040 Arduino Mbed OS RP2040 Boards version: 2.5.2
    ESP32 esp32 version: 2.0.0
    STM32 SparkFun STM32 Boards version: 2.0.0
    Artemis SparkFun Apollo3 Boards version: 2.1.1
    SAMD51 SparkFun SAMD Boards (dependency Arduino SAMD Boards version 1.8.1) version: 1.8.5
    • Requires - Arduino SAMD Boards (32-bit ARM Cortex-M0+) version: 1.8.11
    nRF52840 [DEPRECATED - Please install standalone packages] Arduino Mbed OS Boards version: 1.3.1
    Teensy Teensyduino version: 1.55

Configuring the End Device Information

Once users have registered/added an end (i.e. node) device to their user account, they will need to modify the example sketch to include their device's application EUI (APPEUI), device EUI (DEVEUI), and application key (APPKEY) (provided by the server at the end of the device registration process). Simply, replace the FILLMEIN value in { FILLMEIN }, inside of the sketch at these locations:

  • static const u1_t PROGMEM APPEUI[8]={ FILLMEIN };
  • static const u1_t PROGMEM DEVEUI[8]={ FILLMEIN };
  • static const u1_t PROGMEM APPKEY[16] = { FILLMEIN };

in this section of the sketch:

language:c
// For normal use, we require that you edit the sketch to replace FILLMEIN
// with values assigned by the TTN console. 
//# warning "You must replace the values marked FILLMEIN with real values from the TTN control panel!"

// This EUI must be in little-endian format, so least-significant-byte
// first. When copying an EUI from ttnctl output, this means to reverse
// the bytes. For TTN issued EUIs the last bytes should be 0xD5, 0xB3,
// 0x70. For Helium issued EUIs the last bytes should be 0xF9, 0x81, 0x60.
static const u1_t PROGMEM APPEUI[8]={ FILLMEIN };
void os_getArtEui (u1_t* buf) { memcpy_P(buf, APPEUI, 8);}

// This should also be in little endian format, see above.
static const u1_t PROGMEM DEVEUI[8]={ FILLMEIN };
void os_getDevEui (u1_t* buf) { memcpy_P(buf, DEVEUI, 8);}

// This key should be in big endian format (or, since it is not really a
// number but a block of memory, endianness does not really apply). In
// practice, a key taken from ttnctl can be copied as-is.
static const u1_t PROGMEM APPKEY[16] = { FILLMEIN };
void os_getDevKey (u1_t* buf) {  memcpy_P(buf, APPKEY, 16);}

The format of the values should be in a hex format, as shown in the example code below. Users should doublecheck they haven't mixed up their APPEUI and DEVEUI values and that they have entered those values with the least significant byte (lsb) first. These are the most likely culprits, if users aren't seeing a join/accept response or data transmissions in the LoRaWAN server's console or the serial terminal.

language:c
// This EUI must be in little-endian format, so least-significant-byte
// first. When copying an EUI from ttnctl output, this means to reverse
// the bytes. For TTN issued EUIs the last bytes should be 0xD5, 0xB3,
// 0x70. For Helium issued EUIs the last bytes should be 0xF9, 0x81, 0x60.
static const u1_t PROGMEM APPEUI[8]={ 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x## };
void os_getArtEui (u1_t* buf) { memcpy_P(buf, APPEUI, 8);}

// This should also be in little endian format, see above.
static const u1_t PROGMEM DEVEUI[8]={ 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x## };
void os_getDevEui (u1_t* buf) { memcpy_P(buf, DEVEUI, 8);}

// This key should be in big endian format (or, since it is not really a
// number but a block of memory, endianness does not really apply). In
// practice, a key taken from ttnctl can be copied as-is.
static const u1_t PROGMEM APPKEY[16] = { 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x##, 0x## };
void os_getDevKey (u1_t* buf) {  memcpy_P(buf, APPKEY, 16);}

Once uploaded, users can open the serial monitor to view the progress of the device joining their chosen server's network and data transmissions. When using the RP2040 processor board, the example code will wait until the Serial Monitor is opened to execute the code. Users can also view the same information in the server's console, device information page.

Code Breakdown

In order to get the built-in example for the MCCI LoRaWAN LMIC library working, a few changes needed to be made. Below, is a short explanation of the modifications made to the example code that we provide (see above), to include compatibility with all the available processor boards and improve the code performance.

CS Pin Definition

The SPI library for the Arduino IDE, by default expects the chip select pin to be defined as PIN_SPI_SS. However, this pin definition is different for the ESP32 and Artemis (Apollo3) Arduino cores. Therefore, the code below was inserted to allow the code to compile for all the various processor boards.

language:c
// Redefine CS Pin Name
// SPI_CS0:     ESP32
// SS:          ESP32, nRF, RP2040
// SPI_CS:      Artemis
// PIN_SPI_SS:  STM32, SAMD51, nRF, RP2040

#ifndef PIN_SPI_SS
    // For Artemis
    #ifdef SS
        #define PIN_SPI_SS SPI_CS
    #endif // SS
    // For ESP32
    #ifdef SPI_CS0
        #define PIN_SPI_SS SS
    #endif // SPI_CS0
#endif // PIN_SPI_SS

MicroMod Pin Names

Unfortunately, for the RP2040 MicroMod processor board hasn't been included in the MbedOS Arduino core; current progress is on hold (please refer to this issue in the GitHub repository). However, with the modifications below, the RP2040 Pico board definition can be used.

By using the RP2040 Pico board definition, the generic MicroMod processor board's pin names obviously can't be used. Therefore, all the pins must be declared by their GPIO pin numbers. In addition, the default pin connections for the SPI bus on the RP2040 MicroMod processor board differs from the RP2040 Pico. To accommodate for the different pin connections, a custom SPI object was created.

language:c
// SX1276 pin connections:
//       | SLOT 0 | SLOT 1 |
//==========================
// cs    |   CS0  |   CS1  |
// dio0  |   D0   |   D1   |
// dio1  |   G2   |   G7   |
// dio2  |   G3   |   G8   |
// rst   |   G1   |   G6   |
// tx_en |  PWM0  |  PWM1  |
// rx_en |   G0   |   G5   |

#if !defined(USE_STANDARD_PINMAP)
// All pin assignments use Arduino pin numbers (e.g. what you would pass
// to digitalWrite), or LMIC_UNUSED_PIN when a pin is not connected.
    const lmic_pinmap lmic_pins = {
        #if defined(ARDUINO_RASPBERRY_PI_PICO)
            // MM RP2040 Processor Board (Using RP2040 Pico board definition)
            .nss =  21, //Chip Select
            .rxtx = LMIC_UNUSED_PIN,
            .rst =  17,
            .dio =  {6, 18, LMIC_UNUSED_PIN},

Similarly to the RP2040, the Teensy MicroMod processor board definition doesn't include the generic MicroMod processor board pin names yet (we are currently working on this update). Therefore, all the pins must be declared by their pin numbers.

language:c
#elif defined(ARDUINO_TEENSY_MICROMOD)
    // MM Teensy Processor Board
    .nss =  10, //Chip Select
    .rxtx = LMIC_UNUSED_PIN,
    .rst =  41,
    .dio =  {4, 42, LMIC_UNUSED_PIN},

RP2040 Special Consideration

As mentioned above, a custom SPI object was created. However, the custom SPI object must be passed into code execution for the RP2040 MicroMod processor board. Therefore, the setup() loop includes a modification to do this. Additionally, during our testing, the RP2040 MicroMod processor board had issues with the printouts on the serial port. Including a while() statement to wait for the serial port to be accessed by the Serial Monitor, resolved the issue.

language:c
#if defined(ARDUINO_RASPBERRY_PI_PICO)
    // Wait for serial monitor/port to open
    while (!Serial)
        ; // wait for serial port

// Pass object back into SPI
SPI = SPI_mm;
#endif // defined(ARDUINO_RASPBERRY_PI_PICO)

Helium Network Configuration

In order to improve the performance of the example code, the modifications below were made to address a clock timing issue and limit the transmission band.

language:c
// allow much more clock error than the X/1000 default. See:
// https://github.com/mcci-catena/arduino-lorawan/issues/74#issuecomment-462171974
// https://github.com/mcci-catena/arduino-lmic/commit/42da75b56#diff-16d75524a9920f5d043fe731a27cf85aL633
// the X/1000 means an error rate of 0.1%; the above issue discusses using values up to 10%.
// so, values from 10 (10% error, the most lax) to 1000 (0.1% error, the most strict) can be used.
LMIC_setClockError(1 * MAX_CLOCK_ERROR / 40);

LMIC_setLinkCheckMode(0);
LMIC_setDrTxpow(DR_SF7,14);

#if CFG_LMIC_US_like
    // This makes joins faster in the US because we don't wander all over the
    // spectrum.
    LMIC_selectSubBand(1);
#endif

Enabling the STM32 Serial Port

When uploading to the provided example code (see above) to the STM32 MicroMod processor board, users will need to enable the serial port on the processor board. Otherwise, when the Serial Monitor is opened, nothing will appear. The following settings must be used in the in the Tools drop down menu:

STM32 serial port configuration
The STM32 MicroMod processor board settings in the Tools drop-down menu to enable the microcontroller's serial port. (Click to enlarge)

Resources and Going Further

For more information on the SparkFun 1W LoRa Function Board, check out the links below:

Hardware Documentation:

MicroMod Documentation:

Looking for more inspiration? Check out these other tutorials related to MicroMod.

MicroMod Artemis Processor Board Hookup Guide

Get started with the Artemis MicroMod Processor Board in this tutorial!

MicroMod Weather Carrier Board Hookup Guide

A quick guide to help to create your own MicroMod weather station using the MicroMod Weather Carrier Board and Processor of your choice.

Designing with MicroMod

This tutorial will walk you through the specs of the MicroMod processor and carrier board as well as the basics of incorporating the MicroMod form factor into your own PCB designs!

MicroMod RP2040 Processor Board Hookup Guide

This tutorial covers the basic functionality of the MicroMod RP2040 Processor Board and highlights the features of the dual-core ARM Cortex-M0+ processors development board. Get started with the first microcontroller from the Raspberry Pi Foundation!

MicroMod WiFi Function Board - ESP32 Hookup Guide

The MicroMod ESP32 Function Board adds additional wireless options to MicroMod Processor Boards that do not have that capability. This special function board acts as a coprocessor that takes advantage of Espressif's ESP32 WROOM to add WiFi and Bluetooth® to your applications.

MicroMod Single Pair Ethernet Function Board - ADIN1110 Hookup Guide

With the SparkFun MicroMod Single Pair Ethernet Function Board - ADIN1110 you can prototype and create 10BASE-T1L Ethernet connections that work in noisy environments and over exceptionally long distances of over 1 kilometer! Follow this guide to get started with this Function Board.

MicroMod Alorium Sno M2 Processor Board Hookup Guide

Get started with the MicroMod Alorium Sno M2 Processor Board!

MicroMod Main Board Hookup Guide V2

The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single V2.1 and Main Board - Double and V2.2.