Wireless Remote Control with micro:bit

≡ Pages
Contributors: bboyho

Experiment 2: Wirelessly Driving Forward

Introduction

Remember our micro:bot? The micro:bot was running around loose by itself the last time we were working with the robot. Let's give it some commands so that it only moves when you want it to using the controller:bit carrier board!

Parts Needed

You will need the following parts:

  • 2x micro:bit Boards
  • 2x Micro-B USB Cables
  • 1x Assembled micro:bot Kit
  • 1x controller:bit Carrier Board
  • 4x AA Batteries
  • 2x AAA Batteries (if you are using the battery pack with switch for the controller)

For a few items listed, you will need more than one unit (i.e. micro:bits, AA batteries, etc.). You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

SparkFun micro:bot kit for micro:bit - v2.0

KIT-16275
$77.50

USB Micro-B Cable - 6"

CAB-13244
$2.50

Panasonic Alkaline Battery - AA

PRT-15201
$0.60

750 mAh Alkaline Battery - AAA

PRT-09274
Retired

micro:bit Board

DEV-14208
Retired

SparkFun micro:arcade kit for micro:bit v2.0

KIT-16403
Retired

2.1 Remote Control

For this part of the experiment, we will use the same method as experiment 1 to transmit a command. As soon as a certain combination of buttons are pressed on the controller:bit, the attached micro:bit will transmit one command to a receiving micro:bit. For debugging purposes, we are going to have a short animation when the buttons are pressed for feedback.

Hardware Hookup

If you have not already, insert one micro:bit into the controller:bit's carrier board. Make sure to insert the micro:bit with the LED array facing up (the same direction as all of the buttons) as explained in the micro:arcade kit experiment guide. We’re continuing on from experiment 3. Make sure to check out the guide before continuing on.

micro:arcade Kit Experiment Guide

July 21, 2017
We love games! We love writing games, building games and yes, even building game consoles. So we want to introduce to you the micro:arcade kit for the micro:bit!

Then connect the micro:bit to your computer via USB cable.

controller:bit micro:bit and USB Cable

Running Your Script

Download the following example script and move the *.hex file to your micro:bit. Or use it as an example to build it from scratch in MakeCode. Remember, if you are building from scratch, you will need to install the appropriate extension when using the controller:bit.


Note: You may need to disable your ad/pop blocker to interact with the MakeCode programming environment and simulated circuit!

Code to Note

When the micro:bit is powered up, we'll want it set up the radio to a certain channel. In this case, we set the radio block to 1 just like experiment 1. Then we'll want to check if the P16 button is pressed on the controller:bit, just like an accelerate button used in driving games. For simplicity, we will want the robot to move forward when pressing the up (P0) button on the direction pad. We will be using a nested if statement to check on the buttons defined in the gamer:bit extension. A nested if statement is one or more if statements "nested" inside of another if statement. If the parent if statement is true, then the code looks at each of the nested if statements and executes any that are true. If the parent if statement is false, then none of the nested statements will execute. By using the logic statement, we will be using the gamer:bit ____ is pressed block.

Once both buttons are pressed, we will send a command out. In this case, it will be number 0. For feedback, to see if our code works as expected, we will have the LEDs animate with an arrow pointing up and a square growing bigger. We then give the micro:bit a short pause before clearing the screen and looping back to the beginning of the forever loop.

MakeCode Remote Control Example

Having a hard time seeing the code? Click the image for a closer look.


2.2 Robot Receive

In this part of the experiment, we need to have a receiving micro:bit recognize the command that was sent from the first micro:bit in order to control the micro:bot. For simplicity, we will have the robot drive forward. To debug, the LED array will display an arrow to indicate the direction where the robot should move for feedback.

Hardware Hookup

At this point, you should have your micro:bot kit assembled! We're continuing on from experiment 5. Make sure to check out the guide before continuing on.

micro:bot Kit Experiment Guide

February 20, 2020
Get started with the moto:bit, a carrier board for the micro:bit that allows you to control motors, and create your own robot using this experiment guide for the micro:bot kit.

To avoid confusion when uploading code, unplug the first micro:bit from your computer. Connect the second micro:bit to your computer via USB cable.

Micro:bot Moto:bit Micro:Bit USB Cable

Running Your Script

Download the following example script and move the *.hex file to your micro:bit. You can also use it as an example to build it from scratch in MakeCode. Remember, if you are building from scratch, you will need to install the appropriate extension when using the moto:bit.


Note: You may need to disable your ad/pop blocker to interact with the MakeCode programming environment and simulated circuit!

Code to Note

When the second micro:bit is powered up, we'll want to set the radio to the same channel as the first micro:bit; again to 1. As explained in the micro:bot experiment guide, we will want to set the left and right motors' logic based on the way we connected the motors to the motor:bit. For consistency, we will make both true. Using the on radio received __________ block from the moto:bit extension, we will want to check to see what command was received. In this case, it should be a 0 that was sent from the first micro:bit. If the command that was sent matches 0, we will want the moto:bit to drive forward at 100%. For feedback, we will have an arrow point up. After a short pause of about 50ms, we will want to clear the screen and turn the motors off before checking again. If the pause is too long, the micro:bot will continue to drive forward even after you remove your fingers from the controller:bit's buttons.

MakeCode Receiving micro:bot Code

Having a hard time seeing the code? Click the image for a closer look.


What You Should See

Now that both micro:bits are programmed, let's the test code out. Disconnect the USB cables from both micro:bits and power each with the respective battery packs.

Inserting JST Connector into micro:bit 2xAA Battery Pack INserted into JST Connector of micro:bit

For the micro:bot, insert the 4xAA battery pack into the barrel jack.

Barrel Jack Being Inserted into moto:bit 4xAA Battery Pack Inserted into Barrel Jack of moto:bit

Then move the switch labeled as RUN MOTORS to the ON position. Pressing on the drive button (P16) and up button (P0) on the controller:bit will cause the micro:bot to drive forward. You should also see the LED array animate.

Demo Test Wireless Control micro:bot with controller:bit