Using the Serial 7-Segment Display

≡ Pages
Contributors: jimblom

Resources and Going Further

Now that you're comfortable using one of the Serial 7-Segment Displays, it's time to incorporate it into your own project!

For even more information on the 7-segment displays, please check out the Serial 7-Segment's github repository. There you'll find:

  • Datasheet - A Wiki containing all of the information you should need to use the display.
  • Arduino Example Code galore - We went a little crazy with the test code. You'll find something useful here.
  • Firmware - If you're interested in modifying the behavior of the S7S, definitely check out the firmware (written in Arduino).
    • In addition to the firmware, you'll also need to add the SevSeg library to your Arduino install.
  • Hardware - The Eagle files are hosted here. Do you want to make your own version of the display? Go for it! This is an open-source project.

Additional Tutorials and Examples

For an example using the serial 7-segment display with Raspberry Pi, I2C, and Python, check out this tutorial:

For an example using the 7-segment serial display with Raspberry Pi, I2C, and MatLab support package, check out this tutorial:

Need some inspiration for your next project? Check out some of these related tutorials:

Using OpenSegment

How to hook up and use the OpenSegment display shield. The OpenSegment is the big brother to the Serial 7-Segment Display. They run on the same firmware, however the OpenSegment is about twice as big.

Dungeons and Dragons Dice Gauntlet

A playful, geeky tutorial for a leather bracer that uses a LilyPad Arduino, LilyPad accelerometer, and seven segment display to roll virtual 4, 6, 8, 10, 12, 20, and 100 side dice for gaming.

Reaction Timer

Demonstrate mental chronometry with this simple reaction timer!

Alphanumeric GPS Wall Clock

This is a GPS controlled clock - a clock you truly never have to set! Using GPS and some formulas, we figure out what day of the week and if we are in or out of daylight savings time.

Large Digit Driver Hookup Guide

Getting started guide for the Large Digit display driver board. This tutorial explains how to solder the module (backpack) onto the back of the large 7-segment LED display and run example code from an Arduino.

Building a Safe Cracking Robot

How to crack an unknown safe in under an hour.

Going big? Maybe you would like to build a large 12" GPS Wall Clock installation:

Updated GPS Clock

Updated GPS Wall Clock in the SparkFun Emporium Based on the Old 12" GPS Wall Clock Tutorial

For more information on the updated GPS Clock in the SparkFun Emporium, check out the Big_GPS_Clock GitHub repo.

Or check out the following blog for ideas.